Search Results for rave report setparam
SeeHawk® Reports | Test & Measurement - PCTEL
Report KPIs for 2G/3G/4G/5G cellular, WiFi, P25, TETRA, DMR, NB-IoT, and LAA networks; Report Spectrum Analysis (SA) and Enhanced Power Scan (EPS) measurements; Merge multiple tests into a single report; Filter by operator, channel, and technology; Visualize with maps and optional distribution charts; Automatically export reports to Word
SeeHawk Reports - PCTEL
SeeHawk® Reports is PCTEL’s easy-to-use drive and walk test post-processing solution for PCTEL® scanning receiver data. Compatible with both SeeHawk® Touch and SeeHawk® Collect network testing software, SeeHawk Reports enables you to: NEW! Submit JOTS (Joint Operations Technical Standard) compliant reports with 1st through 5th-best server plots.
Common Reporting Tool - KAYE
The new version 1.4 supports merging of up to three Kaye Validator AVS or ValProbe RT studies into one single report. Additionally, new reports are available for the validation of climatic and thermostatic chambers in compliance with AFNOR FD X15-140 or IEC 60068 normative documents for ValProbe RT.
SeeHawk® Touch Software | Test & Measurement - PCTEL
Generate printable, customizable reports from PCTEL® scanning receiver data within minutes of completing a drive or walk test with SeeHawk® Touch or Collect. SeeHawk Reports even merges multiple data sets, simplifying multi-day benchmarking or site survey campaigns.
SeeHawk® Collect Software | Test & Measurement - PCTEL
Generate printable, customizable reports from PCTEL® scanning receiver data within minutes of completing a drive or walk test with SeeHawk® Touch or Collect. SeeHawk Reports even merges multiple data sets, simplifying multi-day benchmarking or site survey campaigns.
Data Sheet R-Series V RF5 EtherNet/IP - temposonics.com
The R-Series V EtherNet/IP™ can detect and report the position and velocity of up to 20 magnets simultaneously. R-Series V EtherNet/IP™ The sensor supports DLR. The DLR capability provides a fault-tolerant network so that the sensor can be used in ring connection topologies when reliable continuous system operation is required.
Download Antenna Test Results - Amphenol Antenna Solutions
Enter the serial number located on the back of the antenna to download the test results: PLEASE NOTE: It may take some time to generate the test result. Check your downloads folder for the PDF file. Amphenol professionals are ready to assist with any questions you have regarding our products. Do not hesitate to contact us with questions.
RET user guide - Amphenol Antenna Solutions
Amphenol Antenna Solutions offers its own RET control solution. The PCU-4 tool is delivered as a kit comprising of a computer software application together with a HW test interface with all the necessary cables and accessories.
Data Sheet R-Series V RF5 SSI (document part number: 552207)
Each Temposonics® position sensor consists of a ferromagnetic waveguide, a position magnet, a strain pulse converter and supporting electronics. The magnet, connected to the object in motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide.
Data Sheet R-Series V RM5 POWERLINK (Doc Part No. 552117)
With extrapolation, the sensor is able to report data faster than the native cycle time, independent of the stroke length of the sensor.
Amphenol – Antenna Test Result Icon2
Amphenol Antennas is your wireless communications network partner. Supporting your needs with innovative and tailored antenna solutions for optimal coverage and capacity.
AT Connector Evaluation Test Report - Amphenol Sine
The receptacle connector is secured and inserted into a plug connector with a constant speed of about 100mm/min in the direction of the axis. The locking mechanism of the connector body is used with the lock engaged. All tests were passed with the judgment condition satisfied. Refer to No. 1 for test data.
SeeHawk® Network Testing Software | Test & Measurement - PCTEL
Generate printable, customizable reports from PCTEL® scanning receiver data within minutes of completing a drive or walk test with SeeHawk® Touch or Collect. SeeHawk Reports even merges multiple data sets, simplifying multi-day benchmarking or site survey campaigns.
Data Sheet R-Series V RDV PROFINET (Doc Part No. 552139)
The R-Series V PROFINET can detect and report the position and velocity of up to 30 magnets simultaneously. R-Series V PROFINET In addition to the measured position value via the PROFINET protocol further data about the current sensor status, such as the total distance travelled, the internal temperature and the total operating
Automated Spectrum Monitoring and Uplink Testing - PCTEL
Ensure critical communications coverage and meet building code requirements with this automated grid-based testing and reporting solution for public safety, private radio, and LTE/FirstNet networks. Accurately detect interfering frequencies and locate their exact source with the intuitive, hand-held SeeWave® interference locating system.
Testing RxMER at the output of nodes and amplifiers
So, as is the case now, the RF technician doesn’t know whether to report the RxMER estimate as a failure or assume it is good enough and move on to the next node or amplifier. What has just been described goes on every single day in the field and is widely known throughout our
Verification report of Greenhouse Gases emissions Scope 1 and 2 and ...
Amphenol has written and implemented a guidance to provide instructions for reporting on the ENVIRONMENT & GOVERNANCE indicators used within Amphenol’s Sustainable Development Reporting System (SDRS). The key procedures are “Corporate Sustainability Reporting - Guidance for Measuring and Reporting - Part 1 – Environment & Governance”.
Data Sheet R-Series V RF5 PROFINET (document part number: 552211)
The R-Series V PROFINET can detect and report the position and velocity of up to 30 magnets simulta-neously.
Data Sheet R-Series V RF5 EtherCAT - temposonics.com
The R-Series V EtherCAT® can detect and report the position, velocity and acceleration of up to 30 magnets simultaneously.