Search Results for sgs report
Amphenol Corporation - Financials - SEC Filings - SEC Filings Details
Sustainability Report 2016; Supplier Code of Conduct (cn) Supplier Code of Conduct (de) Supplier Code of Conduct (en) Supplier Code of Conduct (fr) Supplier Code of Conduct (sp) Anti-Human Trafficking & Slavery Statement; Conflict Minerals; Investors; Investor Relations SEC Filings Details. Investor Overview. News & Events.
Wire and Cable Certifications Explained
To complete a certification via third-party NRTL, the cable is submitted for testing and evaluation to the required applicable standard(s). The NRTL will perform an investigation of the cable through inspection, evaluation, and testing of the subject cable.
Fiber Cable Preparation, Splicing, and Termination Instructions
equipment was damaged in transit, imm ediately report the damage to the transportation company. 3. Remove outer dome from base. To remove the outer dome, use a 216 tool or can wrench to turn the snap lock’s hex nut 1/4-turn counter-clockwise. Hold the can wrench in that position and lift the dome. Set the dome aside until needed. Hex nut in ...
GENERAL DESCRIPTION im - Charles Industries
damaged in transit, immediately report the extent of damage to the transportation company. Equipment Identification Charles Industries’ equipment is identified by a model and issue number imprinted on the front panel or located elsewhere on the equipment. Each time a major engineering design change is made on the equipment, the
NJMMEN-0002 | OSFP 800G Straight Cable Assembly | Amphenol
OSFP Cable Assembly, Passive, 25AWG, 2M, 112G / Lane, Flex Sleeve
FASTENER TESTING SYSTEMS - PCB
5 EXAMPLE TEST SYSTEM CONFIGURATIONS PART NUMBER DESCRIPTION* 080962-01000 Model 962 2-channel Recorder 08CLEC-00MTR DC Drive Motor, 15-150 Nm, 165 RPM max, controller and
NUMBER GS-12-622 Product Specification - Amphenol CS
GS-29-622 10G Qualification Test Report Summary EL-2012-05-033 14G Qualification Test Report EL-2012-12-023 28G Qualification Test Report 3.2 INDUSTRY DOCUMENTS FIT, FORM AND FUNCTION SFF-8436 QSFP+ Copper and Optical Modules SFF-8661 QSFP+ 28 Gb/s 4X Pluggable Module (Style A) SFF-8662 QSFP+ 28 Gb/s 4X Connector (Style A) or
Airmar WeatherStation 200WXRS232RH Smart Sensor - Gemeco
The WeatherStation 200WX is the best choice for mobile, weather-monitoring applications. Sensor rich, in a durable, rugged, small housing that is IPX6 rated, means the 200WX can be used on moving platforms such as TV-news and military vehicles.
ISO 9001: 2000 - borisch.com
Aerospace Sector Scheme and documented in Report No. 4060. Proof has been furnished that the requirements according to . AS9100D / ISO 9001:2015 . are fulfilled. Further clarification regarding the scope of this certificate and the applicability of AS9100D / ISO 9001:2015 requirements may be obtained by contacting TRNA. Certificate Registration No.
Amphenol Corporation - Financials - SEC Filings - SEC Filings Details
Sustainability Report 2016; Supplier Code of Conduct (cn) Supplier Code of Conduct (de) Supplier Code of Conduct (en) Supplier Code of Conduct (fr) Supplier Code of Conduct (sp) Anti-Human Trafficking & Slavery Statement; Conflict Minerals; Investors; Investor Relations SEC Filings Details. Investor Overview. News & Events.
Digital Fluid-TracTM (DFT-210) Multi-Unit Drum Gauge With 4-20mA ...
report the level readings in two forms – LCD digital display and 4-20 mA current output. The 4-20 mA electrical output can be used to interface to external controllers and test equipment. When powered using two 9-volt batteries depressing the Reset/Select button will initiate a 7 second level measurement. This measurement is then displayed
7305–46 Data Channel Interface W/SC Generator - Charles Industries
If the equipment has been damaged in transit, immediately report the extent of damage to the transportation company. Charles Industries equipment is identified by a model and issue number imprinted on the front panel or located elsewhere on the equipment. Each time a major engineering design change is made on the equipment, the issue
PCTEL Automates Commissioning Tests for In-Building Public Safety Radio ...
BLOOMINGDALE, Ill.--(BUSINESS WIRE)--PCTEL, Inc., an Amphenol company, today announced a commissioning test automation system that makes it easier to install code-compliant BDAs (bi-directional amplifiers) that provide reliable in-building communications coverage for first responders.PCTEL’s BDA commissioning test system automates key tests that are needed to comply with FCC, NFPA (National ...
QUALIFICATION TEST SUMMARY REPORT - Amphenol Aerospace
Qualification Test Summary Report 2M803 Series B 29 July 2013 Page 9 of 10 7.3 Group 3-Sample Breakdown . Two mated pairs of each connector size shall be prepared with two foot lengths of AS22759/11-24 wire. Two mated pairs of Amphenol/Competitor Connectors, each connector size shall be
Amphenol Corporation - 1st Quarter 2021 Earnings
Amphenol will have a conference call to discuss 1st quarter results on Wednesday, April 28, at 1:00 PM ET. To listen to the call, please use the following dial in numbers.
NDYSYH-0005 | QSFP DD 400G - 4x QSFP Splitter Cable Assembly | Amphenol
QSFP DD - 4x QSFP Cable Assembly, Passive, 27AWG, 2.5M, 56G / Lane, Jacket
Telecommunications Group Section 365-280-802 Equipment Issue 2 CAUTION ...
immediately report the extent of damage to the transportation company. Equipment Identification Charles equipment is identified by a model and issue number that is visible on the outside of the unit. The exact location of this information may vary slightly depending on the equipment. Each time a major engineering design change is
IECEx Certificate of Conformity - PCB
Quality Assessment Report: PCB Piezotronics of North Carolina Inc. 10869 Hwy 903 Halifax, NC 27839 United States of America FR/LCIE/ExTR12.0028/00 FR/LCIE/ExTR15.0069/00 FR/LCIE/ExTR15.0117/00 FR/LCIE/ExTR16.0088/00 FR/LCIE/ExTR21.0053/00 FR/LCIE/ExTR22.0065/00 NL/DEK/QAR14.0004/05.
TN-9 Shunt Calibration of a Strain Gage Sensor - PCB
Definition Shunt calibration is the known, electrical unbalancing of a strain gage bridge, by means of a fixed resistor that is placed, or “shunted”, across a leg of the bridge.
630510005 | QSFP 100G Loopback | Amphenol
QSFP Loopback, Mode Select, 1.5W, 0dB Attenuation, Green Lanyard, No Eye/Jitter Test, 28G / Lane