Search Results for show snmp group
360-80 SNMP Network Node Manager (NNM) Setup Guide
SNMP agent software is preloaded in the firmware and is used to manage ICB shelves from a common control center. This is done using SNMP manager software. The SNMP manager is used to monitor, provision and con-trol multiple 360-80 ICBs and can communicate with local and remote shelves.
Network Management System and ICB Management System Software User’s Guide
Use this software to manage the Charles ICB. The NMS system consists of PC software which provides a graphi-cal user interface (GUI) used to provision, control, and monitor multiple 360-80 ICBs. The PC communicates through an Ethernet interface.
Franchise Ph. 3.5 CLI Commands - Amphenol Socapex
Document Conventions Note: Provides related information or information of special importance. Caution: Indicates potential damage to hardware or software, or loss of data. Warning: Indicates a risk of personal injury. Document Status Doc Status: Page 2/876 Version 1.0 06/03/2013
SCU User Guide Version 3 - Amphenol Antenna Solutions
The Site Control Unit (SCU) is a site controller for AISG devices installed at a cell site. It is compatible with the AISG (Antenna Interface Standards Group) standard and can control up to (24) AISGv1.1 and/or AISGv2.0 devices, such as RET (Remote electrical tilt) and TMA (Tower-mounted amplifier), at a site.
nrgSMART CTRL - amphenol-ns.com
Amphenol Network Solutions new integrated nrgSMART controller provides a clean, simple user interface that can be deployed in each 1RU nrgSMART panel. For those desiring a single connection point for multiple panels, the new integrated controller can monitor and communicate data for up to 30 nrgSMART enabled PDUs.
Network Management System and ICB Management System Software for T1 ...
Use this software to manage the Charles ICB. The NMS system consists of PC software which provides a graphi-cal user interface (GUI) used to provision, control, and monitor multiple 360-80 ICBs. The PC communicates through an Ethernet interface.
T1 Controller with SNMP (3603-81) - Charles Industries
This is achieved through the craft interface using RS232, SNMP using Ethernet or a proprietary graphical interface using Ethernet. For operation of this interface, see the Craft Port documentation, SNMP Network Node Manager docu-mentation or Network Management Software documentation.
Network Switch Software Documentation - Amphenol Aerospace
This command will return the parameters/settings for the currently selected VLAN, any specific VLAN by index, or show a list of all configured VLANs. Examples: “GET VLAN” → shows a parameter/settings list for the currently selected VLANs “GET VLAN 5” → shows the parameter/settings for VLAN index 5
nrgSMART™ Remote Monitoring - Amphenol Broadband Solutions
o SNMP interface comes standard when used with nrgCONTROL-BT Key Features • Monitoring: Gain insight to troubleshoot and prevent power issues in your network
Amphenol Network Solutions > nrgSMART CONTROLLER
For customers using legacy nrgSMART products without integrated controller capabilities, the nrgCONTROL-BT controller provides the communications needed, including a rich HTML user interface for configuring settings, and SNMP connectivity for reporting and alarms.
Advanced Real-Time Monitoring Reveals the Details of Power Usage
Integrated controllers/monitors typically utilize a software-based (usually SNMP) network management system (NMS) to provide data 24/7 through remote, non-intrusive monitoring, enabling the archiving of historical data and short- and long-term analysis.
360-80 Intelligent Channel Bank Craft Terminal for T1 User’s Guide
Note: This document’s issue number follows the equipment issue number of the T1 controller unit with SNMP (T1-S). Use this software to manage a single ICB shelf. This interface will not allow the user to communicate with any ICB system other than the one it is connected to.
Amphenol
Our sensors and sensor-based product solutions include gas and moisture sensors, level sensors, position sensor, pressure sensors, temperature sensors and vibration sensors. Our value-added cable assemblies include cable assemblies and harnesses, cable management products and backplane interconnect systems.
Ethernet Military Switch RJSML-8ELMG - Amphenol Socapex
What are SNMP, RMON and MIB? SNMP (Simple Network Management Protocol) and RMON (Remote Monitoring) provide a means to monitor and manage your network. Each SNMP device maintains Management Information Bases (MIB s) containing information about the operation and configuration of the device. Each MIB contains a variety of information such as:
The Brain of Modern Vehicles: Understanding Car Computing
At the core of car computing lies the Central Computing Unit, often referred to as the vehicle's brain. This pivotal component is responsible for aggregating and integrating a myriad of electronic systems, ensuring that every aspect of the vehicle operates in harmony.
Application Overview – SNMP
Description: The SNMP (Simple Network Management Protocol) feature provides a standard user interface to monitor, provision, and control multiple 360-80 systems. To support SNMP, a 360-80 system must be equipped with an SNMP T1 controller card.
International Paris Air show 2025 | Amphenol Socapex
Amphenol is proud to announce its participation in the Paris Airshow 2025, the world’s leading aerospace and defense exhibition. Join us from June 15 to 21 at Le Bourget, Paris, to explore our advanced interconnect solutions for the aerospace and defense industries. What to Expect:
360-80 Intelligent Channel Bank Turn-Up and Acceptance Test Procedure
Use the following steps to turn up the system. Only the T1 controller unit (T1-S) should be installed as instructed. Figure 2 displays the T1 Controller Unit Front Panel. Insert the T1-S into the ICB. Do NOT connect the T1 to J1 at the rear of the T1-S.
Application Overview - Protection Mode - Charles Industries
Description: Protection mode allows two 360-80 systems to be connected with redundant T1 facilities. In this configuration, each 360-80 system is equipped with a Secondary T1 Controller card and a SNMP T1 Controller card. The Primary T1 from the SNMP T1 Card is used as transport.
3608-80 Secondary T1 Unit - Charles Industries
The ST1U is a secon-dary T1 unit for the ICB, providing normal/drop and re-insert (D&RI), dual T1 mode and protection mode when used with the T1 controller with SNMP (T1-S). Mount the ST1U in the secondary (half-size) slot of the 360-80. One T1-S controller unit (issue 2 or later) must be installed in the primary slot for proper system operation.