Search Results for slimline
Circular Connectors for Industries - Amphenol CS
A circular connector can be defined as a circular interface with cylindrical contact housing. These connectors are used in various industries for data, signal and power connections in the AI, military, aerospace, data, communication, and manufacturing. These flexible and versatile connectors find use in harsh environments with its rugged ...
Amphenol Communications Solutions releases Internal High-Speed Link ...
Amphenol Communications Solutions releases Internal High-Speed Link Input Output Connectors Performing to PCI-SIG Gen 6 Specifications - Designed for Next Generation Enterprise Server Equipment
The New Self Aligning BergStak® 0.50mm Connectors - Amphenol CS
BergStak ® 0.50mm Self-alignment connector features a wide guide distance for mating of ±0.85 mm in the pitch direction and ±1.29 mm in the width direction. These low profile connectors are footprint compatible with standard BergStak ® 0.50 connector. These connectors can be ideally used for applications in the Automotive and Industrial ...
PCIe® 6.0- The Ultra-Speed Computing Standard - Amphenol CS
PCIe ® 6.0 Specififcations. Now PCI-SIG has announced its sixth generation, the PCIe ® 6.0, which is targeted to be released by 2021 and is designed to meet the evolving trends including Artificial Intelligence and Big Data. The new standards will be introduced with double the data rates i.e, it will take a leap to 64GT/s from the 32GT/s of ...
Choosing The Right Connectors For PCB - Amphenol CS
Choosing The Right Connectors For PCB. Apr 27, 2018. PCBs are boards made of a non-conductive material which has conductive lines printed or etched on it. Electronic components are mounted on the board and the traces connect them together to form a working circuit. An effective PCB design is vital in determining the performance of any device.
Learn About Connector Termination Styles - Amphenol CS
There are also wire termination styles that deal with how the wire is attached to the contacts of the connector, including crimping, push-in, screw termination, and wire wrapping. Amphenol offers a large portfolio of wire-to-board solutions that have a mix of these styles. Most applications require a particular type of termination to match ...
Mini Cool Edge IO Connectors for 5G and Datacenters - Amphenol CS
Wind Turbine (1) clincher (1) sustainability (1) Amphenol’s Mini Cool Edge IO connectors are internal high-speed OverPass™ connectors that allow high-speed signal transmission in Data Centers, Network Routings, and 5G Telecommunications. These connectors offer more advanced and powerful features over the existing interconnect solutions.
Amphenol ICC at InterBattery Korea
Amphenol ICC at InterBattery Korea. Nov 19, 2018. InterBattery Korea is one of the most important trade fairs for the production and development of rechargeable batteries and has served as an exclusive business platform for the industry’s potential prospects ever since it was first launched in 2013. This year’s exhibition was held from 10 ...
Enabling Connector Innovations through Plating - Amphenol CS
Enabling Connector Innovations through Plating. Dec 7, 2017. Plating technology defines the mating cycles, durability and performance of connectors. GXT ®, AGT ®, and GCS ® are innovative plating solutions that create durable, reliable, and economical connectors with increased efficiency. GXT ® plating, a mix of palladium-nickel with gold ...
Space-Saving PCIe® Gen 5 Flip CEM - Amphenol CS
The PCIe ® Gen 5 Flip CEM is a newly introduced vertical card edge connector that adheres to the PCIe ® standard mating interface. Its unique design features "JJ" or "LL" type contacts, resulting in a significant reduction of up to 19.5% in the keep-out area compared to traditional CEM connectors. Amphenol’s Flip CEM connectors can support bandwidths up to 32GT/s (Gen5) and can mate with ...
Amphenol ICC Develops 112Gb/s Interconnect Technology with eTopus ...
San Jose, CA, USA – Amphenol ICC, the global leader in connector technology, design and manufacturing, and eTopus Technology, a pioneer of ultra-high-speed ADC/DSP-based SerDes for wireline applications including data center, cloud, edge, and 5G base stations, today announced the development of a 112Gb/s interconnect technology built on their products.
Amphenol Cables on Demand: Unparalleled Quality, Unmatched Service
Amphenol Cables on Demand is more than just a cable provider; it's a reliable partner in innovation. With a commitment to quality, customization, and unmatched industry partnerships, ACD stands at the forefront of the cable industry. For those seeking top-tier interconnect solutions, ACD sets the benchmark for excellence and customer satisfaction.
Learn More about Connector Mating Cycles - Amphenol CS
The number of times a connector can connect and disconnect with its counterpart while meeting all its specifications is termed as “mating cycles”. The mating cycle of a connector helps to estimate the life span of a connector in a particular application. For instance, while the mating cycle for a USB connector will be in thousands, a FFC ...
RAM Advancements - From SDR to DDR4 and More
With a data rate of 2GB to 16GB, it enables large capacity subsystems. The DDR4 standard allows for DIMMs of capacity, up to 64GB when compared to a maximum of 16GB per DIMM of DDR3. Many varieties of DDR4 sockets and modules are available in the market. The Ultra Low Profile (ULP) vertical DIMM sockets are an ideal choice for ultra-thin ...
Fundamentals of Signal Integrity
The science of signal integrity makes use of the time, frequency, amplitude and phase characteristics of the signal to set certain rules and regulations to be adhered to obtain the best results. The much popular Laplace Transform used to convert time-bound characteristics of a mathematical function into their frequency-bound counterparts is ...
FlexLock® for Simplifying Battery Management System Designs - Amphenol CS
Amphenol provides many interconnect solutions, that add to the reliability and performance of a battery management system. FlexLock ® FPC-to-Board connector is a key solution that is designed with BMS in mind. This compact automotive grade connector is compliant with USCAR-T2V2 specifications. With a nominal current carrying capacity of 3A per ...
Top Things to Consider for Energy Storage System Connectors - Amphenol CS
Battery Storage System is at the heart of the ESS. Amphenol has Busbar connectors and cables as well as Input Output solutions going into 48V / 1000V / 1500V Lithium ion battery racks. Our BarKlip ® connectors offer the smallest 150A+ ESS solution in the market with a high current rating of up to 160A /200 /300A per contact @ 30°C T-Rise. With a wire range of 8AWG-0AWG, these connectors ...
M-Series – Advanced Ball Grid Array (BGA) Connector for 56Gb/s, PAM4 ...
M-Series™ is designed to support these high technology products, in board-to-board or flex assembly architectures, with next-generation differential pair contact design for 56Gb/s NRZ, 112Gb/s PAM-4 performance. Amphenol ICC is a leading innovator in the design, development and high volume manufacturer of Ball Grid Array ( BGA) connectors ...
The Fastest Path to Wireless Charging with Amphenol and NuCurrent
Shanghai Amphenol Airwave Communication Electronics Co., Ltd, a subsidiary of Amphenol Corporation has partnered with NuCurrent, a global player in wireless power systems. This partnership will address the need to shift toward new standards such as Qi2 (pronounced “cheē tü”) standard. “Our partnersh
E-Bikes – An Easy Biking Solution - Amphenol CS
Amphenol ICC provides customized solutions for several applications in e-bikes including batteries, display units, motors, control levers, and derailleurs. Our custom plug-and-play rectangular connectors interface the charging stations with the batteries. Circular cable assemblies supply the battery power to control lever and derailleurs.