Search Results for smartq c368 usb 3.0 card reader manual
WATER RESISTANT USB3.0 CONNECTOR SERIES ASSEMBLY INSTRUCTIONS
The UTP is intended to transmit the USB 2.0 signalling while the SDPs are used for SuperSpeed; the shield is needed for the SuperSpeed differential pairs for signal integrity and EMI performance.
10129368-001C-TRLF | SAS | Amphenol
Amphenol is one of the leading manufacturers of Storage and Server connectors. Contact us today for more details of Sas, part number 10129368-001C-TRLF
CUSTOMER OUTLINE DRAWING - Amphenol RF
%PDF-1.7 %âãÏÓ 19 0 obj > endobj 34 0 obj >/Filter/FlateDecode/ID[8CE2D950015FF34782F4AED38D5BB884>328ECB041045B74CBC29C95077529137>]/Index[19 25]/Info 18 0 R ...
CUSTOMER OUTLINE DRAWING - amphenolrf.com
NOTICE: These drawings, specifications, or other data (1) are, and remain the property of Amphenol corp. (2) must be returned upon request; and (3) are confidential and not to be disclosed to any person other
SINGLE MODULAR USB - amphenolpcd.com
Available from 10.5W up to 60W, and configurable in any variation of USB-A and USB-C, APCD’s modular charger is the perfect solution to reduce down time, save on replacement cost, and extend the life of initial purchase.
Assembly Instructions-C36 Amphenol TNC
Step 1 Strip cable jacket, braid, and dielectric to dimensions in table above. All cuts are to be sharp and square. Important: Do not nick braid, dielectric, and center conductor. Slide outer ferrule onto cable as shown. Flare slightly end of cable braid as shown to facilitate insertion of inner ferrule. Important: Do not comb out braid.
HT100 Hand-Held Terminal - temposonics.com
manual describes the operation of the HT100 in detail only and will, at times, refer you to either the DDA or STI operation manual for detailed information regarding the command protocol, etc.
UMBER GS-12-0983 PRODUCT SPECIFICATION - amphenol-cs.com
umber gs-12-0983 type product specification title page revision hdmi d type receptacle connector authorized by date 3 of 7 b leif shen 09/30/2011
6-Port Antenna
See details below and refer to the ordering options to see which actuators are available with this particular antenna. A single actuator individually controls the tilt of each band (no need for daisy chain cables between the bands). This module does not add any additional length to the antenna.
Model 485B36 USB, Dual-channel, ICP® Sensor Signal Conditioner ...
%PDF-1.4 %âãÏÓ 8 0 obj > endobj 123 0 obj >/XObject >/ProcSet[/PDF/ImageB]>> endobj 122 0 obj >stream H‰Òw 6TH/æå*äå234Ñ30PAsK 39——Kß3×PÁ%Ÿ ...
Model 1380-03A rod end load cell Installation and Operating Manual - PCB
The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 ... 3 0.72 18.3 0.97 24.6 4 ∅1.50 ∅38.1 ∅1.50 ∅38.1 5 1.86 47.3 2.12 53.8 6 0.83 21.1 0.83 21.1 7 1.31 Wrench Flat 33.3 Wrench Flat 1.31 Wrench Flat
INSTRUCTION MANUAL For Model 7360A/7360AM1 6-DoF SENSOR IM7360A, Revision B
following sections of this instruction manual apply to both 7360A and 7360AM1 except for section 6.1. 3.0 Materials Required . All the materials used in the mounting of the Model 7360A 6-DoF sensor are supplied with the unit in the shipping container. These materials, as shown in Figure 1, include:
Sundy - Amphenol CS
Scope - This specification covers the insulation piercing QuickieTM Connector designed for printed wiring board-to-flat cable (round conductor) interconnection in low power applications. In all applications the mated system (male to female) plating should be gold to gold or GXT to GXT. The specification is composed of the following sections.
10134160-5330LF | Minitek® Pwr 3.0 | Amphenol
Amphenol is one of the leading manufacturers of Wire to Board Connectors. Contact us today for more information of Minitek® Pwr 3.0 Connector, Part Number 10134160-5330LF.
Model 377C41 Precision Condenser Microphone Installation and ... - PCB
Installation and Operating Manual For assistance with the operation of this product, contact PCB Piezotronics, Inc. Toll-free: 800-828-8840 24-hour SensorLine: 716-684-0001 Fax: 716-684-0987 E-mail: info@pcb.com Web: www.pcb.com
Enhanced Cooling with Smart Card-to-Wire (CTW) Fan Modules - Amphenol CS
Amphenol’s CTW (Card-To-Wire) Fan Module connectors come with a flexible design for card-to-wire power applications used in fan modules. These hot-pluggable rear tray connectors are ideal for network switches; accommodating different wire gauges ranging from 28AWG to 22AWG and provide a maximum current rating of 4A/pin.
Model 2508-03A REACTION TORQUE SENSOR Installation and Operating Manual
manual for specific wiring of the supplied torque sensor. The gages are bonded to the sensor’s structure. Typically, a regulated DC or AC excitation is applied between A and D of the bridge. When torque is applied to the sensor, the Wheatstone Bridge becomes unbalanced, causing an output
Model 2508-05A REACTION TORQUE SENSOR Installation and Operating Manual
manual for specific wiring of the supplied torque sensor. The gages are bonded to the sensor’s structure. Typically, a regulated DC or AC excitation is applied between A and D of the bridge. When torque is applied to the sensor, the Wheatstone Bridge becomes unbalanced, causing an output
Model 376B02 ICP Microphone System Installation and Operating Manual - PCB
Installation and Operating Manual For assistance with the operation of this product, contact PCB Piezotronics, Inc. Toll-free: 800-828-8840 24-hour SensorLine: 716-684-0001 Fax: 716-684-0987 E-mail: info@pcb.com Web: www.pcb.com
CHARGE MODE PRESSURE SENSORS - PCB
Charge mode pressure sensors for power generation applications are used for on-turbine combustion instability monitoring. Lean-burn and dry low NOx turbines, designed by gas turbine manufacturers to meet nitrogen oxide emission regulations, operate with low fuel-to-air ratios.