Search Results for soldering iron fail
MILIT A A A RECOMMENDED GUIDELINES FOR SOLDERING AND CLEANING OF ...
Amphenol recommends that cleaning after soldering must not be done by immersion in a cleaning solution. After soldering, solder joints can be brush cleaned with isopropanol, preferably while holding the connector with its soldered contacts facing downward at an angle.
Amphenol Aerospace
Remove the inner contact & tin the cable center conductor using a 47.5 watt soldering iron (inner contact wire well may also be tinned). Solder the center conductor into the inner contact wire well. A pin vice can be used to hold the inner contact. 1.
Repair and Maintenance Returning Equipment Contact Information Safety ...
Solder X O O O O O Copper Alloy/Brass X O O O O O This table is prepared in accordance with the provisions of SJ/T 11364. O: Indicates that said hazardous substance contained in all of the homogeneous materials for this part is below the limit requirement of GB/T 26572. X: Indicates that said hazardous substance contained in at least one of the ...
L-1107-AH.fm - Amphenol Aerospace
3. Tin center conductor, and using a 47.5 watt soldering iron, solder the center con-ductor into the inner pin contact wire well. A pin vise can be used to hold the inner contact. H1. Slide front insulator, large end first, over the inner pin contact until insulator seats against the inner pin contact shoulder.
Amphenol Aerospace
Tin center conductor, and using a 47.5 watt soldering iron, solder the center conductor into the inner pin contact wire well. A pin vise can be used to hold the
termination-instructions-sae-circular-gt-series-amphenol-industrial
This publication contains instructions for installing, disassembling, inspecting and reassembling Amphenol, SAE AS5015, AC Threaded, ACA Reverse Bayonet and GT Reverse Bayonet Connectors manufactured by Amphenol Industrial Operations in it’s different Manufacturing Divisions. SAE AS50151, AC, ACA and GT Series, Containing Crimp Contacts.
Amphenol Amphenol Taiwan Corporation Sheet 1
• Solder area: Gold flash or matte tin plating • Under-plating: Nickel overall 3.2.3 Shell • Copper Alloy or Stainless steel Solder area: Matte tin plating •) • Under-plating: Nickel overall 3.3 Rating • Voltage rating: 30 VAC • Operating temperature: -40°C~ 85°C • Storage temperature: -40°C~ 85°C • Ambient humidity: 85% R ...
Amphenol Amphenol Taiwan Corporation
Unmated Solder shall cover a minimum of 95% of the surface being immersed, when soldered at temperature 245℃+/- 5℃ for in immersion duration 5s. Resistance to soldering heat EIA-364-56 Dip connector terminal tails in solder: Solder Duration:10±0.5seconds; Solder temperature:260±5℃ Unmated No physical damage. (refer to FIGURE 3
97-e-series-first-mate-last-break-fmlb-catalog-amphenol-industrial
Amphenol® Pre-Earth/First Mate Last Break Connectors are designed for applications where a protective circuit from the ground contact to the shell is critical. These connectors provide a path for any stray voltage to be shunted to a safe ground avoiding harm to the operator and the voltage sensitive equipment.
FOR ONE UNIT - Amphenol CS
on solder tail area. 1.27um [50μ"] min. nickel underplating overall. 2.2 shell: 1.27um [50μ"] min. nickel underplating overall. 3. recommended p.c.b thickness : 1.6mm 4. other general spec. to refer : rjf series spec. 5. for reflow soldering lead-free process for one unit led 2 led 1 rj45 pin 1 rj45 pin 8 ww=week yy=year date code amphenol ...
MILITARY POWER CONNECTORS 55181 - Amphenol PCD
Plug, Cable, 18 contacts, Pins, 7.5 AMPS, Size 20 contacts, Solder cup 5935011119956
Gold Embrittlement in Solder Joints - SV Microwave
SV Microwave has developed a proprietary, highly automated and highly repeatable process in-house that can strip the gold from the solder joint.
Aquacon Hermetic Connectors | Aquacon Connectors | MIL-DTL-38999 ...
A resistance soldering unit of approximately 125 watts is recommended. If a soldering iron is used, do not exceed 20 watts for size 22M, 22D and 22 contacts; 80 watts for size 20: and 150 watts for size 16 and 12 contacts. Wipe or brush excess flux from terminations.
Reflow Stable PCB Connectors - SV Microwave
common problem for design engineers is how to avoid the deformation of Printed Circuit Board (PCB) connectors during reflow. Reflow is the process whereby PCBs are placed in an oven and heated beyond the melting temperature of the solder used to fix the connector onto the board.
PCB Connector Basics - SV Microwave
SV ofers many solutions to the typical challenges of RF PCB design. Solder. Precision soldering may require extensive skill and expensive tooling to achieve desired results. Consider these options: 30° Solderless Compression Mount Connectors achieve edge launch performance anywhere on the board.
Ultratane Butane Fuel 15/16 oz Canister - Gemeco
Ultratane Butane Fuel by Master Appliance®. Size 15/16 oz. Butane Fuel Refills for use with all Master butane powered micro torches and soldering irons.
Amphenol Aerospace
2. Tin center conductor, and using a 47.5 watt soldering iron, solder the center conductor into the inner socket contact wire well. A pin vise can be used to hold the inner socket contact. F 1. Slide front insulator, large end first, over the inner socket contact until insulator seats against the inner socket contact shoulder. G 1.
Understanding Press-Fit Technology - Positronic Connectors
Press-fit technology is an alternative to the soldering method and is characterized by the connector’s contacts being collectively pressed into the PCB’s plated through holes. The press-fit pin has flexible beams, and the corresponding PCB serves as a rigid “socket” to ensure a perfect fit.
IDC vs Crimp Termination: A Guide to Choosing the Best - Amphenol CS
IDC termination helps in saving a lot of time and effort, as a large number of wires can be terminated at once without the help of any additional tool or individual soldering. The termination can be done with a simple hand press and these are also cost-effective.
Modular Jack Connectors and Their Applications - Amphenol CS
Amphenol’s new high temperature LED solution solves this problem using a unique design approach, ensuring the LEDs can withstand the thermal shock from the high temperatures of the reflow soldering process, greatly reducing failures, and improving durability, robustness, and overall applied cost.