Search Results for stechkin revolver
Installation Instruction 2800118-C - rfstechnologies.com
Keep the gun always moving to avoid overheating the sleeve or the cable - max. temperature 70°C (158°F) shrinking temperature is around 130°C (266°F). Continue shrinking until the sleeve lies flat all around and the hot solvent discharged (is visible) on both sides. Make sure that the connector will stay in place all the time.
Model 117B12 CONFORMAL BALLISTICS PRESSURE SENSOR Installation and ...
installed in the gun chamber, conforms or blends in precisely with the inside surface of the chamber actually forming a portion of the wall adjacent to the cartridge case. When the round is fired, the pressure builds up rapidly inside the case, obturating the case outward against the chamber. The force, transmitted through the thin