Search Results for substance use
Model 138A51 Tourmaline ICP® underwater blast sensor, 4.2 length ... - PCB
O: Indicates that said hazardous substance contained in all of the homogeneous materials for this part is below the limit requirement of GB/T 26572. X: Indicates that said hazardous substance contained in at least one of the homogeneous materials for this part is above the limit requirement of GB/T 26572.
Static Preloading of 1-DoF & 3-DoF Force Ring Sensors
described herein is based on use of the sensor’s resultant output as a measureand of the applied preload. This methodology produces the most accurate results and duplicates the process followed by PCB® during sensor calibration. There are numerous benefits of applying a static preload on piezoelectric force rings. The primary reasons include ...
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
The Council of 8 June 2011 on the restriction of the use of certain hazardous substances in the electrical and ... Since equipment consists of different components, the EEE itself can only meet the substance requirements if all its components and parts meet the substance restriction requirements of RoHS 2, including non-electronic or non ...
SMPM Female VITA 67.1/67.2 to SMA Male 12" Cable ... - SV Microwave
These products comply with the substance restrictions of the Restriction on Hazardous Substances Directive 2011/65/EU (RoHS2). The RoHS2 Directive requires that certain electrical and electronic equipment products do not contain mercury, cadmium, hexavalent chromium, PBB, PBDE, lead, DEHP, BBP, DBP and DIBP above defined thresholds.
SMPM Female to SMPS Female VITA 67.3 Backplane Adapter
These products comply with the substance restrictions of the Restriction on Hazardous Substances Directive 2011/65/EU (RoHS2). The RoHS2 Directive requires that certain electrical and electronic equipment products do not contain mercury, cadmium, hexavalent chromium, PBB, PBDE, lead, DEHP, BBP, DBP and DIBP above defined thresholds. ...
Assembly Instructions - Document Library - Amphenol RF
Back; N-Type Adapters; N-Type to 1.0-2.3 Adapters; N-Type to 2.2-5 Adapters; N-Type to 4.1-9.5 Adapters; N-Type to 4.3-10 Adapters; N-Type to 7-16 Adapters
16617 MIL-DTL-26482, Series 2, Matrix - Amphenol Aerospace
26482 4 Contact Amphenol Aerospace for more information at 800-678-0141 • www.amphenol-aerospace.com MATRI 2 J Insert Arrangements Insert Arrangement 8-33 8-98 10-06 12-03 12-08 12-10 14-04 14-05 Service Rating I I I II I I I II Number of Contacts 3 3 6 3 8 10 4 5
LUMINUS - amphenolpcd.com
Isopropyl Alcohol & Mineral Spirit Solution Skydrol Hydraulic Fluid: Hydraulic Fluids per MIL-PRF-83282 MIL-PRF-87257: Ethylene Glycol Propylene Glycol: Aviation Jet A: Flammability: UL94, V0. DOTG section 26.6.2 & 26.6.3: FAR Part 25 App F Part I: Contact Insertion & Removal Force (not to exceed) size 22 10 lbs:
Careers - XMA
Be Responsible: I take ownership and meet commitments I make. Corporate Commitment: I choose excellence and am committed to exceeding the expectations of internal and external customers. Professionalism: I respectfully and openly discuss issues in an effort to get the best possible solutions. Reach Higher: I recognize that results are driven by my individual commitment to continuously improve ...
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
The Council of 8 June 2011 on the restriction of the use of certain hazardous substances in the electrical and ... Since equipment consists of different components, the EEE itself can only meet the substance requirements if all its components and parts meet the substance restriction requirements of RoHS 2, including non-electronic or non ...
ASVG | Amphenol Global Search | Amphenol
Circular Connectors. Our Circular Connector portfolio begins with our Mil-spec qualified connectors, which includes MIL-DTL-D38999 Series I, II, and III; MIL-DTL-26482 Series II; MIL-DTL-83723; MIL-DTL-5015; and MIL-DTL-22992 Class L connectors.There are many custom and derivative connectors based on these military specifications, including EMI filter connectors, hermetic connectors, lanyard ...
42125200 | Amphenol Global Search | Amphenol
Search Results for 42125200. Radially sealed flat connector housings with secondary lock. The plug housings for 1.2-mm, 1.5-mm, 2.8-mm, 4.8-mm and 9.5-mm flat connectors are used for electrical connections between the harness and the various components in the car. ngs are available for 1- to 14-pin connectors.
Model 080B160 0.55/14mm Triax cube adhesive mounting clip Installation ...
O: Indicates that said hazardous substance contained in all of the homogeneous materials for this part is below the limit requirement of GB/T 26572. X: Indicates that said hazardous substance contained in at least one of the homogeneous materials for this part is above the limit requirement of GB/T 26572.
Liquid Level Transmitters | MTS Sensors - Temposonics
But what are the liquid level transmitters doing when they are installed in a tank? And how do you decide which sensor is the right one? To answer the first question: the magnetostrictive liquid level transmitters deliver the most exact product level, interface level, and temperature measurement of a tank from one process opening.
SS510 EchoRange™ 200kHz Portable Survey, DT - 20m Cable - Airmar
Internal transformer provides impedance match to echosounder and allows use of longer cable 500 W RMS, power rating is at 2% duty cycle Robust, stainless-steel housing
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
The Council of 8 June 2011 on the restriction of the use of certain hazardous substances in the electrical and ... Since equipment consists of different components, the EEE itself can only meet the substance requirements if all its components and parts meet the substance restriction requirements of RoHS 2, including non-electronic or non ...
Amphenol AMAO Product Compliance - Environmental Engineering
different components, the EEE itself can only meet the substance requirements if all its components and parts meet the substance restriction requirements of RoHS 2, including non-electronic or non-electric components like fasteners or the plastic case of a desktop computer. Therefore components being used in finished EEE or for
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
The Council of 8 June 2011 on the restriction of the use of certain hazardous substances in the electrical and ... Since equipment consists of different components, the EEE itself can only meet the substance requirements if all its components and parts meet the substance restriction requirements of RoHS 2, including non-electronic or non ...
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
The Council of 8 June 2011 on the restriction of the use of certain hazardous substances in the electrical and ... Since equipment consists of different components, the EEE itself can only meet the substance requirements if all its components and parts meet the substance restriction requirements of RoHS 2, including non-electronic or non ...
NovaSensor NPC-100 and NPC-120 Disposable Medical ... - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.