Search Results for swedish primary care - bellevue
Board-to-Board - SV Microwave
The primary goal of any B2B RF connection is to transfer the signal between PCBs while sacrificing as little RF power as possible. This translates to the best VSWR/Return Loss and Insertion Loss possible. Radial Misalignment and Axial Misalignment are two key conditions that must be kept within tolerance in
Medical Applications - Amphenol Alden
Whether it’s creating custom assemblies and connectors for complex surgical tools or developing high-density connectors for advanced imaging systems, Amphenol Alden is dedicated to supporting the medical industry with the same exceptional care and support that they show patients.
Operation Manual T-Series Analog - Temposonics
operated with utmost care. 1.The sensor systems of all Temposonics ® series are intended exclusively for measurement tasks encountered in industrial, commercial and laboratory applications. The sensors are consid-ered as system accessories and must be connected to suitable evaluation electronics, e.g. a PLC, IPC, indicator or other electron-
Operation Manual Level Plus CHAMBERED - Temposonics
Level Plus ® CHAMBERED Operation Manual I 3 I 1. Contact information United States General Tel: +1-919-677-0100 Fax: +1-919-677-2343 E-mail: info.us@temposonics.com
Get Return Authorization RMA - KAYE
KAYE HEADQUARTERS. Amphenol Advanced Sensors Germany GmbH Sinsheimer Strasse 6 D-75179 Pforzheim. T +49 (0) 7231-14 335 0 F +49 (0) 7231-14335 29 kaye-ccpf@amphenol-sensors.com
Model 208C02 ICP® Force Sensor Installation and Operating Manual - PCB
ICP FORCE SENSOR OPERATION MANUAL 1 1.0 INTRODUCTION . ICP force sensors incorporate a built-in MOSFET microelectronic amplifier. This serves to convert the high impedance charge output into a low impedance voltage signal
Signal Conditioning Basics | PCB Piezotronics
In addition to ease-of-use and simplicity of operation, ICP ® sensors offer many advantages over traditional charge output sensors, including: 1.) Fixed voltage sensitivity independent of cable length or capacitance. 2.) Low output impedance (<100 Ohms) allows signals to transmitted over long cables through harsh environments with virtually no loss in signal quality.
CiAC A239AXXX Sealed T1 Mini-Repeater - Charles Industries
The T1 Mini-Repeater is installed into the T1 span within 4 feet of a primary over-voltage protector. Secondary surge protection is provided for side 1 and 2 inputs and outputs. This protection is capable of eliminating line surges and spikes experienced during normal operation of the T1 span. If the T1 span is in an unprotected area
Troubleshooting accelerometer installations - Wilcoxon Sensing Technologies
Troubleshooting accelerometer installations Accelerometer based monitoring systems can be tested to verify proper installation and operation. Testing
ASTG Electrification EV/HEV Applications - amphenolsensors.com
ASTG Electrification EV/HEV Applications - amphenolsensors.com
Spade Terminals | TPC Wire & Cable
Hoff-Trex ® S pade Terminals are indispensable electrical terminals designed to simplify the connection of wires and cables in various industrial applications. These highly versatile terminals are a must-have for electricians and other professionals in industries ranging from automotive and electronics to industrial manufacturing. Ranging from small 26 AWG to 10 AWG sizes and offering stan ...
AE-AN-SK-006 - SK SERIES - CARE AND MAINTENANCE - Amphenol Ardent Concepts
AE-AN-SK-006 - REV B - SK SERIES - CARE AND MAINTENANCE • Avoiding the Contacts - It is important to avoid touching the contacts with bare skin as the contacts can be bent or oils from the skin can be transferred onto the contacts. If the contacts are touched, the suggested procedure is cleaning with a small brush and isopropyl alcohol.
Model 337A30 ICP® Accelerometer Installation and Operating Manual - PCB
DOCUMENT NUMBER: 21354 DOCUMENT REVISION: D ECN: 46162 Component Name Hazardous Substances Lead (Pb) Mercury (Hg) Cadmium (Cd) Chromium VI Compounds
Cellular Low Profile Vertical Antenna - PCTEL
The BMLPVMB/LTE low-profile vertical antenna provides superior multiband pattern coverage for mobile or fixed applications operating in frequencies from 600 MHz to 2700 MHz. This antenna is designe...
Computer System Validation - KAYE
Computer System Validation - KAYE
731A seismic accelerometer and P31 power unit/amplifier Operating guide
the user should take care not to overload the system at the natural frequency. 3.0 Operation 3.1 Inspection After carefully unpacking the 731A seismic accelerometer, the P31 power unit/amplifier, and cables, inspect the external parts for damage to switches, indicator and connectors. If there is
Model 027137-04022 PCB L&T Hand Torque Wrench, 200 in-lb (22.7 Nm), 12 ...
the primary sensing element. The four-arm Wheatstone Bridge configuration is shown below in Figure 1 . Also pictured in Figure 1 is the wiring code for the standard 10-pin PT receptacle. Figure 1–Hand Torque Wrench Wheatstone Bridge With Angle Wiring Code The gages are bonded to the wrench’s flexure. Typically, a
Ant™ Combination Antenna - PCTEL
Dear Customer, Thanks for your interest on the 72488-1 and 72488-L1. Both products have reached end of life (EOL). Click on the link below for the replacement options Replacement Part: 710737 Conta...
connor
sionate working environment that is the primary catalyst for our highly creative solutions. This has in turn, led to long-lasting, reciprocal relationships ... We care about our customers’ needs and operate globally to provide products and services effectively and efficiently. precision CUSTOMER BUSINESS MANAGEMENT
Model M119B12/PCS-8 Charge Output Pressure Sensor Installation and ...
frontal area. Extra care should be exercised to avoid bottoming in the mounting hole when recess mounted or when mounting into existing ports. Install the sensor, using only one of the seals provided, with the aid of a torque wrench to monitor the mounting torque value. The recommended torque range can be found on the installation drawing.