Search Results for tci 613 antenna grounding rings installation manual pdf
ATEX Product Manual - AMPHENOL PROCOM
potential than the system, it’s then necessary to install the grounding wire (to be bought separately) to ensure equipotential bonding in accordance with EN 60079-14:2014. See section 4.1 for instructions on how to install the ATEX grounding kit on the LW-SS mounting bracket.
696-960 MHz - Amphenol Antenna Solutions
Important Installation Instructions In order to operate RET control, the transparent caps covering the tilt adjustment indicators must be engaged and locked. Do not cut them from the antenna.
Catalogs, Brochures & User Manuals - Amphenol Antenna Solutions
Resources Resources Brochures & Catalogs Small Cell Antennas Quick Reference Guide Venues & Private Networks Antenna Selection Guide In-Building Antenna Solutions 2024 Base Station Antennas EMEA Catalog
6878308G - amphenol-antennas.com
• Tri band antenna, dual polarisation, 6 connectors • Independent, continuously adjustable tilt on each band 2-12° / 2-12° / 2-12° • RET version, 3GPP/AISG2.0 with four integrated RCUs
Base Station Antenna Components ATEX Grounding Kit - AMPHENOL PROCOM
Universal ATEX grounding kit for LW-SS, LW-SS-1” and C mounting bracket. The ATEX grounding kit is to be used to ensure equipotential bonding if the point of installation has a different electrical potential than the system. Can only be used with Procom ATEX antennas.
Installation instructions - Amphenol Antenna Solutions
WPS Boot Guide AFJ89-3, for WPS Boot installation after cable jumper assembly. NOTE: The technical specification contains proprietary information and such information may not be disclosed to others for any particular purpose or used for manufacturing purposes without written permission from Amphenol Fuyang. VER HISTORY
Fiber Splice ox (FS A) Installation Instructions
All grounding should follow local codes and practices. Grounding components are available for grounding the box and/or non-dielectric cable(s). Refer to the Ordering Guide section of the product datasheet for details. If this accessory was selected, a Ground Feed-thru (GFT) will be supplied with the kit. 1.
6-Port Antenna
Please read all installation notes before installing this product. Always attach the antenna by all mounting points. Do not install the antenna with the connectors facing upwards. Do not cut the tethered transparent caps(s) that cover the antenna's tilt adjustment indicators.
Ground Plane Antennas GP 27 - AMPHENOL PROCOM
GP 27 is a glass fibre ground-plane antenna of the triple-leg type. The antenna is delivered factory-tuned to 27 MHz – further adjustment is not necessary for this band. Tunable (by cutting) to frequencies within the range: 27…45 MHz.
DISCONTINUED - Amphenol Antenna Solutions
Important Installation Instructions In order to operate RET control, the transparent caps covering the tilt adjustment indicators must be engaged and locked. Do not cut them from the antenna.
BA6312-6 - amphenol-antennas.com
INSTALLATION Please read all installation notes before installing product. Always attach the antenna using all mounting points. Do not install antenna with the connectors facing upwards.
696-900 / 696-900 MHz - Amphenol Antenna Solutions
Important Installation Instructions In order to operate RET control, the transparent caps covering the tilt adjustment indicators must be engaged and locked. Do not cut them from the antenna.
SCU Installation Guide - amphenol-antennas.com
The SCU provides a web interface for performing antenna tilt adjustment, TMA mode adjustment and device monitoring from remote locations. The SCU also permits local control using the LAN port of a laptop computer.
BA6312-0 - Amphenol Antenna Solutions
INSTALLATION Please read all installation notes before installing product. Always attach the antenna using all mounting points. Do not install antenna with the connectors facing upwards.
INSTALLATION INSTRUCTIONS - amphenol-antennas.com
INSTALLATION OF THE N275F OMNIDIRECTIONAL ANTENNA MOUNTING HARDWARE The BA1012, BA1312, BA6012 and BA6312 antennas can be mounted on the top of mast Ø33-40 mm (1.3-1.6 inches) with the feeder cable inside or on a mast 25-58mm (1.0-2.3 inches) with the cable on the outside. The U-shaped stainless steel mounting brackets are included in the N275F
RETU-Ex01 Installation Guide - Amphenol Antenna Solutions
These instructions describe how to fit a RETU-Ex01 (RET) to an Amphenol Antenna Solutions SmartTilt antenna with remote adjustable electrical tilt. Typically, the RET unit is installed at the factory and further install work or adjustment isn’t necessary.
GroundingKit - Amphenol Antenna Solutions
Supporting your needs with innovative and tailored antenna solutions for optimal coverage and capacity.
6-Port Antenna
actuators are available with this particular antenna. A single actuator individually controls the tilt of each band (no need for daisy chain cables between the bands).
Grounding-Kits - Amphenol Antenna Solutions
Grounding-Kits - Amphenol Antenna Solutions
BA6110-1 - Amphenol Antenna Solutions
BA6110 “Heavy Duty” is permanently affixed to a unique mounting fixture which allows mounting on top of or along-side most vertical supports. Due to their wide bandwidth, they are ideal for use as emergency backup antennas. Their size and mounting fixtures allow for easy storage and fast installation.