Search Results for tend kingsland
Recent Design Updates and Selection Considerations - PCB
not be affected, but the low frequency noise will tend to increase. And some charge measuring equipment will not tolerate low input resistance and will clip the output signal. Ordinarily the leakage resistance of a sensor is understood and the appropriate signal conditioning is used, thus there will be no noticeable effects.
4-20 mA vs. IEPE vibration sensors for control systems
The majority of faults on rotating machines are in the mid-frequency range and appear as rising vibration levels over time. Imbalance, misalignment, and looseness – some of the most common causes of machine failure – tend to have fault frequencies between 30-60,000 CPM and can generally be detected with this method.
TECHNICAL NOTE TN-15 - PCB
Solenoid valves are generally not well-suited, as they tend to produce an oscillating pressure source during the switching process. In pneumatically operated calibrators, the use of helium will provide the fastest rise time. Hydraulic Impulse Calibrator This versatile aperiodic calibrator is structured with a free-falling
Q&A - Public Safety Uplink Radio Performance - PCTEL
A) To ensure the correct power level and good quality for active channels, measure the noise contribution to the site, etc. Because uplink signals tend to be lower power, objective uplink signal quality measurements can be particularly useful for verifying network quality and reliability.
SSI Technologies - Application Note FT-AN6
senders. They tend to get stuck in the frozen urea and may brek the float anda or give in/ ccurate reada ngs. i FluidTrac has an operating temperature of -40°C to +85°C and is not affected when urea freezes since it does not protrude into the liquid. In temperatures greater than60°C, ammonia is released from urea.
Tech note – measurement locations - wilcoxon.com
8435 Progress rive Frederick, M 2101 Tel: +1 (301) 330 8811 info@wilcoxon.com wilcoxon.com buy.wilcoxon.com Wilcoxon Sensing Technologies Tech note – measurement locations
Tech note - measurement locations - Wilcoxon Sensing Technologies
the ability to mount one permanent sensor, then the user should tend toward mounting that one sensor in a location most likely to indicate the most probable failure mode of the pump. Wilcoxon Sensing Technologies 20511 Seneca Meadows Parkway Germantown, MD USA Tel: +1 (301) 330 8811 info@wilcoxon.com www.wilcoxon.com
Seismic Monitoring of a Retaining Wall in Reinforced Concrete Piles - PCB
In both cases, however, people tend to develop completely automated damage identification methods to take full advantage of the recent progress in communicationtechnology (Aktan et al. 2005). In this context, it is very important to identify the modal parameters of the structures under operative
RADSOK® | High Power 38999 | Products | Amphenol Aerospace
RADSOK® technology is based upon a stamped and formed flat grid, uniquely twisted into a hyperbolic geometry to provide robust, high-density contact to the mating pin contact.Most pin and socket technologies rely upon spring (beam element) properties of the contact elements, which tend to weaken over time. Unlike most other pin and socket solutions, the RADSOK® also utilizes the tensile ...
Understanding Torque-angle Signatures of Bolted Joints - PCB
PCB LOAD & TORQUE, INC. 24350 Indoplex Circle, Farmington Hills, MI 48335 USA Phone: 866-684-7107 Fax: 716-684-0987 Email: ltinfo@pcbloadtorque.com www.pcbloadtorque.com