Search Results for the never built dutch schelde – gunning submarine
U.S. Army air defense laser prototype successfully downs targets
Developmental testing of the system is expected to continue throughout the next quarter. The DE-M-SHORAD features a 50-kilowatt laser weapon developed by Raytheon mounted on a Stryker armored vehicle. Raytheon received a $123 million Army contract in 2021 to develop the laser weapon.
Defense | Markets - Amphenol
Amphenol is a world leader in the design, manufacture and supply of high-performance interconnect systems for harsh environment defense applications including vibration, pressure, humidity, nuclear radiation and severe temperature changes.
Marine Antennas - AMPHENOL PROCOM
Amphenol Procom is the leading developer and manufacturer of RF solutions within the Maritime sector, which will contribute to successful onshore and offshore operations.
Amphenol RF Military & Defense Solutions Overview
Amphenol RF’s broad interconnect portfolio includes a wide variety of ruggedized and high-frequency products that deliver mission-critical solutions for military and defense applications.
A connector that can really plug in - Lutze Inc.
With the new DT06-2 suppressors for valves, LÜTZE, the Weinstadt-based automation specialist offers a new connector system specially designed for robust outdoor use. Typical uses include construction machines, commercial vehicles and agricultural and forestry machinery.
Solaris - Amphenol PCDAmphenol PCD
STAY CONNECTED. Sign up to receive the latest news from Amphenol PCD
CTA - temposonics.com
Find out how we at Temposonics implement sustainability in our daily work and what we do to make our world a better place. We are strongly committed to supporting programs and initiatives that contribute to a cleaner, safer and more sustainable world. LEARN MORE.
CXL 2-1LW/... - AMPHENOL PROCOM
This multi-purpose, omnidirectional, 0 dBd, rod-type base station and marine antenna covers the 160 MHz band in three models with 10 MHz overlap and can be used in a wide variety of applications.
Marine Antennas FLG - AMPHENOL PROCOM
Using this flange all antennas specifically designed for mounting on 1” threaded water pipe can be mounted on deck, wheelhouse roof, cabin roof or any other horizontal or near-horizontal surface. Inside the marine sector the 1” water pipe mounting system for antennas has gained worldwide acceptance.
123GB-0841 Issue1 (2) - amphenol.co.uk
%) :, (1* ,03257$17 ,vvxh &khfn wkh ,qwudqhw wr hqvxuh \rx duh xvlqj wkh odwhvw lvvxh ri wklv )rup $pskhqro 1xpehu *% ,vvxh 3ulqw whvw er[
Series 3 - amphenol-in.com
Amphenol Tri-Start connectors provide EMI/EMP shielding capability which conform to MIL-DTL-38999 Series III requirements. metal to metal coupling, EMI grounding fingers and conductive finishes has proven to be the ultimate in EMI/EMP shielding effectiveness.
The B-21 stealth bomber kickstarts sixth-generation military aerospace
Developed to deliver conventional and nuclear weapons while remaining nearly invisible to radar, the B-21 Raider is slated to serve as the backbone of the Air Force’s bomber fleet once its development is finished this decade.
安费诺(常州)电子有限公司
o mm m z o o this drawing supplied for information only. design features, specifications and performance data shown hereon are the property of the
ProFin Plus Antenna for Mission Critical Radio Networks - AMPHENOL PROCOM
Multi- Band – coverage for L-Band, BAS, S-Band, GPS, GNSS Lower and Upper C Band all supported by 2x2 MIMO. ProFin Plus is truly a state-of-the-art device for vehicles connected to Public Safety or Mission Critical Networks. If you want to learn more, click on the following link: ProFin and ProFin Plus. Do you want to keep up with our work?
TRO1-VU0 - amphenol-antennas.com
TRO1-VU0 Quoted performance parameters are provided to offer typical, peak or range values only and may vary as a result of normal testing, manufacturing and operational conditions.
US Navy awards contracts for more Arleigh Burke-class destroyers
The U.S. Navy recently awarded shipbuilders Huntington Ingalls Industries and General Dynamics Bath Iron Works contracts to build several Arleigh Burke-class guided-missile destroyers. Bath Iron Works' contract is for the design and construction of three ships, while Huntington Ingalls’ contract is for six ships.
TWIN458CU000x - Amphenol Antenna Solutions
Can be ordered with a Multi-Device Dual Unit (MDDU) with two separate inputs for independent control of each band. Ideal for antenna sharing.
Amphenol Adronics
1. Aceptación: Esta Orden de Compra debe ser aceptada por escrito por el Vendedor.Si por alguna razón el Vendedor no aceptara este pedido por escrito, el envío de los bienes solicitados por el presente, la prestación de cualquier servicio solicitado en virtud del presente o la aceptación de cualquier pago por parte del Vendedor en virtud del presente o cualquier otra conducta del Vendedor ...
NJFVAF-0002 | DSFP 56G Straight Cable Assembly | Amphenol
DSFP - 2x SFP Cable Assembly, Passive, 30AWG, 2m, 56G / Lane, Jacket
Ground Plane Antennas 438.02.05.00 - AMPHENOL PROCOM
The 438 Series are heavy duty omni antennas consisting a broadband quarter wave radiator and four radial ground planes of an extremely rugged and reliable construction. The quarter wave radiator incorporates a d.c. short to minimise static interference.