Search Results for transfer of technology
High Bandwidth Connectors for New Technologies - Amphenol CS
The tolerances for the connectors and breakout regions are limited by the PCB process technology, but there are factors that need to be addressed in the design. This can range from feature alignment, signal pad connector wipe and tolerance regions, back drill stub depth, and board perimeter routing tolerances.
Quality System Certifications | PCB Piezotronics
These and similar standards increase the reliability and effectiveness of the goods and services we use. Users typically have more confidence in products and services that conform to international standards. The aim is to facilitate trade, exchange and technology transfer through: enhanced product quality and reliability at a reasonable price,
LUTZE Inc. - Lutze Inc.
Railway technology is another important industry for LUTZE as one of the leading suppliers worldwide. LÜTZE Transportation was among the first companies in the world to comply with the demanding IRIS Standard in 2007. Since then the quality management system has been continuously developed in parallel with the IRIS Standard and fulfills the ...
5G Connectors - Positronic The Science of Certainty
Delivering Power for 5G Connectivity. The introduction of 5G technology in 2019 brought with it the next leap in performance for mobile telecommunications. Smartphone manufacturers were quick to capitalize on this new network to launch handsets that offer the promise of faster-than-ever internet access and the most advanced functionality.
Battery Connectors | Custom Battery - Amphenol
The future of technology is heading towards energy-efficient and environmentally friendly battery-powered solutions. E-bikes, electric forklifts, and Energy Storage Systems are some examples of this shift. At Amphenol, we understand the crucial role that connectors play in ensuring efficient power transfer and reliable performance.
USB 4 Gen 3 Type C | Input Output Connectors | Amphenol
USB 4 connectors by Amphenol are compatible with Thunderbolt 4, combine power charging, PCIe ® , data transfer, and DP video/audio in a single Type C connector. Toggle Nav. Search. Search. Advanced Search . Search ... factory automation equipment and automotive infotainment applications and Amphenol is one the earliest adopters of this technology.
Press-Fit Connectors - Positronic The Science of Certainty
Press-fit technology allows manufacturers to avoid soldering when assembling PCB electronics. The press-fit connection is formed when a pin is pressed into a fitted, plated-through hole in a PCB. ... and shaky environments won’t transfer to the PCBs or backplanes). Plus, some bi-spring power press-fit connectors eliminate the need for costly ...
Technology - Amphenol Invotec
Data Transfer; Data Guidelines; Printed Electronics; Technology Data Guidelines. Drill Information. Accepted Formats: Excellon File (Format 1 or 2) Gerber; Sieb and Meyer; The files supplied should contain X Y co-ordinates of all the relevant tools separately defined. If tools of equal size exist in the program (i.e. 2.00mm (.079") plated, 2 ...
Connectors | Products - Amphenol
USB 4 connectors compatible with Thunderbolt 4 interface combines power charging, tunneling USB, PCIe® data transfer, and DP video and audio capability in a single Type C connector. ... The small form factor made this interconnection a unquestioned technology across devices. The reversible design enables quick and easy connections, no matter ...
AUTONOMOUS MOBILE ROBOTS (AMR) APPLICATIONS - Amphenol RF
• Load Transfer • Pallet Truck • Assembly Line • Light Load Transporters • Heavy Load Transporters • Pickers ... emerging autonomous warehouse technology. The rise in autonomy within the warehouse logistics ecosystem enables increased efficiency, reduced cost and helps to ensure safety. Autonomous
Staying in time - Data acquisition and transmission with ... - Temposonics
In the idle state, when no data is transmitted, the data line and the clock line are at the high level (1).; The current position data is frozen in the shift register with the first falling clock edge. It is no longer possible to update the position data in this cycle (2).; The bit is applied at the following rising edge (3).
Next Generation Infotainment for Smart Vehicles - Amphenol CS
The components make it possible to evolve the technology beyond the simple information-and-entertainment-hub concept to becoming a crucial part of the vehicle architecture. ... with USB 3.1 Gen 2 variant delivering twice the data transfer rate of SuperSpeed USB, with an added advantage of highly improved power efficiency. We also have Micro USB ...
SATA Connectors | Amphenol
It is an advanced version of Parallel Advanced Technology Attachment or PATA. The SATA connectors and cables are capable of transmitting data much, much faster than PATA. With data transfer speeds from 1.5Gb/s to 12Gb/s, these also support major storage innovations like Shingled Magnetic Recording (SMR), DEVSLP, and other advanced power ...
Amphenol DC Electronics Expands to Mexico - DC Electronics
Amphenol DC Electronics Adds New Injection Molding Technology January 27, 2014 San Jose, Calif., December 23, 2013 – Amphenol DC Electronics (ADCE), a division of Amphenol Industrial Global Operations Group (NYSE: APH) today announced the opening of a new, state of the art manufacturing facility in Nogales, Mexico.
Ethernet | Products | Amphenol Aerospace
CTF-10G-1 is an integrated hybrid connector and media converter that couples high speed copper technology with M29504 fiber technology. Now you can transfer high speed data seamlessly from copper to fiber and fiber to copper.
Future of Datacenter with Ethernet SSDs - Amphenol CS
These days as speed and performance requirements are advancing SSDs are now taking the center stage of mass storage media. This is where the most advanced storage technology, Ethernet SSD takes its position. As the name suggests, these are storage drives that can transfer massive data in seconds via Ethernet but not confined to it.
Connectors | Products - Amphenol
SuperSpeed USB will deliver 10x the data transfer rate of Hi-Speed USB, as well as improved power efficiency. With 5Gb/s signally rate, SuperSpeed USB 3.1 has a Sync-N-Go technology that minimizes user wait time. No device polling and lower active and idle power requirements are other significant features of these connectors.
Immersion Cooling - Positronic
A sealed enclosure protects the components, allowing the heat to transfer to the liquid surrounding the component. Two-Phase. In two-phase cooling, the equipment is submerged into a bath of dielectric heat transfer liquid, which has a low boiling point of about 50°C. The heat from the components produces a vapor that rises from the liquid.
OverPass Cable System - Amphenol CS
The OverPassTM cable system allows for the transfer of high-speed signals to twinax cables shortly after they are launched from the ASIC. Delivering a simple, low-loss, direct link to ... frequency SkewClear EXD cable technology and manufacturing expertise. • Offerings include multi-pair cables: 2, 4 and 8 pair constructions in wire gages ...
Blog | Industry Insights | Amphenol NEXUS Technologies
Mil-Spec connectors are paired male and female components that transfer signals […] The Importance of Mil-Spec Connectors 1:52 pm Leave a Comment. ... Even with the continued rise of wireless technology, many high-quality headsets, microphones, and other audio equipment still rely on wired connections to boost sound quality and functionality. ...