Search Results for ui ux designer
Medical Interconnect Solutions | Amphenol Alden
These reliable connectors ensure robust performance in a space-saving design — perfect for complex medical equipment. Learn more High Voltage Connectors. We craft our high voltage connectors to deliver exceptional performance in demanding medical environments. With robust designs that ensure safety and reliability, these connectors provide ...
2013-08 Staff of The Month - Amphenol-ast
From:Amphenol Author:Admin Clicks:19432 times PubDate:2013/8/28 Staff of The Month in August,2013,from Production.
ProFinPlus - About Amphenol Procom
design of the LTE element, ensuring the best correlation coefficients to enhance data speeds in market. Low band and high band Wi-Fi both 2x2 MIMO. Precision Geo-location is provided with GNSS and GPS. The ProFinPlus is future proofed in the glob-al market as 5G networks roll out. With 2x2 MIMO offered for 5G, up to 3.8 GHz, and 5G
Product Finder - Lutze Inc.
LUTZE Inc. 13330 South Ridge Drive • Charlotte, North Carolina 28273 • USA Phone: 704-504-0222 • Fax: 704-504-0223 • E-Mail: info (at) lutze.com
Mini-D RF Connection System - SV Microwave
Rev. 3 (12/22) O: 561.840.1800 marketing@svmicrowave.com Mini-D RF Standard Part Numbers Mini-D RF Male PCB Edge Launch Connector, 8 Port P/N: 9311-60112
Brainstorming with innovative experts - Amphenol
Our R&D and engineering teams have diverse and international bases of knowledge, spanning the entire industry. Amphenol Tel-Ad has particular, state-of-the-art expertise in design and production of control panels and other electrical enclosures, offering simple and smart solutions. We provide added value every step of the way to designing a winning product.
EU-TYPE EXAMINATION CERTIFICATE - Amphenol Fiber Systems International ...
11 This EU-Type Examination Certificate relates only to the design and construction of the specified equipment. If applicable, further requirements of this Directive apply to the manufacture and supply of this equipment. 12 The marking of the equipment shall include the following: II 2 GD Ex db IIC T* Gb * This is a list of marking options that ...
2021/7/30-31 IATF16949:2016&ISO9001:2015 Internal auditor training
2021/7/30-31, due to the annual internal audit activities will be launched, considering the expansion of the internal auditor team, we need more new internal auditors to participate in the annual internal audit activities.
USB Connectors | Products | Amphenol
Micro USB 2.0 connectors have power contacts of 1.8A and 3A current for fast charging. The plastic tongue and two-layer shells design ensure high reliability and prevent connector damage. Amphenol offers customized designs to suit various customer requirements. These connectors also offer high-speed signal stability of up to 480Mb/s transmission.
INIR2-R32 Refrigerant R32 (Leakage Detection Sensor ... - Amphenol Sensors
Rugged design for maximum protection and direct immersion in liquids or gases Gas Detection Sensors. Detects the presence of Hydrocarbon gases that indicate fuel leakage. 0 to 10,000 ppm; Linearized digital output; Mechanically robust; Monitoring Air Quality: Detectable gases: VOCs, CO 2, ozone, NO 2, NH 3;
Michelle Marin, Wilcoxon Sensing Technologies recognized as a 2022 ...
Wilcoxon Sensing Technologies congratulations transducer design engineer Michelle Marin for being recognized as a Champion of Maryland Manufacturing for outstanding contributions from Women in Manufacturing by the Regional Manufacturing Institute of Maryland. Michelle began working at Wilcoxon in 1997, shortly after immigrating to the US from Romania with a degree in Mechanical Design ...
CLASSIFICATION UNRESTRICTED - Amphenol CS
The HPCE connector design has not included a guide system therefore the design is not for a blind mate application. The mis-alignment allowance of the HPCE product is depended on the condition of the connector system and the chamfer of the edge card. Please see figure 5 and table 4 for explanation. Figure 5 X Y X Y 0.50 1.85 ± 0.125 1.00 2.35 ...
2014-1 Staff of The Month - Amphenol-ast
From:Amphenol Author:Admin Clicks:16035times PubTime:2014/1/23 0:00 Staff of The Month in January,2014,from Engineering.
LUTZE Connectivity Solutions Brochure - Lutze Inc.
Press contact LUTZE Inc. 13330 South Ridge Drive Charlotte, North Carolina 28273 USA info (at) lutze.com Tel 704-504-0222 Fax 704-504-0223. Tweet
Model CA102B06 High frequency ICP® pressure sensor, 500 psi, 10 ... - PCB
internal design. Typical ICP® Probe Style Sensor . the above mentioned series, mounted in a 3/8. Each utilizes the acceleration-compensated Series M10 x 1.0 113 installed at the factory in an "off ground" quartz piezoelectric element coupled to a source follower type miniature electronics. (See “General Guide to ICP® Instrumentation,” G ...
CUSTOMER OUTLINE DRAWING - Amphenol RF
any product, process or design, patented or otherwise, that may in any way be related to or disclosed by said drawings, specifications, or other data. EAR# REF: 33,66 REF [1.325] 7,11 REF [0.280] 18,03 REF [0.710] 11,58 REF [0.456] 12,90 [0.508] 11,25 [0.443] REVISIONS REV DESCRIPTION DATE ECN APPR
Small Microphone Has Big Impact on NVH Testing - PCB
The design goal is, for the particular field type, to achieve constant sensitivity regardless of frequency, which is known as a flat frequency response. In usage, to achieve the flat response the microphone must be correctly aligned with the field. For instance, a free -field microphone
156-Channel Rugged Ethernet Switchbox - Amphenol Aerospace
Amphenol’s Octonet Contacts are a proven design used in a variety of Military Programs. The Octonet is a Size 8 contact which houses (4) differential pair contacts. It is a 100 Ohm impedance contact, capable of a data rate of 4 Gbps maximum per contact pair. The contact system has been tested and passed all the Qualification Requirements of ...
LÜTZE Transportation Acquires the Passenger Information Systems ...
LÜTZE Transportation: climate-friendly by rail. Increasing emissions, accelerating climate change, more dramatic consequences for humans and the environment: The ecological balance sheet shows that emissions can be reduced through your choice of transportation.
Product Finder - Lutze Inc.
LUTZE Inc. 13330 South Ridge Drive • Charlotte, North Carolina 28273 • USA Phone: 704-504-0222 • Fax: 704-504-0223 • E-Mail: info (at) lutze.com