Search Results for uses of non-magnetic materials
Data Sheet R-Series V RM5 EtherNet/IP - temposonics.com
2 Temposonics® R-Series V RM5 EtherNet/IP™ 5 3 1 Measurement cycle 1 Current pulse generates magnetic fi eld 2 Interaction with position magnet fi eld generates torsional strain pulse 3 Torsional strain pulse propagates 4 Strain pulse detected by converter 5 Time-of-fl ight converted into position Sensing element (waveguide) Position magnet (magnetic fi eld)
Impact and Drop Testing - PCB
material, the material is absorbing the energy and thus the impact force is minimized and is therefore not a perfectly elastic collision. On the other hand, if the same steel ball is dropped on to a steel plate, it may rebound back to the same height to which is was originally dropped. Thus, very little energy is absorbed.
Model 623C01 High Frequency Industrial ICP® Accelerometer ... - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
Model 628F11 Precision Quartz Industrial ICP® Accelerometer ... - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
Model 625B61 Precision Industrial ICP® Accelerometer Installation and ...
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
SMP Straight PCB Smooth Bore Jack Surface Mount 50 Ohm Non-Magnetic
RF Connector SMP Straight PCB Smooth Bore Jack Surface Mount 50 Ohm Non-Magnetic Shop Categories Search. Products. Back; RF Connectors. Back; Featured Category. RF Connectors; 1.0-2.3 Connectors ... Contact Material: Beryllium Copper: Contact Termination: Solder: Coupling Mechanism: Push-on: Detent Type: Smooth Bore: Export Control ...
Model 621B51 High Frequency ICP® Accelerometer Installation and ... - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
MAC800 vibration meter - Wilcoxon Sensing Technologies
Non-approved; approved models available: We are using cookies to give you the best experience on our website. ... but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Model HT622B01 Platinum Precision Industrial ICP® Accelerometer ... - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
Model 621B41 High Frequency ICP® Accelerometer Installation and ... - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
Model TO603C02 Accelerometer Installation and Operating Manual - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
Model M603C91 Industrial ICP® Accelerometer Installation and ... - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
Data Sheet E-Series EH Analog - Temposonics
Material: Fluoroelastomer Durometer: 75 ±5 Shore A Operating temperature: −40…+204 °C (−40…+400 °F) Material: Steel, zinc plated Material: Steel, zinc plated Application: Used to secure sensor rods (Ø 10 mm (Ø 0.39 in.)) when using an U-magnet or block magnet Material: Brass, non-magnetic
Data Sheet R-Series V RM5 PROFINET (Doc Part No. 552118)
2 Temposonics® R-Series V RM5 PROFINET IO RT & IRT 5 3 1 Measurement cycle 1 Current pulse generates magnetic fi eld 2 Interaction with position magnet fi eld generates torsional strain pulse 3 Torsional strain pulse propagates 4 Strain pulse detected by converter 5 Time-of-fl ight converted into position Sensing element (waveguide) Position magnet (magnetic fi eld)
Model 603M170 Industrial ICP® Accelerometer Installation and ... - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
Model 605B11 Low-cost Biaxial Industrial ICP® Accelerometer ... - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
Temposonics
sensors make use of the properties offered by the specially designed magnetostrictive waveguide. Inside the sensor a torsional strain pulse is induced in the waveguide by momentary interaction of two magnetic fields. The interaction between these two magnetic fields produces a strain pulse, which is detected by the electronics at the head of the
Model M602D01 Platinum Stock Products; Low profile, industrial ... - PCB
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful
Data Sheet E-Series EH Analog - Temposonics
Material: Fluoroelastomer Durometer: 75 ±5 Shore A Operating temperature: −40…+204 °C (−40…+400 °F) Material: Steel, zinc plated Material: Steel, zinc plated Application: Used to secure sensor rods (Ø 10 mm (Ø 0.39 in.)) when using an U-magnet or block magnet Material: Brass, non-magnetic
Model MS622A01 Precision Industrial ICP® Accelerometer Installation and ...
frequency interference. Other critical material selection criteria include non-magnetic stainless steel housing, hermetic sealing, and industrial military connectors. See Figure 1. Dynamic expectations are application-specific and refer to the frequency range of measurement and the anticipated amplitudes of vibration. After careful