Search Results for vertical cargo plane
ExtremePort Z-Link Connector - Amphenol CS
www.amphenol-icc.com Amphenol Information Communications and Commercial Products SFF-TA-1002 STANDARD SOLUTION – UP TO 56G PAM4. Amphenol ICC introduces the SFF-TA-1002 standard . solution – ExtremePort ™ Z-Link, which is a 0.60mm
ms27474 | Amphenol Global Search | Amphenol
ms27474 3d | Amphenol Global Search | Amphenol Search Results for 10144517041802 10144517-041802LF | Bergstak ® Lite 0.8mm | Amphenol Description. BergStak ® Lite 0.80mm, Board-to-Board Connector, 40 Positions, Dual Row, Vertical Receptacle. Environmental Compliance. Drawing. 3D Model (STP) Product Specification. ...
Robotics Archives - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
EMI Filters - Markets | Amphenol Aerospace
Electric Vertical Takeoff and Landing (eVTOL) aircraft are poised to bring urban air mobility to cities around the world in the coming years. Large cities are also rife with all sorts of EMI and RFI caused by many types of communications and transmissions as well as power line noise, electronics, and competing systems.
Whip Antennas MU 3-BZ - amphenolprocom.com
The adjustable ball-joint ensures that the whip can always be mounted in a vertical position independent of the angle of the installation spot. The BZ-mount is particularly well suited for mounting on car-roofs because of its ability to be installed exclusively with access from the outside. The BZ-Mount for roof thickness from 2 mm to 7.5 mm ...
Panel Antennas 766.12.08.00 - amphenolprocom.com
H-Plane | 425 MHz . Ordering Designations. Model Product No. Description Frequency; XPOL panel antenna 120°, 8 dBi: 766.12.08.00-7/16(f) 7/16(f) termination: 380 - 470 MHz: Add to quote: XPOL panel antenna 120°, 8 dBi: 766.12.08.00-N(f) N(f) termination (not PIM specified) 380 - 470 MHz ...
696-798 / 824-900 / 1695-2400 / 1695-2400 MHz - amphenol-antennas.com
696-798 / 824-900 / 1695-2400 / 1695-2400 MHz OCT857KBU102L Connector Description The antenna has eight (8) connectors located at the bottom. Low Band #1 R1 696-798 MHz
Charles Universal Broadband Enclosure CUBE-RL22021FB3 General ...
• Leave adequate horizontal and vertical space between multipleinstallations to allow for proper cable access, as well as enough room around the enclosure to open the door(s). • The site must meet minimal personnel and equipment safety requirements.
696-900 MHz - Amphenol Antenna Solutions
8° | Vertical | 850 MHz 10° | Vertical | 850 MHz Quoted performance parameters are provided to offer typical or range values only and may vary as a result of normal manufacturing and operational conditions. Extreme operational conditions and/or stress on structural supports is beyond our control. Such conditions may result in damage to this ...
ASRN7A12P - Amphenol Air LB
Plug ASR Metallized 10 pin contacts size 22 (A1) Polarizing 2. Products. Quick connection junction modules. 1750 modules. 1750 modules for crimped contacts
696-960 MHz - amphenol-antennas.com
696-960 MHz CX063X24x00 Single Band | Panel Antenna | X-Pol | 65° | 16.8 dBi | Variable Tilt Quoted performance parameters are provided to offer typical, peak or range values only and may vary as a result of normal testing, manufacturing and operational conditions.
All Products - Amphenol
Brush Rack and Panel connector series utilizes Amphenol’s durable and reliable B3 contact system in a rugged, non-floating Rack and Panel connector.
Base Station Antennas | Huge range | Amphenol Procom
Amphenol Procom delivers state-of-the-art Base Station Antenna products for both RF and mechanical constructions. Our innovative approach to product development offers the highest quality and our thorough testing protocol guarantees our Base station antennas are the mos t reliable on the market. W e test all of our products performance against dust, water, wind load, temperature and lightning ...
ASRN2A13S - Amphenol Air LB
Receptacle ASR panel mounting Metallized 10 socket contacts size 22 (A1) Polarizing 3
MIL-DTL-38999 Series II - JT Connectors - Amphenol Aerospace
Amphenol® MIL-DTL-38999 Series II Connectors were developed to meet the needs of the aerospace industry and provided the impetus for the development of the MIL-C-38999 specifications, which later was superseded by MIL-DTL-38999.
Base Station Antennas | Huge range | Amphenol Procom
Amphenol Procom delivers state-of-the-art Base Station Antenna products for both RF and mechanical constructions. Our innovative approach to product development offers the highest quality and our thorough testing protocol guarantees our Base station antennas are the mos t reliable on the market. W e test all of our products performance against dust, water, wind load, temperature and lightning ...
Base Station Antennas | Huge range | Amphenol Procom
Amphenol Procom delivers state-of-the-art Base Station Antenna products for both RF and mechanical constructions. Our innovative approach to product development offers the highest quality and our thorough testing protocol guarantees our Base station antennas are the mos t reliable on the market. W e test all of our products performance against dust, water, wind load, temperature and lightning ...
00176093356 - Amphenol Air LB
1750 series consists of Quick junction modules for signal and low current distribution, where sealing (IP66 / IP68 and IP69K), space and weight-saving are prime requirements.
Micro-Miniature Ruggedized Connectors - amphenol-aerospace.com
Micro-Miniature solutions featuring an array of small form-factor, lightweight, ruggedized connectors for military and aerospace applications
Cross Reference - Airmar
AIRMAR provides information in this cross-reference as a guideline for choosing the correct transducer for your specific fishfinder. Our OEM customers frequently change their models, software versions and plug configuration, which may not be reflected in this cross-reference guide.