Search Results for viscosity meaning glue
Accelerometer Adhesives | PCB Piezotronics
Many accelerometer adhesives have been successfully used for securing mounting bases to test objects. These include epoxies, waxes, glues, gels, and dental cement. Some provide more permanent attachment than others. Stiffer adhesives provide better transmission of high frequencies.
Fundamentals of Torque- tension and Coefficient of Friction Testing - PCB
a torque-tension test and at times a coefficient of friction test. The torque-tension test usually consists of an acceptance input torque window at a specified tension or clamp load value, while the coefficient of friction test requires an acceptance coefficient of friction window (typically the reference coeffi.
ADHESIVE SOLUTIONS - Amphenol PCD
Small, versatile mounting solution for wire bundle management. The base can be mounted by VHB tape or wet adhesive. Interchangeable grommets ensure that you can switch the wire bundle diameter without removing the mounted base. Ideal mounting solution for small, hard to reach places.
Accelerometer mounting and installation techniques
Adhesive mounting • Spot face surface • Abrade surface • Clean surface • Use proper adhesive – VersiLock® 406 / Cat 19 – Loctite® Depend – Loctite® Liquid Metal • Use proper mix ratios 9 Accelerometer mounting considerations August 2012 | Wilcoxon Sensing Technologies proprietary
Mounting hardware and accessories - Wilcoxon Sensing Technologies
Adhesive mounting provides a secure attachment and is the next best alternative to stud mounting. The sensor’s operational frequency range will be reduced because the adhesive acts as a shock absorber, introducing a lower resonance than stud mounting.
Amphenol-BSI Overview - Wilcoxon Sensing Technologies
Deep understanding of interconnect, PCB materials, and the latest in design practices lead to high performing assemblies at the best possible cost. Customers can take advantage of our full design capabilities or use our resources as technical advisors during the design process.
Adhesive Solutions Archives - Amphenol PCDAmphenol PCD
Adhesive cable and pipe supports to mount wires where drilling is not allowed. Ensuring a strong and secure hold for wires, adhesive solutions are resistant to moisture, heat, vibration, and chemicals. Offering adhesive anchor supports, standoffs for elevation, or clamps to immediately secure wires.
Improved Stiffness Specifications for Piezoelectric Force Links - PCB
This paper first defines the physical meaning of the stiffness coefficients and the FEA method used to determine them. Physical testing is shown to build confidence in the determined
Advanced Material Development - MSI Transducers
MSI’s advanced material development team is focused on developing new materials and capabilities to support emerging transducers designs. All this while focusing on: Short lead times. Lower development cost. Advanced performance.
Specifying 4-20 mA vibration transmitters - Wilcoxon Sensing Technologies
Are you looking for the right vibration transmitter for your application? Wilcoxon can help! We have created the form below to walk you step-by-step through the selections you will need to make. To learn more about the meaning behind each parameter, watch our webinar on CBM Connect or read our 4-20 mA vibration sensor selection guide.
Model 352A59 ICP® Accelerometer Installation and Operating Manual - PCB
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may ... Mounting Adhesive Adhesive [4] All specifications are at room temperature unless otherwise specified.
Product Manual - rfstechnologies.com
602400011500 Revision E Radio Frequency Systems 200 Pond View Drive Meriden, CT 06450 Ph. (203) 630-3311 Fax (203) 634-2272 www.rfsworld.com
12 things to consider when selecting an industrial accelerometer
Selecting an industrial accelerometer – what to consider • Acceleration and velocity sensors monitor for different faults – Velocity sensors are used for the majority of applications because velocity is the best overall
TN-23 Pyroshock Explained - PCB
environment of pyroshock. Specifically, it (1) defines pyroshock, (2) identifies those situations where pyroshock can induce equipment failure, (3) explains the response of structural systems to pyroshock, and (4) discusses uniqueness in the shock spectra (see PCB® Tech Note 19) .
TN-42 Load Cell & Torque Sensor Technical Information - PCB
Axis Definition Principal of Operation Figure 1. Wheatstone Bridge Figure 2. Load Cell Wiring Code Figure 3. Right-handed Orthogonal Coordinate System Figure 2 Load Cell Wiring Code PCB Piezotronics, Inc. Toll-Free in USA 888-684-0004 716-684-0001 www.pcb.com 9.1 Load Cell Technical Information ˜ Introduction to load cells ˜ Glossary of terms
6:1 Shrink Tubing - TPC Wire
It easily fits over and seals large, bulky connections and only three sizes are needed to cover cable and connections from 3/4 to 3-1/2 inches. The inner adhesive provides a watertight seal, excellent strain relief, and added tensile strength.
Model TO608A11 Platinum Low-cost Industrial ICP® Accelerometer ... - PCB
Definition of Terms and Symbols The following symbols may be used in this manual: DANGER Indicates an immediate hazardous situation, which, if not avoided, may result in death or serious injury. Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage
UNDERSTANDING TORQUE-ANGLE SIGNATURES OF BOLTED JOINTS - PCB
Torque-angle curve analysis is known to be one of the most basic and practical methods of determining not only what the fastener went through during the tightening process, but also the integrity of the joint itself.
REVIEW OF THE APPLICATION OF DESIGN GUIDELINE VDI 2230 - PCB
In the Guideline VDI 2230 Part 1, bolted joints are treated which have to transmit constant or alternating working loads and which are designed with high duty bolts. A bolted joint is a separable joint between two or more components using one or more bolts.
Model 3741E122G DC Response Accelerometer Installation and ... - PCB
ral amplifier provides a low impedance output to follow-on instrumentation. These particular accelerometers provide a dc or steady state acceleration measurement capability as opposed to a predetermine.