Search Results for volumetric trading reviews
Amphenol Reports First Quarter 2022 Results
First Quarter 2022 Highlights: Sales of $2.952 billion, up 24% in U.S. dollars and 17% organically compared to the first quarter 2021 GAAP diluted EPS of $0.68, up 28% compared to prior year Adjusted Diluted EPS of $0.67, up 29% compared to prior year Operating Margin of 20.0% Operating Cash Flow and Free Cash Flow of $351 million and $274 million Returned more than $320 million to ...
Level Plus - temposonics.com
GOVP (Gross Observed Volume Product,产品总观测体积) 储罐中的产品液体总体积。当仅测量一种液体时,也等于储罐 中的液体总体积 (GOVT)。当测量两种液体时,等于储罐中的液 体总体积减去界面液体体积(GOVT – GOVI)。 GOVT (Gross Observed Volume Total,总观测体积)
EU RoHS II CoC - amphenol-aerospace.com
Per review of the materials & processes utilized in the manufacture of the above-listed part number, Amphenol Aerospace Operations (AAO) and Commercial Air Division (ACAD) hereby acknowledge the referenced product is in conformity with the following: Directive 2011/65/EU (as amended)
Level Plus DDA Tank Gauge Monitor - Temposonics
The Level Plus Monitor system includes volumetric correction software, which is useful in many tank gauging applications. The volume software is powerful, fast, and easy to use; providing the user with gross observed volume (GOV), net standard volume (NSV), and net mass information. See the section below labeled VOLUMETRIC SUPPORT for addi-
EU RoHS II CoC - amphenol-aerospace.com
Per review of the materials & processes utilized in the manufacture of the above-listed part number, Amphenol Aerospace Operations (AAO) and Commercial Air Division (ACAD) hereby acknowledge the referenced product is in conformity with the following: Directive 2011/65/EU (as amended)
EU RoHS II CoC - amphenol-aerospace.com
Per review of the materials & processes utilized in the manufacture of the above-listed part number, Amphenol Aerospace Operations (AAO) and Commercial Air Division (ACAD) hereby acknowledge the referenced product is in conformity with the following: Directive 2011/65/EU (as amended)
aspirador de conductos | Amphenol Global Search | Amphenol
Bestellschlüssel / How to order / Système de référence 5 – 7 VG95234 / GCB-B – Polbilder / Contact arrangements / Arrangements 8 – 13 Einbaumaße / Mounting dimensions / Cotes d’encombrement 13 – 14 Gehäuseformen / Shell style / Style de boîtier 15 VG95234 Form A / VG95234 Style A t VG95234 Form B1, B2 / VG95234 Style B1, B2 16 ...
Level Plus - temposonics.com
The total volume of the tank occupied by the interface liquid. The GOVI is only given when measuring two liquids and is calculated by subtracting the volume of the product from the total volume of liquid in the tank (GOVT – GOVP). GOVP (Gross Observed Volume of the Product) The total volume of the tank occupied by the product liquid. When
EU RoHS II CoC - amphenol-aerospace.com
Per review of the materials & processes utilized in the manufacture of the above-listed part number, Amphenol Aerospace Operations (AAO) and Commercial Air Division (ACAD) hereby acknowledge the referenced product is in conformity with the following: Directive 2011/65/EU (as amended)
CHAMBERED ¸z² - temposonics.com
VCF(Volume Correction Factor, 부피 보정 계수) ‘Volume Correction Factor’의 약자로 액체 팽창/수축에 대한 보정 계수와 온도 포인트(지점)에 대한 상관 관계를 나타내는 측정 표입니다. 트랜스미터는 최대 50 포인트까지 포함할 수 있습니다. 3. 소개 3.1 사용 설명서 목적 및 ...
EU RoHS II CoC - amphenol-aerospace.com
Per review of the materials & processes utilized in the manufacture of the above-listed part number, Amphenol Aerospace Operations (AAO) and Commercial Air Division (ACAD) hereby acknowledge the referenced product is in conformity with the following: Directive 2011/65/EU (as amended)
EU RoHS II CoC - amphenol-aerospace.com
Per review of the materials & processes utilized in the manufacture of the above-listed part number, Amphenol Aerospace Operations (AAO) and Commercial Air Division (ACAD) hereby acknowledge the referenced product is in conformity with the following: Directive 2011/65/EU (as amended)
Amphenol SF-NLMAMB0001-0001 OSFP 400G Loopback Adapter Module for OSFP ...
Genuine Amphenol 400G OSFP loopback adapter modules provide the ideal 400-Gigabit Ethernet rated port testing solution for OSFP enabled ports (50.0 Gbps x 8 channels). This low-profile passive OSFP 400G loopback cable features typical insertion loss (attenuation) characteristics of a mere 0dB; consuming no more than 0.0 Watts of power in the process.
MMCX Right Angle Solder Plug 0.047-inch Conformable 50 Ohm
Under Review - Please Contact Us; California residents see Prop 65 Warning Additional compliance information is available in our Compliance Center. Skip to the end of the images gallery. Skip to the beginning of the images gallery. Description. RF Connector MMCX Right Angle Solder Plug 0.047-inch Conformable 50 Ohm ...
Betriebsanleitung Level Plus CHAMBERED - temposonics.com
Level Plus ® CHAMBERED Betriebsanleitung I 5 I S Schnittstelle Substantiv.;Die grafische Benutzeroberfläche (GUI) der Software, über die der Benutzer auf Software-Protokolle zugreifen kann (HART®, DDA, MODBUS).Spezifisches Gewicht Das Verhältnis der Dichte einer Flüssigkeit zur Dichte von Wasser unter gleichen Bedingungen.
Trasmettitori di livello liquidi magnetostrittivi
liquido, corrisponde al volume del prodotto (GOVP). Quando si misurano due liquidi, corrisponde al volume dei liquidi del prodotto e dell'interfaccia (GOVP + GOVI). GOVU (Gross Observed Volume Ullage, volume vuoto lordo osservato) Differenza di volume tra la capacità utile del serbatoio e il volume totale nel serbatoio (capacità utile - GOVT).
EU RoHS II CoC - amphenol-aerospace.com
Per review of the materials & processes utilized in the manufacture of the above-listed part number, Amphenol Aerospace Operations (AAO) and Commercial Air Division (ACAD) hereby acknowledge the referenced product is in conformity with the following: Directive 2011/65/EU (as amended)
UST850 Smart™ Sensor Thru-hull NMEA 2000® - Airmar
Airmar’s patented UST850 just turned your maintenance time into more cruising time—and made your boat smarter too. Get ultrasonic speed and temperature in a single thru-hull housing with no moving parts.This sensor is a high-precision, low-maintenance solution for use on power and sail boats of all types and sizes.
SMB PCB Through Hole Straight Jack 50 Ohm | 903-499J-51P2 - Amphenol RF
Under Review - Please Contact Us; California residents see Prop 65 Warning Additional compliance information is available in our Compliance Center. Skip to the end of the images gallery. Skip to the beginning of the images gallery. Description. RF Connector SMB PCB Through Hole Straight Jack 50 Ohm ...
BNC Straight Crimp Plug Times LMR-400 Optimized 50 Ohm
Under Review - Please Contact Us; California residents see Prop 65 Warning Additional compliance information is available in our Compliance Center. Skip to the end of the images gallery. Skip to the beginning of the images gallery. Description. RF Connector BNC Straight Crimp Plug Times LMR-400 Optimized 50 Ohm ...