Search Results for what is a platform in technology
AirMax VS High-Speed Backplane Connector | Virtual Shield Technology ...
AirMax VS® connectors use innovative edge-coupling and air dielectric between adjacent conductors to deliver insertion loss and crosstalk. The shieldless open pin field design with no pre-assigned ground pins provides the ultimate flexibili
High Current Pin Contacts | Temper-Grip - Amphenol Aerospace
Using high conductivity alloys and precision machining, Amphenol has developed a high current pin to reduce power loss in your application. Push the current carrying capability past the limits of a Mil-Spec contact, or simply improve the efficiency of your system while reducing the heat dissipated into your platform.
AE-AN-CA-001 - ANATOMY OF A CONNECTOR ASSEMBLY (CA)
Our core technology is the smallest, fastest, most electrically efficient compression mount connector technology worldwide. As data rate requirements increase and devices and systems shrink, Ardent’s products deliver superior signal integrity in a dense footprint that can be reusable across programs to maximize cost savings.
D-Shaped Connectors | Products - Amphenol
This standard Micro-D interface connector is equipped with Amphenol surface mount clip technology. It is fully intermateable with standard M83513 connectors but provides a reduced footprint allowing for increased contact density. It eliminates the need for washing and soldering processes saving time and cost in PCB assembly.
Amphenol Corporation Releases 2019 Sustainability Report
Amphenol Corporation (NYSE: APH) today released its 2019 Sustainability Report highlighting the progress the company has made over the past three years in the areas of resource efficiency, product impact, supply chain, employee engagement and governance. “The world is currently facing a unique crisis as a result of the COVID-19 pandemic, with individuals, companies and countries experiencing ...
V17-001-01-A0 - Amphenol Antenna Solutions
2T2R Lens Antenna, 3300-4000 MHz, 17° Azimuth, 17° Elevation, 299 mm Length
Amphenol Solar Interconnect Solutions - Amphenol Industrial Operations
RADSOK® Technology with long-term stability Voltage level: TUV 1000V / 1500V DC UL 1000V/ 1500V DC 1. www.amphenol-industrial.com Protecon: o IP68(1m,24H) o UV resistance o Safety class II Compability H4 H4 Plus H4 H4 Plus 2 An-backspin ratcheng backnut gland. Connectors Rated Current Rated Voltage Locking ...
Other Connectors | Products - Amphenol
For modern society and industry, energy supply is a key element. A high-performance, reliable connection technology is required. Our solar connectors are ideally suited for connecting solar cables, connection to photovoltaic panels, and for connection to solar inverters.
News - Wilcoxon Sensing Technologies
Wilcoxon and KCF Technologies Partnership Enhances KCF’s Predictive Maintenance Platform > Dec 4, 2024. ... HART communication is a field proven technology that offers the ability to interrogate and remotely program field installed devices. Meggitt’s new programmable transmitter allows vibration data to be accessed by HART enabled process ...
Fiber Splice Solutions - Amphenol Broadband Solutions
Mechanical compression technology provides cost-effective, reliable sealing Sealed IP68 rated and can be used both aerially and below grade 8 drop ports can accommodate flat or round drop cables 24 splice capacity 1x4 or 1x8 PLC splitters available Info Sheet
3U VPX 56 CHANNEL 25G ETHERNET SWITCH - Amphenol Aerospace
The changes in technology where R-VPX connectors are used has rapidly evolved in recent years, specifically driving a demand for higher data rates from copper contact based connectors, which have typically resided in the 10 & 16 Gbps speed realm. The fastest connector in the market to date is performing to 25 Gbps, but the market
Trooper Max 5G Combination Antenna Platform with LMR Option - PCTEL
Trooper TM Max antenna platform with sharkfin form factor allows seamless installation on leading public safety sports utility vehicles and fire trucks with ridged rooftops. Supports the high-speed requirements of complex RF communication systems used for critical communications in public safety fleets and Intelligent Transportation Systems (ITS).
GPLUS Sensor - ssi-sensors.com
Ultrasonic technology, combined with an on-board thermistor for temperature compensation provides a more accurate sensor than alternative low-cost level sensing technologies. GPLUS comes with a simple analog output, diagnostics, a programmed fluid averaging filter, and a simple twist-lock installation making it the perfect solution for your ...
PCTEL’s David Adams Named President of Safer Buildings Coalition (SBC ...
PCTEL Public Safety Network Testing Expert Takes on Leadership Role in SBC’s Mission of Eliminating In-Building Wireless Dead Zones. BLOOMINGDALE, Ill.--(BUSINESS WIRE)--Aug. 31, 2023-- PCTEL, Inc. (Nasdaq: PCTI), a leading global provider of wireless technology solutions, today announced that David Adams, PCTEL’s Director of Market Development for critical communications test and ...
J2496 More Information - Positronic The Science of Certainty
Provide flexibility for expansion as technology advances while minimizing hardware and software upgrade costs; The VAN Subcommittee was successful in meeting these objectives. Their efforts have resulted in the SAE J2496 Transit Area Network Cabling Standard. This is comprised of a series of access boxes and cables, which are simple, effective ...
New Products | PCB Piezotronics
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
Power | Amphenol Network Solutions
22425 East Appleway Ave #11 Liberty Lake, WA 99019 Phone: 509.926.6000 Email: getinfo@amphenol-ns.com
Catch Sensors User Guide - Marport
Technology Corporation. Disclaimer Marport endeavors to ensure that all information in this document is correct and fairly stated, but does not accept liability for any errors or omissions. The present user guide is applicable for the following versions: • Scala: 01.06.06-01.06.34 / Scala2: 02.10.x • Mosa2: 02.11.x Patents apply to products.
Market Connector: Lunar Exploration - Amphenol Aerospace
The moon holds clues to help scientists understand the early history of our solar system, and there is potential for mining valuable lunar resources such as water ice and helium-3. The moon also serves as a stepping stone for future deep-space exploration and a platform for international collaboration in space.
Hydroelectric dam | Innovative energy solutions - CMR Group
We supply efficient and advanced systems that understand the latest technology. A global partner: we offer a local realization thanks to support in our 12 operational sites around the world. ... Integrated control and command platform & cyber security, turnkey system delivered from studies to commissioning. Let's discuss your project together.