Search Results for what is oxidizing metaaal
The Advantages of Gold Plating in Connectors - Positronic
Gold is incredibly resistant to oxidation, especially when compared to other metals. If a connector’s contacts will be exposed to corrosive environments or agents, gold plating can provide a strong defense and protect against oxidation and corrosion.
Gold Plating On Connectors - SV Microwave
Corrosion in connectors typically manifests as rust, base metal bleed-through, or tarnish, reducing electrical reliability. Rust, in particular, reduces reliability by forming an oxide layer that causes connection and conductivity issues.
Glossary of RF Terms - Amphenol RF
A form of accelerated oxidation that appears at the interface of contacting materials undergoing slight cyclic relative motion. All non-noble metals (tin) are susceptible to some degree of fretting corrosion and will suffer contact resistance increases.
Installation guide for hazardous areas - Wilcoxon Sensing Technologies
While the oxidizer in most fires is oxygen, other chemicals may be oxidizers. For example, elemental magnesium will react violently with water to release heat. The magnesium is the fuel and water provides the oxidizer. The fuel component can be almost any substance. Most materials will burn under the right temperature and pressure conditions.
Pellistor Application Note 1 Pellistor Sensor Technology & Applications
Pellistors are gas sensors that detect combustible gases and vapours in air (or atmospheres containing oxygen), in concentrations approaching the explosive range. In this case, they are operating in a catalytic mode where the target gas is burnt and the heat liberated is measured by the sensor.
Learn More about Connector Mating Cycles - Amphenol CS
The number of times a connector can connect and disconnect with its counterpart while meeting all its specifications is termed as “mating cycles”. The mating cycle of a connector helps to estimate the life span of a connector in a particular application.
Superseal Connectors - CONEC
The overmoulded VSS Superseal connectors developed by CONEC offer optimum protection even in the most difficult applications, such as underground, at sub-zero temperatures or in dusty, hot environments. The VSS Superseal connectors are designed as a cable-to-cable connection and latch/lock securely with the mating connector via a latch.
Hybrid overmoulded - CONEC
Hybrid overmoulded connectors are offered as single ended and connection cables in various standard lengths and are electrically tested with regard to transmission properties according to IEC 11801 Cat 5e. All four sizes (B12, B17, B23, B40) are equipped with a bayonet locking mechanismand thus guarantee a fast and secure connection.
EMI/EMP FILTER PROTECTION WORKSHEET - amphenol.co.jp
This section deals with connectors that contain active devices such as diodes, metal oxide varistors (MOVs) and fuses. • What connector needs to be protected? • Does the solution require both filters and transient protection or just transient protection? • What devices are preferred? Diodes, MOVs, or fuses?
Protocol Manual MH-Series with J1939 Safety - temposonics.com
It is the responsibility of the user to adhere to the SAE J1939 specification and to properly integrate the sensor protocol into the Safety System. The sensor electronics and functionality will remain current to the development of the SAE J1939 standard.
MH-Series with CANopen Safety (Document part number 901997)
Structure of the SRDO, position and velocity in the process data. The safety relevant function of the sensor with “S02” protocol is providing the position of the target magnet along the measuring axis.
Welding Best Practices & Processes - TPC Wire
The weld area and electrode are protected from oxidation or other atmospheric contamination by an inert shielding gas. GTAW is commonly used to weld thin sections of metal such as steel and aluminum.
The Evolution of R-VPX - Amphenol Aerospace
R-VPX EVO2 is a VITA 46 compliant connector system. The R-VPX EVO2 connectors, like previous R-VPX and R-VPX EVO1 versions, are fully intermateable with the aforementioned connectors. (as well as RT2, RT2-R, & RT3 from TE) Intermountability is described below:
FAQ - Amphenol Socapex
The « IP » defines the resistance of the product against solids (first number) and liquids (second number).
When mated, the Powersafe is defined as IP68.
Low frequency measurements - Wilcoxon Sensing Technologies
Low frequency vibration • Very little vibration amplitude in terms of acceleration is produced at low frequencies • Much larger amplitudes are produced in terms of
Installation Guide Hazardous Areas 0908 CCS - Wilcoxon Sensing Technologies
While the oxidizer in most fires is oxygen, other chemicals may be oxidizers. For example, elemental magnesium will react violently with water to release heat. The magnesium is the fuel and water provides the oxidizer. The fuel component can be almost any substance. Most materials will burn under the right temperature and pressure conditions.
D38999 Series III Filter Connectors - Amphenol Aerospace
Amphenol’s MIL-DTL-38999 Series III connectors are unrivaled in their performance and reliability. With added filter features, the high-performance general duty threaded connector is designed to withstand the pressures of severe environment applications.
THHN Wire, Meet Your Replacement!
THHN is a thermoplastic high-heat-resistant, nylon-coated wire. It’s designed with a specific insulation material, temperature rating, and condition of use for electrical wire and cable.
Sensor Mounting Techniques | PCB Piezotronics
Four main methods are used for attaching sensors to monitoring locations in predictive maintenance. They are stud mounted, adhesive mounted, magnetically mounted and the use of probe tips, or stingers. Each method affects the high frequency response of the accelerometer.
10162068 | Amphenol Global Search | Amphenol
Sensing element electrically isolated from tag. For more technical details, refer to product specification and application specification. Have any questions? Talk with us directly using LiveChat. Click on the Check Sample (if available) button to check the allowed sample quantity in the cart.