Search Results for what is the long item in the front of the ch 53k called
Charles Universal Broadband Enclosure CUBE-SC3NN12HN5 General ...
Obtain the following recommende d or needed items for installing the CUBE. • Sufficient length and quantities of fiber cable (or pigtails) • Cable scoring, opening, and cutting tools for cable sheathing, shields, wrappings, strength members and buffer tubes • Wire strippers • Crimpers • Cable, tube, wire, and fiber cleaning materials
Model 3503A1020KG Triaxial High Amplitude MEMS Shock ... - PCB
ZMO – Zero Measurand Output, also called bias or offset, is the output when no input acceleration is applied. TSS – Thermal Sensitivity Shift, the change of sensitivity due to temperature. The sensors are uncompensated, so they display a slight linear decrease in sensitivity as temperature increases.
FS34 - Amphenol Fiber Systems International (AFSI)
The FS34 is a rugged circular fiber optic connector designed by Amphenol Fiber Systems International for harsh environments.
H3 Sensor Rod - Temposonics
The H3 sensor rod guides 3 RFV sensors, boosting availability by preventing downtime. Its compact design accommodates different sensor outputs efficiently with a Ø 25 mm diameter. Each sensor is independently guided for easy replacement without disrupting others, maintaining a closed hydraulic circuit.
Model 5310D-04A TORKDISC® Rotary Torque Sensing System ... - PCB
found on the title page at the front of this manual. Our ship to address and general contact numbers are: PCB Piezotronics, Inc. 3425 Walden Ave. Depew, NY14043 USA Toll-free: (800) 828-8840 24-hour SensorLineSM: (716) 684-0001 Website: www.pcb.com E-mail: info@pcb.com
Amphenol
The front insulator must butt the rear insulator, and inner contact retention shoulders must enter front insulator bores. 2. Observe the front insulator’s keyway. When the inner pin assembly is held in the ver-tical position (with inner pin contacts on top), the inner pin contact with the insulator
RET - Amphenol Antenna Solutions
RET - Amphenol Antenna Solutions
High-Speed Voice and Data Link Local Powered Remote Terminal
The system must be configured for repeater mode (RPTR). This is done through the front panel of the COT. Up to 3 repeaters can be put between the COT and the RT, increasing the system range. In repeater mode, the COT applies DSL voltage (+/–130 VDC) to the DSL line immediately to begin synchronizing with the Repeaters and RT. 1.3 Equipment ...
El Sharko Datasheet - amphenol-aerospace.com
front and RTM areas of the chassis Heat sensing automatic fan speed plus manual dial override Environmental The DK3 is intended for lab use in benign environments Controls and I/O Rear switch for AC ON/OFF, Status indicators: AC, +12V, +5V, +3.3V, Backplane Options 8 slot power and ground 40Gb backplane, 1.2" pitch, slots 1 -4
3652–69 4-Wire Tandem Channel Unit (4W TDM) - Charles Industries
eject lever in the form of a hinged front panel which ensures a positive connection of the channel unit’s card-edge connector to the backplane connector when the unit is installed. The insert/eject lever also makes the channel unit easier to remove. Install and remove modules with care. Do not force a module into place. If excessive resistance is
Amphenol Network Solutions > 2RU HIGH DENSITY SHELF
The 2RU High Density Shelf (Gen 4) offers unparalleled capacity in a variety of headend, hub, or data center applications. This shelf takes advantage of the industry-leading density of Amphenol cassettes to pack much greater fiber capacity into a 2RU space. Because the depth of the Mini-LGX® is half (or less) of traditional industry devices, the shelf may be populated on both the front and ...
Temposonics
This product may be used only for the applications defined under item 1 and only in conjunction with the third-party devices and components recommended or approved by MTS Sensors. As a prerequisite of proper and safe operation, the product requires correct transport, storage, mounting and commissioning and must be operated with utmost care.
Mask Group 23 - Amphenol Antenna Solutions
Mask Group 23 - Amphenol Antenna Solutions
MACH-D Connectors: Highly Reliable & Customizable
At Positronic, we’re proud to be an industry leader known for high-reliability electronic connectors. When we say “high-reliability,” we mean connectors that are built to withstand the harshest conditions.
www.amphenol-aerospace.com
www.amphenol-aerospace.com
3632–00 Digital Signal Level Zero Data Port (DS–0 DP) Channel Unit
Charles Industries’ equipment is identified by a model and issue number imprinted on the front panel or located elsewhere on the equipment. Each time a major engineering design change is made on the equipment, the issue number is advanced by 1 and imprinted on subsequent units manufactured. Therefore, be sure to include both
Repair and Maintenance Returning Equipment Contact Information Safety ...
Manual 21354 Rev E ECN 50523 CAUTION Refers to hazards that could damage the instrument. NOTE Indicates tips, recommendations and important information.
3657-02 2W FXS/GT Channel Unit Installation Guide - Charles Industries
insert/eject lever in the form of a top-hinged front panel, which ensures positive connection of the channel unit’s card-edge connector to the backplane connector. The insert/eject lever also facilitates channel unit removal. Installation and removal of channel units should be done with care. Do not force a unit into place. If
21-33382-21 (PIN) 21-33383-21 (SOCKET) Contact, Pin and Socket, Quadrax ...
The front insulator must butt the rear insulator, and inner contact retention shoulders must enter front insulator bores. 2. Observe the front insulator’s keyway. When the inner pin assembly is held in the verti-cal position (with inner pin contacts on top), the inner pin contact with the insulator key-
Expanded Base Installation Guide for Charles CP212-EP Pedlock®
Lift the front half over and onto the four alignment pins. 11 Determine base installation location. Position the base in the approximate desired position in the trench. The front or drop side of the base (Charles logo) generally faces the street. Using either the back half of the base or the entire assembly, position the feed