Search Results for where is the diamond certification located
Adrienne Cooper - svmicrowave.com
Certificate of Compliance GENERATED: 12/27/2022 This is to certify that the parts supplied by SV Microwave, Inc listed in the table below meet the requirements of RoHS Directives 2011/65/EU and 2015/863/EU, except on any that are marked as "NO" in the 'RoHS COMPLIANCE STATUS' column. Exemptions, if taken, are noted in the same column.
Universal Broadband Enclosure (CUBE) - Amphenol Broadband Solutions
Construction: 0.125″ Aluminum Welded Construction Outer Enclosure, Powder Coated Cool White Finish. Mounting Style: Pad Mount Enclosure. Thermal Management: Solar Shield and Venting on all models, Direct Air Cooling, DC HVAC or AC HVAC for Env.Conditioning. Door Latching: 3-Point Latching with Pad Lockable Handle in Front, Removable Panels in Rear, Wind Latch Each Door
Whip Antennas DFA 2/70-X/... - AMPHENOL PROCOM
3. Operation using a Diplexer. Several advantages are gained by using only one antenna. Only one single hole has to be drilled into the car body, only one cable installation has to be run, the car appearance is not destroyed by carrying several whips and also, it may be a particular demand that it should not be too obvious to see that the car is equipped with transceiving equipment.
Model ADP008A | PCB Piezotronics
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
Model 2508-05A | PCB Piezotronics
Model 2508-05A:PCB L&T Reaction Torque Transducer, 1,000 in-lb/83 ft-lb (113 N-m) rated capacity, 50% static overload protection, 2-in (50.8 mm) Steel
RFS Technologies an Amphenol Company
RFS Technologies designs and manufactures premium-quality cable and antenna solutions for wireless, public safety, distributed antenna system (DAS) and other telecom markets in North America. As an Amphenol company, we’re part of a global powerhouse in high-technology, interconnect, sensor and antenna solutions that’s enabling the electronics revolution across almost every industry.
10127720-081LF | Minitek® Pwr 3.0 | Amphenol
Amphenol is one of the leading manufacturers of 3.00mm Wire to Board Signal. Contact us today for more details of Minitek ® Pwr 3.0, part number 10127720-081LF.
EU RoHS II CoC - amphenol-aerospace.com
(8 5r+6 ,, &huwlilfdwh ri &rqirupdqfh 2fwrehu 'hdu &xvwrphu ,q uhvsrqvh wr \rxu frpsoldqfh vwdwxv lqtxlu\ uhjduglqj wkh iroorzlqj surgxfw $pskhqro $hurvsdfh
696-798 / 824-896 / 1695-2400 / 1695-2400 MHz - amphenol-antennas.com
Total Number of Connectors Antenna has 8 connectors located at the bottom Connectors Per Band 696-798 MHz (2x) 7/16-DIN Female 824-896 MHz (2x) 7/16-DIN Female 1695-2400 MHz (2x) 7/16-DIN Female 1695-2400 MHz (2x) 7/16-DIN Female Diplexed No Lightning Protection Direct Ground Operating Temperature -40° to +60° C (-40° to +140° F)
PCTEL Enhances In-Building Public Safety Testing for FirstNet, LTE and ...
LAS VEGAS--(BUSINESS WIRE)--Jun. 10, 2019-- PCTEL, Inc. (Nasdaq: PCTI) today announced it is adding public safety LTE grid testing and enhanced P25 signal quality measurements to its award-winning public safety network testing solution today at the In-Building Wireless Congress.The new testing capabilities support two growing trends in public safety communications across the United States ...
XMAPD10-2-8-2S - XMA
Power Divider, SMA-f, 2-8GHz, 2-Way, 10W
2.4mm Male to SMPM Female 24" Cable Assembly for .047 Cable
Use personal protective equipment as required. Do not eat, drink or smoke when using this product. Wash thoroughly after handling. Recycle if possible and dispose of the article by following all applicable governmental regulations relevant to your geographic location. CE / UKCA Compliant. This products meets the requirements for CE and UKCA.
April Birthday Party|Warm April, Cherish the Spring Light
Every year brings a gift, brings joy. The most beautiful April day in the world, On April 20th, Amphenol welcomed a beautiful April birthday party~
N-Type Straight Crimp Jack RG-316 Bulkhead Front Mount 50 Ohm IP67
Compliant with Exemption 6C - View Certificate; California residents see Prop 65 Warning Additional compliance information is available in our Compliance Center. Skip to the end of the images gallery. Skip to the beginning of the images gallery. Description. N-Type Straight Crimp Jack RG-316 Bulkhead Front Mount 50 Ohm IP67 ...
Deep Space 38999 | MIL-DTL-38999 Connectors | Mil-Spec Type Circulars ...
The Deep Space 38999 Connector series is designed for extreme cold environments. They are built to retain a grommet-to-wire and contact-to-contact seal in temperatures below -85 °F (-65 °C), with inserts that have been cycle tested between -319° F (-195 °C) to 392 °F (200 °C).
2002-7010-0X-CRYO - XMA
Industries. Space High performance from Earth to orbit; Cryogenic Increasing density and decreasing thermal noise; 5G Communication High frequency for ever-increasing network traffic; Mil/Aerospace Using Advanced Disruptive Principles to Ensure Future Success; Products. Attenuators. Reducing input power while maintaining signal integrity
Website Registration - amphenol-ns.com
Your shopping cart is empty. Product Qty Amount; From: Until:
SMA Right Angle Plug to SMA Straight Bulkhead Jack IP67 RG-316 12 ...
Compliant with Exemption 6C - View Certificate; California residents see Prop 65 Warning Additional compliance information is available in our Compliance Center. Skip to the end of the images gallery. Skip to the beginning of the images gallery. Description. SMA Right Angle Plug to SMA Straight Bulkhead Jack IP67 RG-316 12 Inches (305 mm) ...
300308 | aldenproducts.com
Maximum Cable Diameter. 0.3. Housing Color
Amphenol AAO/ACAD Product Compliance - Environmental Engineering
EU RoHS Certificate of Conformance October 31, 2017 Dear Customer, In response to your compliance status inquiry regarding the following product, Amphenol Aerospace Operations and Commercial Air Division offers the following information: AAO/ACAD Part Number EU RoHS Compliant