Search Results for where is this place
Busbars | Products | Amphenol Interconnect Product Corp
Benefits. Eliminates or reduces the need for heavy (oz) copper layers; Opens up areas of the PCB for improved high-speed signal management; Can be wave-soldered or bolted into place
Careers - Amphenol RF
If you are a professional who is seeking to establish a career with a world leader in electronic component manufacturing, Amphenol RF is the place for you. Amphenol RF offers competitive salaries, comprehensive benefits, work/life balance, an outstanding work environment, entrepreneurial spirit and opportunities for growth.
Level Plus - Temposonics
7.5 Clean-in-Place Floats 24 7.6 Special Products 25 7.7 Long Gauge Floats 26 8 MAINTENANCE 27 9 ADJUSTMENTS 28 9.1 Alarm Settings 28 9.2 Calibration for C4 Transmitters 28. 1 INTRODUCTION MTS is recognized as the pioneer, innovator, and leader in magnetostrictive sensing. The new Level Plus
TN-25 How High in Frequency Are Accelerometer Measurements Meaningful - PCB
3991) was designed and introduced into the market place. While this accelerometer has the same foot print as the Endevco 7270, its most significant differences are its contained damping (~ 0.05 of critical viscous, Q=10) and over-range stops [2]. The goal of the damping is to reduce the “Q” of the sensor at its resonant frequency. This ...
D-Subminiature High Density Connectors - Amphenol CS
board using pick and place processes § Various PCB and Panel mounting accessory options available § Wide variety of choices for secure connection § Hoods available in plastic, metalized and metallic form with locking screws § Supports cable connection; Prevents risks of pulling up and accidental un-mating
BNC Straight Crimp Plug RG-58 RG-141 Times LMR-195 50 Ohm
RF Connector BNC Straight Crimp Plug RG-58 RG-141 Times LMR-195 50 Ohm. This connector is machined from brass and features a nickel plated body and coupling nut. A male center contact is held in place by a Delrin insulator.
Amphenol @ 2024 OCP Global Summit
The 2024 OCP Global Summit, scheduled for October 15-17 in San Jose, California, is poised to be a landmark event in the Open Compute community.Under the theme "From Ideas to Impact," the summit will bring together industry leaders, researchers, and innovators. It will be an engaging arena of dynamic discussions and workshops aimed at transforming theoretical concepts into practical solutions.
AZIMUTH TILT TABLE INDICATOR TILT (DEG) A 0° B 5° C 10° B D 15° E 20° F ...
0 place 1 one place .5 two place .2 proprietary and confidential the information contained in this drawing is the sole property of amphenol antenna solutions. any reproduction in part or as a whole without the written permission of amphenol antenna solutions is prohibited. a drawn do not scale drawing bracket mounts to pole
Assembly Instructions-C26 Amphenol BNC
Place contact on cable center conductor so that it butts against cable dielectric. Crimp contact in place using Die Set Cavity indicat-ed in table above. When using RG-62, 71, 210 cable, install bushing over center con-ductor before installing contact. Step 3 Install cable assembly into body assembly so that inner ferrule portion slides under ...
µCom-10Gb+ Series - Amphenol PCDAmphenol PCD
Interconnect systems optimized for the extensive data transmissions that take place within modern missiles and guided munition systems during flight. Ruggedized products, optimized for performance and endurance in the world’s harshest environments, and engineered to achieve consistently exceptional performance.
TN-9 Shunt Calibration of a Strain Gage Sensor - PCB
5. Place a shunt calibration resistor across an appropriate leg of the Wheatstone Bridge as discussed above. 6. Record the value of the signal conditioner's output signal and/or numeric display. This value is the shunt calibration value, or equivalent load. 7. It is important to note that the shunt calibration value is specific for the
Push Pull Connectors | Products | Amphenol Aerospace
What is Push/Pull? Push/pull connectors are circular connectors that prioritize quick connection and disconnection. Amphenol push/pull connectors provide audible and tactile feedback, a system that provides immediate feedback when the connector is mated.
Mobile Devices | Markets - Amphenol
Amphenol designs and manufactures an extensive range of interconnect products, antennas and electromechanical components found in a wide array of mobile computing devices.
Installing the Sensor on the Trawl - marport.com
Place sensor (1) at the centre of the net's headrope (2), facing the vessel.Install a double-mesh piece of netting (3) to stabilize the sensor.Buoys (4) on either sides provide a level platform for the unit during trawling operations.Buoys ensure that down-looking transducer beam (5) is vertical for footrope (6) detection.
Charles Universal Broadband Enclosure SHRD56-051 ... - Charles Industries
The GB5 model has a Raycap disconnect device in place of the AC load center. The SHRD56-601xTGB1, TGB3, and TGB6 models support two radios total. Choose from Ericsson 8843, 4449, 4478, 4426, and 4415 RRH. It also supports either two Ericsson 6302 or four Ericsson AC -08 power supplies, two Commscope diplexers, and one Charles CFTT
Metral® Board Connectors | FCI Basics | Backplane Connector | Futurebus+
FCI Basics Metral® product family offers the broadest range of backplane connector solutions which includes right angle and vertical for both header and receptacle series.
Section 319–29F–301 Equipment Issue 1 STS 3192–9F Alarm Module ...
place. If excessive resistance is encountered while installing a module, remove the module, and check the card guides and connector to verify proper alignment and the absence of for-eign material. Step Action 1. Release and rotate the securing bar. Push the spring clip tab on the left pivot point away from the shelf while rotating
Amphenol RF
third angle proj. rev description date revisions eco appr cad file dwg size rev unless otherwise specified, dimensio ns are in inches and tolerances are:
Expanded Base Installation Guide for Charles CP212-EP Pedlock®
Place a 2” diameter washer and lock washer onto each bolt. Tighten bolt to a maximum of 75 in- lbs. Use only the supplied galvanized hardware. Figure 5 Mounting the UMS Stake on the Base 10 Assemble the base. If the cable tails can fit through the base collar, the two halves can be assembled prior to positioning the base.
ForwardScan 2D 9-pin
“The best way to stay safe is to not hit anything in the first place!” – judging committee member David Schmidt, Boating Writers International. ForwardScan Technology. ForwardScan provides forward-looking, two-dimensional sonar imaging of the bottom ahead of your boat. In shallow, unfamiliar, or poorly charted waters, ForwardScan is a ...