Search Results for where is this place
Mobile Connector & Cable Introduction - Amphenol Mobile Consumer Products
Spring Clips are suitable for automatic assembly processes: pick & place, tape & reel packaging and SMT solderable. Amphenol MCP offers a wide variety of WTB and BTB connectors for consumer products applications. We also offer cable assembly solutions for mobile consumer products including wearables.
3658–05 2-Wire Foreign Exchange Office with Gain Transfer (2W FXO/GT ...
Place switch S1 to the NORM (down) position to condition the 3658–05 for normal (in-service) operation. Place S1 to the BUSY (up) position to create an out-of-service condition for testing or alignment purposes. This will also light the BUSY LED on the front panel and on the Alarm Logic Unit (ALU), and will busy the channel unit on the far-end.
Cyber Security Caps (CapLock & PlugLock) - Amphenol PCD
Interconnect systems optimized for the extensive data transmissions that take place within modern missiles and guided munition systems during flight. Ruggedized products, optimized for performance and endurance in the world’s harshest environments, and engineered to achieve consistently exceptional performance.
Application solution - Wilcoxon Sensing Technologies
Two of the greatest problems facing the vibration analyst are how many sensors to mount and where to place them. For typical equipment sets of direct-driven fans there will usually be four total bearings with one of them acting as a thrust bearing. This means a total of five sensors would be the usual optimum number of sensors because there ...
Model 607A01 Swiveler® Industrial ICP® Accelerometer ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
ValProbe RT Humidity/Temperature Logger - KAYE
The ValProbe RT logger with humidity and temperature sensors comes with RF technology to give users real-time data viewable on their Validation Console. With a humidity range of 15% to 95%, and a temperature range from 0°C to 70°C, this logger has a wide range of capabilities for temperature and hum
CTR-80 Ultra Low Temperature Bath - KAYE
The Kaye CTR-80 Calibration Bath is the ideal unit for the precise calibration of temperature sensors and data loggers used in the qualification of freeze-dryers, freezers, and ultra-low temperature units.
CUSTOMER OUTLINE DRAWING - amphenolrf.com
third angle proj. rev description date revisions eco appr cad file dwg size rev unless otherwise specified, dimensio ns are in inches and tolerances are:
Charles Universal Broadband Enclosure WIC 101010SXAN1 General ...
Place the WIC on the pad. Loosen the slings so that all the weight is on the pad. Check that the WIC is level and properly aligned. 5. Secure the WIC to the pad using the 3/4" hex head bolts and washers (two washers per bolt). Tighten all bolts securely. 6. Once the WIC is secured, remove the slings and tagline and close the door.
PCTEL Appoints Kevin McGowan as Chief Financial Officer
BLOOMINGDALE, Ill.--(BUSINESS WIRE)--Nov. 12, 2018-- PCTEL, Inc. (Nasdaq: PCTI), a leader in Performance Critical TELecom solutions, announced today the appointment of Kevin McGowan as Vice President and Chief Financial Officer effective December 1, 2018.In this role, Mr. McGowan will oversee all financial functions for the Company, participate in business planning and strategy, and play an ...
Model 602D11/-0012 Low-cost Industrial ICP® Accelerometer Installation ...
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
Model 352C34 ACCELEROMETER Installation and Operating Manual - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
21-033470-081 (PIN) 21-033471-081 (SOCKET) Contact, Pin and Socket ...
2. Cut inner wires with foils in place to dimension shown. All wires must be cut to equal length. It may be helpful to cut one wire pair to length. Then, cut remain ing wire pair to equal length as the first wire pair. E 1. Strip individual differential pair foil shields as close to flaired cable braid as pos sible. 2.
Liquid-Nitrogen (LN2) Solutions - KAYE
Cryogenic gases like liquid nitrogen (LN 2) are crucial in the pharmaceutical and biotechnology industries, enabling the safe storage of intermediates and raw materials by preventing interactions with moisture or oxygen.LN 2 and dry ice are also used in various processes, including mixing, storage, and cryogenic cooling.. Benefits of Cryogenic Containers
SMPM Product Series Solutions Guide Catalog - Amphenol RF
www.amphenolrf.com 7 Straight Jacks – Full Detent (continued) Part Number Packaging Type Body Mount Max Frequency (GHz) Image 925-196J-51P Individual Bag Surface Mount 26.5
PC420 series installation guide - Wilcoxon Sensing Technologies
with a threaded stud. Cementing pads can be epoxied in place of the tapped hole; the transducer is then mounted to the pad. In some cases, the transducer can be mounted directly to the machine using epoxy. Cementing pads approach the capabilities of stud mounts when used properly. The following are recommended permanent mounting procedures.
Tier Rated Underground Enclosures (TRUE) | Tier 15 & Tier 22 Handhole ...
Explore Charles Industries' Tier Rated Underground Enclosures, with Tier 15 & Tier 22 handhole and load rating offering durable, secure solutions for protecting telecom equipment. Enquire Now!
Model 608A11/030BZ Low-cost Industrial ICP® Accelerometer ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
Board-Level Connectors | Products - Amphenol
Conan® Lite 1.00mm connectors come with a robust metal down feature that helps in establishing a reliable connection with the PCB in both parallel and perpendicular board-to-board applications. These connectors also feature an audible "click" sound ensuring mating in place.
Nano Pegasus - Amphenol PCDAmphenol PCD
Interconnect systems optimized for the extensive data transmissions that take place within modern missiles and guided munition systems during flight. Ruggedized products, optimized for performance and endurance in the world’s harshest environments, and engineered to achieve consistently exceptional performance.