Search Results for where is this place
Protimeter - Professional Moisture Meters & Hygrometers
Professional Moisture Meters & Accessories That Deliver . An industry leader with more than 70 years of experience, Protimeter offers innovative, dynamic, and high-performance professional moisture meters and accessories.Designed with the end-user in mind, Protimeter devices allow for accuracy, are easy to use, and are built with durable quality for everyday use.
Contact Us - Amphenol NEXUS Technologies
TTI INC. 2441 Northeast Pkwy. Fort Worth, TX 76106 Phone: 800-225-5884 Fax: 817-740-9494 Website: www.ttiinc.com
Charles Composite Pad (CPAD) Small Cell
CPAD-S3EXXXXXXX INNOVATIVE ENCLOSED SOLUTIONS™ Charles Industries, Ltd. Phone: (847) 806-6300 Fax: (847) 806-6231 Web: www.charlesindustries.com Charles Composite Pad (CPAD) Small Cell
Model 699B07 Portable Vibration Calibrator with 5-10k Hz frequency ...
Always rock the sensor in place as one would on the machine. Test the accelerometer to the maximum frequency of interest (Fmax) on the analyzer to see if response is amplified at relevant high frequencies. To create a NIST traceable calibration certificate for a vibration analyzer or meter, the following items are required:
Prevent Mechanical Warping of a PCB Connector during the Solder Reflow ...
This barb affixes the center contact in place but still allows rotation. Using Kovar/Glass materials as the dielectric prevents center contact rotation. PTFE With Barb . Kovar/Glass Target Applications. Our glass-sealed connectors are ideal for: Phased array systems; Modular systems; Communication systems; Missile guidance systems
Smart Coil DSL Line Conditioning Device - An Amphenol Company
A service provider’s legacy copper network is a major financial asset. Telephone companies place the value of a single copper pair from several hundred to over a thousand dollars. Used in conjunction with the latest digital technology, Smart Coil-equipped legacy copper pairs help not only retain but increase revenue from customers.
Thermometrics Water Detection Sensor - amphenol-sensors.com
- Place specimens at below temperature for 30 mins and then, operate for 30 mins [°C] (-40, -30, +80, +90, +100, +110, +120, +130) - Check water immersion at 5V DC Water Detection Sensor - Specifications (Cont.) 4 No. Construction List Material Notes 1 Case PBT Black 2 Bush C3604
Kaye ValProbe Temperature/Humidity Logger
The ValProbe humidity logger is designed for accurate, convenient and reliable process measurement for pharmaceutical, medical device and food processing applications.
Model 3741B1210G DC Response Accelerometer Installation and ... - PCB
2 PCB’s High Sensitivity DC accelerometers are designed utilizing a MEMS (Micro -Electro Mechanical Systems) silicon sensor approach. The micro machining design process provides sensor design flexibility, reliability &
Model 627A11 Low-cost Quartz, ICP® Industrial Accelerometer ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
Hyperbolic Contacts - Optional ATAT Series - Amphenol Sine
move out of place. FRONT SEAL The superior design ensures a tight environmental seal when used in conjunction with the recessed cavity of the connector body. RECESSED SEALING AREA The recessed cavity allows for a secure fitting front seal. ERGONOMICALLY DESIGNED CLIP The increased size and tactile design of our clips allow for easier mating and ...
Telaire T8031 CO2 duct mount sensor - amphenol-sensors.com
to place the transmitter in small, i.e. 6 inch [15.24 cm] diameter, return air ducts. This product offers a sleek design, a simple analog output, and it is easy to install. The transmitter includes mounting hardware and installation instructions. Measurement Range 0-2000 ppm factory calibrated Duct Air Velocity 0 to 1500 ft/min (0-450 meter/min)
ValProbe RT CO2 Logger - kayeinstruments.com
The 3-in-1 data logger from the Kaye ValProbe RT product line offers the capability to measure critical parameters such as CO 2 (carbon dioxide), relative humidity (RH), and temperature with a single device. For applications where these measurements are quality-critical, the Kaye ValProbe RT CO 2 Logger provides economical, accurate, and GxP-compliant recording and documentation of these ...
Model 625B21 Precision Industrial ICP® Accelerometer ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
Troubleshooting accelerometer installations - Wilcoxon Sensing Technologies
is very rare to have a short inside the sensor. The most common fault location is in junction box terminations. Check to make sure that a frayed shield is not shorting across the signal leads.
Power Safe - Amphenol Aerospace
linked to the shell, stays in place even in case of overheats. LAST MATE/FIRST BREAK: one pilot contact with a breaking capacity (brings the information to a relay to turn on/off the power). These features protects the user even if the connectors are mated or unmated. Amphenol recommends to connect / disconnect connector when unloaded.
Amphenol Aerospace
Amphenol Aerospace Page 1 of 7 01/2018 72-85-6F TERMS AND CONDITIONS OF SALE 1. APPLICABLE TERMS AND CONDITIONS: The acknowledgment of this order by the seller or commencement of any performance by the seller pursuant to this order shall constitute purchaser’s acceptance of the seller’s terms and conditions and the prices set forth
FEP Fahrzeugelektrik Pirna GmbH - fepz.de
The rapid changes currently taking place in the automotive industry are not stopping at FEP. With new future-oriented products, such as fuse boxes and other components for high voltages and currents in hybrid or fully electric vehicles, we are actively, supporting these changes and are thus optimistic about the future.
Intelligent current monitoring - Lutze Inc.
Status messages take place as optical and electrical signals for each channel separately, either as collective fault messages or on achievement of the 90 percent utilisation. The 2-channel version has a galvanically isolated remote input for the switch-on and switch-off of each channel as well as an independent adjustment of current range and ...
Kaye Calibration and Metrology Solutions
KAYE HEADQUARTERS. Amphenol Advanced Sensors Germany GmbH Sinsheimer Strasse 6 D-75179 Pforzheim. T +49 (0) 7231-14 335 0 F +49 (0) 7231-14335 29 kaye-ccpf@amphenol-sensors.com