Search Results for stealth carrier
The B-21 stealth bomber kickstarts sixth-generation military aerospace
After years spent hidden away, the next-generation aircraft of the U.S. Air Force’s long-range bomber fleet was unveiled to the public for the first time during a special ceremony late last year, marking a major milestone for the sixth generation of military aerospace.
F-22 versus F-35 - Amphenol Aerospace
The requirements for stealth, speed, advanced avionics, C4ISR, and electronic warfare mean fighter jets have more electronics on board than ever before. Electronic signals need to be protected to function properly making electromagnetic interference or EMI protection a priority.
MOSA is slated to redefine defense development and procurement
Slated to replace the U.S. Air Force’s F-22 Raptor fifth-generation fighter, the sixth-generation NGAD fighter is to be developed with the latest in stealth, weapons, and aerospace technology. Leveraging open systems is going to be critical to its development.
Defense | Markets - Amphenol
Amphenol is a world leader in the design, manufacture and supply of high-performance interconnect systems for harsh environment defense applications including vibration, pressure, humidity, nuclear radiation and severe temperature changes.
2L6U4VX065X06Fwxys4 - Amphenol Antenna Solutions
Panel, 2FT, 24-Port, 65°, (2x) 617-906 | (6x) 1695-2700 | (4x) 3300-4200 MHz, Fixed Tilt
Lockheed Martin to have hypersonic missile launcher ready for flight ...
Lockheed plans to develop the launcher for the Zumwalt-class destroyer — the Navy’s advanced stealth destroyer that was commissioned in 2016. The Navy plans to have its three Zumwalt ships retrofitted into sea-based hypersonic missile platforms under its Conventional Prompt Strike (CPS) hypersonic program.
ST61 Transom Mount - Airmar
The ST61 consists of a paddlewheel speed carrier that snaps into a small transom housing containing sensing electronics. This standalone unit gives accurate speed readings over a wide speed range.
Pole Side Radio Concealment Shrouds | Small Cell Concealment Shrouds ...
Charles Industries’ pole side radio concealment shrouds offer aesthetically-pleasing concealment of radios and remote equipment at small cell, densification, and DAS remote sites.
The Brain of Modern Vehicles: Understanding Car Computing
At the core of car computing lies the Central Computing Unit, often referred to as the vehicle's brain. This pivotal component is responsible for aggregating and integrating a myriad of electronic systems, ensuring that every aspect of the vehicle operates in harmony.
Military and Commercial Air Electrification: Part 2 — Advancing Toward ...
Electrically powered vehicles and aircraft could also operate with lower acoustic and thermal signatures that bring tactical advantages in stealth and survivability, which would be of particular benefit to warfighters.
South Korea to purchase more F-35A aircraft - Amphenol Aerospace
South Korea plans to purchase an additional 20 F-35A Lightning II stealth fighters to bolster its current fleet. The $2.9 billion purchase will bring South Korea’s F-35 fleet to about 60 fighters with the planes expected to be procured by 2028.
Low-Profile Whipless Cellular Antennas - PCTEL
These low profile whipless antennas are purpose built for applications requiring reliable cellular connectivity. Learn more about the low-profile, whipless cellular antennas from PCTEL that provide superior pattern coverage for 2G-5G, LTE, & CBRS communications.
How MIL-DTL-38999 has Advanced Military Technology
MIL-DTL-38999 incorporates integrated shielding features that provide significant protection against EMI and RFI, including built-in shielding around individual contacts and overall connector shielding.
Military and Commercial Air Electrification: Part 1 — Harnessing Hybrid ...
Harsh environment applications across the military and commercial air landscape are slated to undergo a major transformation. Electrification is coming, and the technology is advancing rapidly. Its potential is receiving a lot of hype throughout various industries, and for good reason.
Quad-Channel 160 MSPS PDS-268 14-bit Analog Input A/D Connector ...
PS to 160-MSPS, analog-to-digital CLOCKS, TRIGGERS, converter & SYNCHRONIZATION (ADC). The devices are designed The ADC-4CH-160M-14-F specifically to sample support clock demanding, can be driven high from input either frequency an external source signals.
U.S. Army to test tactical vehicle system tech on AMPV armored ...
The U.S. Army expects to conduct testing of a tactical vehicle-based system on its AMPV armored personnel carrier next year that’s designed to provide vehicle occupants with advanced situational awareness.
Airbus receives 500-aircraft A320 order with Indian low-cost carrier ...
Airbus has received an order for 500 A320 aircraft from Indian low-cost airline IndiGo in what is the largest order in commercial aviation history by quantity. The news was announced during the first day of this year’s Paris Air Show on June 19. The aircraft are expected to be delivered between 2030 and 2035.
Boeing reaches deal with Ethiopian Airlines for up to 67 passenger ...
The agreement with the Ethiopian flag carrier features an order for 11 of the 787-9 Dreamliner models and 20 of the 737-8 MAX models, with an opportunity for 15 and 21 additional jets, respectively. The 206-foot 787-9 can seat 296 passengers and has a range of 7,565 nautical miles (14,010 kilometers).
Air Canada orders 18 Boeing 787-10 Dreamliners
Canadian flag carrier Air Canada has placed an order with Boeing for 18 787-10 Dreamliner aircraft. The order includes an option for 12 additional aircraft at a later date. Deliveries of the aircraft are expected to begin in late 2025. The 787-10 is the largest of Boeing’s line of 787 jetliners.
Vietnam Airlines orders 50 Boeing 737 MAX aircraft
Vietnam Airlines and Boeing have reached a deal for the Vietnamese flag carrier to acquire 50 Boeing 737 MAX-8 aircraft. The deal is valued at $7.8 billion. The MAX 8 planes are expected to eventually phase out older aircraft in the carrier’s fleet.