Search Results for absolute linux
Unmanned Aerial Vehicle (UAV) - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Temperature Sensors | Temperature Sensor Assemblies
Thermometrics Pressure & Temperature Combination Sensor provides both pressure and temperature measurements in one sensor assembly. For reliable and accurate measurements, the sensor utilizes NTC thermistor technology for temperature sensing alongside silicon-based Microelectromechanical Systems (MEMS) technology for absolute pressure sensing.
Voltage Compensated, Media Isolated, High Pressure Sensors
in absolute or sealed gage • Standard configurations include: —1/2–20 UNF threaded male port with 1.0 in (24.4 mm) flange —0.59 in (14.98 mm) diameter x 0.87 in (22.09 mm) long cylinder with o-ring seals —1/4–18 NPT male port with 7/8 in flange —1/8–27 NPT male port with 7/8 in flange • Custom configurations and other pressure
MEASURING MECHANICAL & PYRO SHOCK - pcb.com
2 1. Introduction to the Measurement of Shock n Brief introduction into the topic 2. Accelerometer Types Used for Shock n Key technology choices including sensing type (PR & ICP®), mechanical isolation, and onboard analog filtering 3. Cables and Interconnects n How cables can add unwanted noise and lowpass filtering effects, and how to avoid this 4. Signal Condition
Temposonics
For position measurement, the absolute, linear Temposonics® position sensors make use of the properties offered by the specially designed magnetostrictive waveguide. Inside the sensor a torsional strain pulse is induced in the waveguide by momentary interaction of two magnetic fields. The interaction between these two magnetic fields produces
NovaSensor P111 Medium Silicon Pressure Sensor Die
1. 0 KPaA for absolute sensors, 0 KPaG for differential or gage sensors. 2. Best fit straight line. 3. Between 32°F and 158°F (0°C and 70°C). 4. Typical value over one year. 5. All values measured at 77°F (25°C) and 1 mA excitation, unless otherwise noted. Shipping and Handling All wafers are shipped in protective containers. The wafers ...
Product Brief Temposonics
Absolute, Non-contact Position Sensors MH-Series Model MT Product Focus SENSORS ® Redundant sensor designed for in-cylinder position feedback in off-highway equipment. MTS Sensors, a division of MTS Systems Corporation, is the global leader in the development and production of linear-position and liquid-level sensors. Based
Data Sheet R-Series V RF5 EtherCAT - temposonics.com
The absolute, linear position sensors provided by Temposonics rely on the company’s proprietary magnetostrictive technology, which can determine position with a high level of precision and robustness. Each Temposonics® position sensor consists of a ferromagnetic waveguide, a position magnet, a strain pulse converter and supporting electronics.
Amphenol MP-64RJ4528GB-001 Slim Category-6 Ethernet Cable (Thin CAT6 ...
Buy 1ft Amphenol MP-64RJ4528GB-001 Thin-Line CAT-6 Ethernet Cables Direct from the Factory at Cables on Demand. Amphenol's NEW 28-AWG Slim Category-6 Ethernet Cables (Thin CAT6) Network Patch Cords (Color: Blue) are designed with a dramatic reduction of cable diameter (over 33%), enabling IT professionals improved cable routing flexibility and enhanced airflow in today's high-density server ...
RaptorLink 64X50 SOSA Ethernet Switch | Ethernet Switches | Products ...
• Linux OS with comprehensive network management software. RUGGEDIZATION • Fully ruggedized to withstand extreme environmental and EMI/EMP conditions. • Interfaces for power diagnostics and more. • Meets the following environmental specifications: • Operating Temperature: -40ºC to 85ºC while operating.
ChipCap 2 humidity and temperature sensor - amphenol-sensors.com
Capacitive polymer RH Sensor, PTA (Proportional to Absolute) Temperature sensor integrated ASIC chip in LCC (Leadless Chip Carrier) package, SMD, RoHS compliant Parameter Min Max Supply Voltage (VDD) -0.3V 6.0V Storage Temp (Tstrg) -55°C 150°C Junction Temp (Tj) -55°C 150°C.
Data Sheet - Temposonics
The absolute, linear position sensors provided by Temposonics rely on the company’s proprietary magnetostrictive technology, which can determine position with a high level of precision and robustness. Each Temposonics® position sensor consists of a ferromagnetic waveguide, a position magnet, a strain pulse converter and a supporting electronics.
SGX - SGX Sensortech Sensor
Head office. Switzerland, Courtils 1, 2035 Corcelles-Cormondreche +41 (0) 32 732 16 70. contact@sgxsensortech.com
Amphenol All Sensors Products | All Sensors
Pressure Type: Absolute. Pressure Min: 0. Pressure Max: 100. Units: PSI. Operating Temperature:-25 to 85 C. Supply Voltage: 5 VS. Honeywell PN: Supply Voltage: 5 VS. Download Data Sheet Contact our Team of Experts Today. Contact Us Home Products Solutions About ...
T RSERIES - temposonics.com
between an absolute position sensor and a controller. SSI uses a clock pulse train from a controller to initiate a gated out-put from the sensor. A clock pulse train from a controller is used to gate out sensor data: one bit of position data is transmitted to the con-troller per one clock pulse received by the sensor. The absolute position data ...
Thermopile IR Detectors and Their Uses
Thermopile IR Detectors and Their Uses
Data Sheet E-Series ER Analog - temposonics.com
The absolute, linear position sensors provided by Temposonics rely on the company’s proprietary magnetostrictive technology, which can determine position with a high level of precision and robustness. Each Temposonics® position sensor consists of a ferromagnetic waveguide, a position magnet, a strain pulse converter and supporting electronics.
Data Sheet E-Series ER IO-Link - Temposonics
The absolute, linear position sensors provided by Temposonics rely on the company’s proprietary magnetostrictive technology, which can determine position with a high level of precision and robustness. Each Temposonics position sensor consists of a ferromagnetic waveguide, a position magnet, a strain pulse converter and a supporting electronics.
LiNC™ - Amphenol Broadband Solutions
LiNC™ is Amphenol’s revolutionary rapid-deployment multi-fiber end- to-end solution. LiNC consists of our streamlined 1RU 19/23” rack/ cabinet mount LiNC chassis, up to four 12 or 24 fiber LiNC MPO breakout modules, and the time-saving option of ready-to-use 12/24F MPO-MPO factory integrated spooled trunk cables, with up to 200 feet of fiber for rapid deployment.
Rugged SOM | Super Small Form Switches - Products | Amphenol Aerospace
Rugged SOM runs a custom distro of embedded Linux and can be accessed via the onboard UART serial port, RS485/422 serial port or USB port in device mode. Features & Benefits: Documents Request Quote. Rugged SOM Product Datasheet Rugged SOM - Ultra-Compact Embedded Computer Module View Download. First Name. Last Name ...