Search Results for airmar
SS175H Chirp-ready Tilted Element Thru-hull - Airmar
1 kW. Airmar’s low-profile, Chirp-ready, transducer models are the perfect addition to smaller boats such as center consoles. The high-frequency band, transmitting between 130 and 210 kHz, has a narrow beamwidth—excellent for pinpointing fish holding tight to wrecks, reefs, and other structures.
110WXS WeatherStation® Instrument - Airmar
Solar-radiation Shield. The model 110WXS is Airmar’s entry-level solution for land-based, stationary, weather-monitoring applications. A complete multisensor WeatherStation, the 110WXS features a solar-radiation shield for increased accuracy and stability of temperature and relative humidity readings.
SmartFlex Diesel Flow Meter, 80-4000 LPH, Single-Chamber, Alloy housing ...
SmartFlex Single-Chamber Diesel Fuel Flow Meter. The SmartFlex ™ single-chamber flow meters are designed for fuel consumption measurement of diesel engine systems with flow rates up to 4,000 L/h. Single-chamber models can be synched with other single-chamber DFMs (feed and return) for calculated fuel burn/consumption data for display on multi-function displays or Signal K interfaces.
ARK41 Airducer® Ultrasonic Transducer - Airmar
The ultrasonic ARK41 brings proven dependability to level, flow and distance measurement applications. Its rugged one-piece Kynar PVDF housing makes it suitable for chemically aggressive environments.
300WX-IPX7 WeatherStation® Instrument - Airmar
Features. New Features of the 300WX WeatherStation Instruments: New communication protocols – J1939, ISOBUS; Wireless connectivity via Bluetooth to Airmar’s CAST app for viewing instrument data, system configurations and firmware updates
B122 Smart™ Sensor Thru-hull - Airmar
100 W. The B122 has an extra-long housing designed for use in thick-hulled, wooden boats or vessels with a steep deadrise. The included High-performance Fairing vertically orients the beam for strong return echoes, resulting in optimal performance even at higher speeds.
Process Improvement Coordinator - Airmar
Explore exciting career opportunities at Airmar, a leading company. Join us as a Process Improvement Coordinator and contribute to our innovative culture. Discover a fulfilling career where your skills make a difference. Apply now!
Commercial - MSI Transducers
MSI is a global leader in the design and development of commercial transducers and arrays for more than 30 years. However, meeting the cost needs of this market was always a challenging obstacle for MSI to hurdle, until MSI was acquired by Airmar Technology Corporation.
ST800 Speed/Temperature Sensor Bronze Thru-hull Analog - Airmar
The ST850/800 is an analog, retractable speed and temperature sensor. The sensor fits inside a low profile, bronze thru hull housing that is nearly flush to the hull, with only 5 mm (3/16”) extending outside of the hull.
ATK120 Airducer® Ultrasonic Transducer - Airmar
Non-contact level, flow, distance, proximity and object detection measurement is reliably delivered by the ultrasonic ATK120. Its rugged one-piece Kynar PVDF housing makes it suitable for the most chemically aggressive environments.
AIRMAR - Production Technician I
Embark on a fulfilling career journey as a Production Technician I at Airmar Technology Corporation. Discover opportunities to grow your skills and make a meaningful impact in the dynamic world of marine and industrial sensor technology.
B285HW Chirp-ready Thru-hull - Airmar
1 kW. Get more coverage under your boat with Airmar’s unique, wide-beam, high-frequency, Chirp-ready B285HW. The high-frequency band operates across a range of 150 to 250 kHz and has a fixed 25° beam for all frequencies.
Smart Modules - Airmar
SmartBoat - Bridge Only, No Analog Inputs, W/ CAN2 and Serial. Learn More. SmartBoat Wire Block - 2 Position, Screw Terminals
Transducer Identification - Airmar
AIRMAR ISO Certification (PDF Download) Supplier Change Notification (PDF Download) Supplier Corrective Action Request (PDF Download) Supplier Quality Support Manual (PDF) DISCOVER. Videos. What is XID? AIRMAR Certified Installers. Installer Finder. WeatherStationWX.com
MSI Technical Program Manager - Airmar
Join MSI Transducer Corporation as a Technical Program Manager in Littleton, MA! Lead development efforts for complex electro-mechanical sonar assemblies from concept to completion. Ideal for engineers with a background in acoustics, program management experience, and a knack for cross-functional teamwork. Apply now to drive innovation in defense and commercial applications!
M194 Survey Transducer - Airmar
Airmar’s commitment to innovative technology has produced the M194. This broadband, 200 kHz transducer has a Q of 2 and very good sensitivity.
UST850 Smart™ Sensor Thru-hull NMEA 2000® - Airmar
Airmar’s patented UST850 just turned your maintenance time into more cruising time—and made your boat smarter too. Get ultrasonic speed and temperature in a single thru-hull housing with no moving parts.This sensor is a high-precision, low-maintenance solution for use on power and sail boats of all types and sizes.
AIRMAR - Configuration Project Engineer
Join our dynamic team at AIRMAR! As a key member collaborating with the Configuration Engineering team, you'll play a vital role in managing projects and developing part configurations for new and existing products. With 2-3 years of manufacturing or equivalent experience, coupled with a Bachelor’s in business administration or a technical degree, you'll oversee new part development and ...
B785M Chirp-ready Thru-hull - Airmar
600 W. The B785M is an economical, Chirp-ready transducer designed for offshore fishing and freshwater anglers. Operating at a frequency range of 80 to 130 kHz, this transducer reveals fish in shallow, murky waters at medium depths up to 274 m (900') along with ultra-clear target resolution.
DST810 Smart™ Multisensor - Airmar
NOTE: AIRMAR HAS REPLACED THIS PRODUCT WITH THE DST810 SMART ™ MULTISENSOR WITH GEN2 PADDLEWHEEL. Depth, Speed-Through-Water, Water Temperature, Boat Attitude. The new DST810 Smart Multisensor, featuring the new Gen2 paddlewheel and AIRMAR's CAST ™ app, delivers a powerful combination of best-in-class speed performance and a simple, reliable way to calibrate accurate speed using your ...