Search Results for amphenol corporation completes acquisition of commscope
CRIMP TERMINATION FOR TYPE 2 – 75ΩCONNECTORS
Amphenol Corporation Tel: 800-627-7100 www.amphenolrf.com Assembly CRIMP TERMINATION FOR TYPE 2 – 75ΩCONNECTORS Step 1 Strip cable jacket, braid, and dielectric to dimensions in table above. [for RG-62,71,210/U cable, trim an additional .039"(1.0mm) of insulation off center conductor and add bushing] All cuts are to be sharp and square.
Amphenol Supplier Responsible Labor Policy (EN)
Amphenol is committed to respecting human rights in our global operations and supply chain. This Supplier Responsible Labor Policy sets forth standards to ensure that supplier working conditions are safe and that workers are treated with dignity and respect.
Amphenol Amphenol Taiwan Corporation Sheet 1
This document is the property of Amphenol Corporation and is delivered on the express condition that it is not to be disclosed reproduced or used, in whole or in part, for manufactu re or sale by anyone other than Amphenol Corporation wi thout its prior consent, and that no right is granted to disclose or to use any information in this document
Amphenol Assembletech
Amphenol Corporation was founded in 1932,It is one of the largest manufacturers of interconnect products in the world. The Company has been actived in China since 1984, and was listed on the New York Stock Exchange in 1991. As an excellent listed company on the NYSE, Amphenol ranked 54th of the TOP 100 of the World's Best Performance ...
employment | Amphenol Global Search | Amphenol
KAYE HEADQUARTERS. Amphenol Advanced Sensors Germany GmbH Sinsheimer Strasse 6 D-75179 Pforzheim. T +49 (0) 7231-14 335 0 F +49 (0) 7231-14335 29 kaye-ccpf@amphenol-sensors.com
fc connectors | Amphenol Global Search | Amphenol
Model 1203-12A/084A100:PCB L&T load cell, low profile, 1000 lbf rated capacity, 50% overload protection, 2mV/V output 5/8-18 UNF-2B thread, PTO2E-10-6P
BDO Series for Fiber Access Terminals - Charles Industries, LLC
12" dia. pedestal, mounting bracket accommodates Charles FSDC or CFIT-SL, Commscope OFDC or OTE-300, or various fiber terminal blocks. UMB102A. Universal Pole Mount Bracket w/hardware. UMS36-STD. 36” Metal Mounting Stake w/hardware. ... About Amphenol ©2025 Charles Industries, LLC.
About Us - Amphenol PCDAmphenol PCD
Amphenol Corporation, founded in 1932, is one of the largest manufacturers of interconnect products in the world and is the leading supplier in the Military-Aerospace application market. Amphenol Corporation has the ability to design, manufacture, and market a vast array of products. These products include: electrical, electronic, and fiber ...
About us - Amphenol Ltd
As part of the Amphenol Corporation, we offer a broad portfolio of cutting-edge technical solutions that enable both existing and future innovative applications. About Amphenol Corporation Amphenol Corporation is one of the world’s largest designers and manufacturers of interconnect systems, including electrical, fibre optic, antennas ...
Code of Business Conduct and Ethics - Amphenol Invotec
AMPHENOL CORPORATION CODE OF BUSINESS CONDUCT AND ETHICS Amphenol consists of companies located around the globe with one common goal – to be the best that we can be. Amphenol’s reputation is one of our most important assets. This reputation has been, in large measure, earned through the honesty and integrity of our employees, officers and
Broadband | Markets - Amphenol
AFSI’s line of 109 series hermaphroditic connectors offers the ultimate in flexibility and is a direct replacement for the TAC4. The 109 connector line meets or exceeds the pertinent requirements of SMPTE standard 358M on harsh environment multi-channel fiber optic connectors suitable for deployment in demanding outdoor broadcast applications, including HDTV signal transmission.
Assembly Instructions-C1 Amphenol UHF
Amphenol Corporation Tel: 800-627-7100 www.amphenolrf.com UG STANDARD SOLDER TYPE PLUGS 83-1SP, 83-1SP-1050, 83-1SP-15RFX, 83-822 Step 1 Step 2 Step 3 Step 1 Slide coupling ring onto cable. Cut end of cable even and strip jacket, braid and dielectric to dimensions shown in table . All cuts are to be sharp and square.
Amphenol Network Solutions > WaveTrax—A sturdy, rigid cable raceway ...
The snap-together WaveTrax overhead cable raceway system from Amphenol Telect reduces time spent on installations and retrofits. The Mighty Clamp Trough Support Clamp holds up WaveTrax trough along a horizontal fiber raceway. ... - CommScope's FiberGuide® to WaveTrax® Cross Reference - Installation Guide - Ordering Guide - Panduit Cross ...
Amphenol RF
amphenol rf www.amphenolrf.com date 2/1/90 engineer d royce material see notes date 20-jun-12 drawn eric wankoff finish drawing no. 31-5431 item no. 31-5431 part no. 31-5431 notes: 1. materials and finishes: body - zinc die cast, nickel plating contact - phosphor bronze, gold plating (.000003 thick) @ contact area only, tin plating at tail ...
L-725.pmd - Amphenol Aerospace
diameters for each connector shell size. Amphenol catalogs are available on-line at www.amphenol-aerospace.com or www.amphenol-industrial.com. NOTE: See torque value notes (6, 7, 8) following Table I for accessories having three threads or less. 6. The torque values listed in Table I are for UN (Handbook H-28) threads.
Amphenol DC Electronics Expands to Mexico - DC Electronics
San Jose, Calif., December 23, 2013 – Amphenol DC Electronics (ADCE), a division of Amphenol Industrial Global Operations Group (NYSE: APH) today announced the opening of a new, state of the art manufacturing facility in Nogales, Mexico. The 30,000 square foot facility was designed to be a near mirror image of ADCEs Silicon Valley facility.
Micro Connectors - Amphenol Canada
Amphenol Micro Connectors provide small inter-connect solutions, which will exceed the requirements of the US military standard M83513. What differentiates Amphenol from the competition is our overall connector design. Custom solutions can easily be engineered to ensure exact performance in any application.
Declaration of Conformity to RoHS
This declaration of conformity is issued under the sole responsibility of Amphenol RF. This is to certify that the part/product listed above are in conformance with the EU Directive 2011/65/EU as amended by (EU)2015/863. The following table lists the restricted materials and their respective allowable limits: RoHS Restricted Substance Allowable ...
Backshells, Strain Reliefs, Caps, Dummy Receptacles - Amphenol ...
Amphenol offers a complete collection of backshells, protective caps, and other accessories for all of our D38999 connectors. Custom solutions are available upon request. Consult an Amphenol Representative for more information.
Commitment To Quality - Amphenol RF
Amphenol is committed to creating a more sustainable manufacturing presence throughout our factories. Our manufacturing locations now use more natural light to minimize the use of electric lighting, we have installed water fill stations to encourage the use of reusable water bottles and our product packaging has been redesigned to minimize water and improve customer usability.