Search Results for concentration of measure
2 Sensor for Automotive Applications - Amphenol
Accuracy and Measurement Range: • 400 to 5,000 ppm CO2: +/-200 ppm • 5,000 ppm to 4% CO2: +/- 10% of the reading • 4% to 6.5%: accuracy not specified • Temperature Dependence (outside 0C to 50C): +/- 0.5% of the reading Measurement and Sample Rate Characteristics: • Active Mode: 5 seconds sample rate
Telaire CO2 Zone Ventilation Control In Buildings Application Note
ventilation measurement described in ASTM Guide Standard D6248-98, considers the CO 2 concentration difference between inside and outside. Inside CO 2 levels are a dynamic measure of the number of people in the space exhaling CO 2 and mixing with the amount of lower CO 2 concentration air introduced from outside for ventilation.
Telaire CO2 Zone Ventilation Control In Buildings Application Note
ventilation measurement described in ASTM Guide Standard D6248-98, considers the CO 2 concentration difference between inside and outside. Inside CO 2 levels are a dynamic measure of the number of people in the space exhaling CO 2 and mixing with the amount of lower CO 2 concentration air introduced from outside for ventilation.
Vibration Sensors - Amphenol Sensors
Vibration Sensors Vibration Sensors: Wilcoxon Sensing Technologies Wilcoxon Sensing Technologies has a strong legacy of success in vibration monitoring with hundreds of thousands of sensors currently in service around the world. Built for long use and excellent performance, our high quality accelerometers, 4-20 mA sensors, transmitters and instrumentation provide accurate and reliable ...
Telaire CO2 Zone Ventilation Control In Buildings Application Note
ventilation measurement described in ASTM Guide Standard D6248-98, considers the CO 2 concentration difference between inside and outside. Inside CO 2 levels are a dynamic measure of the number of people in the space exhaling CO 2 and mixing with the amount of lower CO 2 concentration air introduced from outside for ventilation.
2 Sensor for Automotive Applications - Amphenol
Accuracy and Measurement Range: • 400 to 5,000 ppm CO2: +/-200 ppm • 5,000 ppm to 4% CO2: +/- 10% of the reading • 4% to 6.5%: accuracy not specified • Temperature Dependence (outside 0C to 50C): +/- 0.5% of the reading Measurement and Sample Rate Characteristics: • Active Mode: 5 seconds sample rate
Test Results and Alternate Packaging of MEMS 2008 Fuze Conf #6520 - PCB
Uniformity of concentration thus reduces both ZMO and TZS. The tension and compression gauges on the legacy sensor are on opposite faces of the ... independent measure of acceleration. That value was overlaid in the graphs, to be compared to that measured by the accelerometers. -30000-20000-10000 0 10000 20000 30000
Thermometrics TST-10 Turbidity Sensor - amphenol-sensors.com
or an extraneous matter concentration using the refraction of wavelength between photo transistor and diode. By using an optical transistor and optical diodes, an optical washing machine sensor measures the amount of light coming from the source of the light to the light receiver, in order to calculate water turbidity. Amphenol Advanced Sensors
Telaire CO2 Zone Ventilation Control In Buildings Application Note
ventilation measurement described in ASTM Guide Standard D6248-98, considers the CO 2 concentration difference between inside and outside. Inside CO 2 levels are a dynamic measure of the number of people in the space exhaling CO 2 and mixing with the amount of lower CO 2 concentration air introduced from outside for ventilation.
Telaire CO2 Zone Ventilation Control In Buildings Application Note
ventilation measurement described in ASTM Guide Standard D6248-98, considers the CO 2 concentration difference between inside and outside. Inside CO 2 levels are a dynamic measure of the number of people in the space exhaling CO 2 and mixing with the amount of lower CO 2 concentration air introduced from outside for ventilation.
Frequently Asked Questions for MiCS Gas Sensors
terms of temperature, humidity and gas concentration. Once the set of calibration parameters is obtained, the data can be interpreted using polynomials or curve fitting techniques. For some applications where accurate absolute measurement is required, a periodic recalibration is recommended. Other applications where less precision is
Telaire CO2 Zone Ventilation Control In Buildings Application Note
ventilation measurement described in ASTM Guide Standard D6248-98, considers the CO 2 concentration difference between inside and outside. Inside CO 2 levels are a dynamic measure of the number of people in the space exhaling CO 2 and mixing with the amount of lower CO 2 concentration air introduced from outside for ventilation.
Automotive Sensor Solutions | Amphenol Advanced Sensors
Amphenol Advanced Sensors is a leading innovator in automotive and EV sensor technologies and measurement solutions. Offering the most diverse sensor portfolio of standard and customized products for the world’s most demanding regulatory and industry-driven applications, Amphenol creates value by providing critical information for real-time decisions.
2 Sensor for Automotive Applications - amphenol-sensors.com
• Factory-calibrated to measure CO2 concentration levels up to 5,000 ppm. • Adjustable firmware variables • Custom packaging options • Subject to commercial consideration, customization of firmware, connector and enclosure is possible The Telaire Internal Carbon Dioxide (CO2) Sensor is a nondispersive infrared (NDIR) CO2 sensor that
MINITEK TM Header SMT HORIZONTAL JM COMPAGNON 11 Jan 2011 - Amphenol CS
c. Salt concentration : solution 5% weight d. Specific treatment: The measurement shall be conducted after the mated conductor is mildly rinsed in running water to remove deposition of salt, followed by natural drying by placing it for 24 hours at room temperature. 6.7 Resistance to solder heat for Pb Free connectors a. GS-22-012 b.
Industrial Applications | Outdoor Air
All units are factory calibrated to measure CO2 concentration levels up to 5000 ppm. Telaire T6703 Series | Miniature CO2 Sensor Modules. Telaire T6703 Series of CO2 Modules is ideal for applications where CO2 levels need to be measured to assess indoor air quality, such as residential applications. All units are factory-calibrated to measure ...
l Sensors Division Temposonics Intrinsically Safe Position Sensors
4 3. HOW TO ORDER SYSTEM COMPONENTS 3.1 Temposonics Intrinsically Safe Position Sensor Enclosure Style 1 = Standard, dust-tight (similar to NEMA 1) 2 = Ruggedized, dust-tight (similar to NEMA 1) 3 = Ruggedized, splash-proof (similar to NEMA 4) Stroke Length Units U = U.S. Customary (inches and tenth -- xxx.x inches) M = Metric (millimeters) Stroke Length The value to enter depends on stroke ...
SGX - SGX Sensortech Sensor
Through the diffusion holes, the gas reaches the sensor's working electrode, where an electrochemical reaction takes place at the so-called 3-phase boundary. A current signal is generated at the output, which is linearly proportional to the gas concentration. Key applications • Gas measurement equipment • Environmental air monitoring