Search Results for concentration of measure
Telemetry Sensors
Accumetrics Accumetrics, Inc., offers digital telemetry systems used in a wide variety of applications from aerospace to power generation. Systems transmit sensor data from rotating structures using wireless techniques. Measurement solutions range from single channel solutions, measuring torque, temperature or voltage, to advanced rotor ground fault detection systems. View Website
Thermal Validation - Amphenol Sensors
Thermal Validation Kaye The Kaye product range is relied upon by the world’s leading pharmaceutical and biotechnology companies to validate and monitor critical assets and processes, such as sterilization, as required by governing regulatory bodies. Kaye products are designed to meet the most demanding requirements for process improvement, thermal validation and environmental monitoring ...
About - Amphenol Sensors
Where Innovation Thrives Amphenol Sensors is a leader in innovative sensor technologies and forward-thinking measurement solutions built for a large variety of industries. We create value by providing critical information for real-time decisions. We offer domain expertise, rapid customization, world-class manufacturing capabilities and lasting customer relationships. We strive to give our ...
Automotive - Amphenol Sensors
Amphenol Sensors is a leading innovator in sensor technologies and measurement solutions. Offering the most diverse sensor portfolio of standard and customized products for the world’s most demanding regulatory and industry-driven applications, Amphenol creates value by providing critical information for real-time decisions.
Industrial Applications | Room Monitoring
All units are factory calibrated to measure CO2 concentration levels up to 5000 ppm. Telaire T6703 Series | Miniature CO2 Sensor Modules. Telaire T6703 Series of CO2 Modules is ideal for applications where CO2 levels need to be measured to assess indoor air quality, such as residential applications. All units are factory-calibrated to measure ...
Datasheet - SGX Sensortech
H2 Concentration range CO detection Pollution level from 0 to 10 Based on CO concentration Accuracy H2 vol.% in air ≤ 4% : ± 0.4 vol.% H2 ... The sensor must be exposed to measure the air from thebatterypackonly. Preferably, the filtering membrane included in the module should be facing downward. If this is not possible, it should be
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
Temperature Sensors - Amphenol Sensors
Thermometrics, Inc. With more than 70 years of experience in the development, design and manufacture of high quality sensors, Thermometrics offers one of the most comprehensive ranges of temperature measurement and sensor products in the world today – NTC Thermistors, PTC Thermistors, Infrared (IR) Sensors, Current Limiters, Temperature Standards, and Temperature Sensor Assemblies. View ...
Product Spotlights | Amphenol Advanced Sensors
Indoor agricultural facilities and greenhouses require proper environmental conditions for optimal plant growth and health. Most critical to productivity, quality, and energy conservation are the monitoring and control of carbon dioxide (CO2) concentration in combination with temperature, humidity, and ambient light. Read on to learn more.
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
Ultrasonic Sensors - Amphenol Sensors
Celebrating 40 years of custom sensor design and manufacturing, SSI utilizes patented ultrasonic technology along with piezoresistive and hall effect technologies to produce standard and custom ultrasonic level, concentration, speed and pressure sensors for the automotive, industrial and consumer markets.
Telaire ABCLogic Self Calibration Feature Application Note
to measure and control for ventilation, it is most important to consider not the absolute ppm levels, but the differential concentration between inside and outside concentrations. In general terms, the higher the differential, the lower the ventilation rate. One of the additional benefits of ABCLogic is that the sensor
Coolant Temperature Sensor - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
SGX - Sensor Selector
SGX Sensortech - Filter Sensors. Module VOC. Range VOC 0-1000 ppb, Range Equivalent CO2 400-2000 ppm
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
SC-SFV08 PRODUCT SPECIFICATION - Amphenol CS
1)Measure contact resistance before and after the test according to the method in clause 9-1-1 by using accommodated conductor specified in clause 5. 2) Salt solution concentration : 5% 3) Period of exposure : 48 hours 4) Expose conductor and connector in mated condition and leave them under normal temperature after posttreatment. (24 hours)
Automotive Sensors | HVAC
Telaire T6615 is a Dual Channel CO2 Sensor Module designed to integrate into existing controls and equipment for use in instumentation and applications up to 50,000 ppm. Dual channels consist of one CO2 channel that measures gas concentration and one reference channel that measures the sensor signal intensity.
Military - Amphenol Sensors
Amphenol Sensors is a leading innovator in sensor technologies and measurement solutions. Offering the most diverse sensor portfolio of standard and customized products for the world’s most demanding regulatory and industry-driven applications, Amphenol creates value by providing critical information for real-time decisions.