Search Results for concentration of measure
SSI Technologies, LLC
Pressure measurement technology translates force from an induced pressure into an electrical signal. SSI's family of pressure sensors use piezoresistive technology for its sensor signal processing to measure pressure. SSI Technologies, LLC full line of Pressure Sensors is sure to fit your automotive, industrial or commercial application needs.
Test Results and Alternate Packaging - PCB
Uniformity of concentration thus reduces both ZMO and TZS. The tension and compression gauges on the legacy sensor are on opposite faces of the ... independent measure of acceleration. That value was overlaid in the graphs, to be compared to that measured by the accelerometers. -30000-20000-10000 0 10000 20000 30000
Kaye Calibration and Metrology Solutions
The precise measurement and documentation of critical process parameters are essential in many industries and are defined by a series of norms and standards in the ISO 9000 environment. ... CO2 Concentration; These measurement variables are critical in various applications of pharmaceutical manufacturing and storage and are heavily regulated by ...
Vibration, Pressure & Mems Sensors - Amphenol Sensors
Vibration, Pressure, and Mems Sensors Endevco Endevco provides a complete range of dynamic test and measurement sensor solutions, including piezoelectric and MEMS accelerometers, shock sensors, miniature pressure transducers, signal conditioners, cables, and accessories. Our brand is known for providing high reliability products for a wide range of testing applications, including automotive ...
NO - SGX Sensortech
Concentration [ppm] 0 Hydrogen NO NO2 RED sensor, continuous power ON, 25°C, 50% RH OX sensor, continuous power ON, 25°C, 50% RH 0.01 0.10 1.00 10.00 ... MiCS-4514 with measurement circuit (top view) The two voltages measured on the load resistors are directly linked to the resistances of the RED and OX sensors
Thermal Runaway Sensor - amphenol-sensors.com
Gas Concentration % %PPM Output Voltage Range@3.3Vcc Symbol Value Unit Value Unit Symbol Value Unit Min H_in,1 0 % 0 ppm V_out,1 0.33 V Max H_in,2 16 ... Measurement Time T[m] 55 60 65 ms 1. Default shown in typ. value, Min and Max show configurable limits. Sample Rate is defined
Industrial Sensors for Consumer Electronics
All units are factory calibrated to measure CO2 concentration levels up to 5000 ppm. Telaire T6703 Series | Miniature CO2 Sensor Modules. Telaire T6703 Series of CO2 Modules is ideal for applications where CO2 levels need to be measured to assess indoor air quality, such as residential applications. All units are factory-calibrated to measure ...
TULC Sensor
SSI Technologies Controls Technologies Division. SSI Technologies, LLC introduces our TULC Sensor, an in-tank combination sensor for accurate, reliable measurement of temperature, level, and fluid quality/concentration, for SCR Diesel Exhaust Fluid (DEF) tanks to meet legislated mandates for cleaner diesel emissions.
Temposonics
Through continuos measurement, it is . always known how much fluid is in the containers. This enables continuous reloading without interruption of the analysis and anticipatory planning. Increased dosing accuracy, reduced consumption The dosing accuracy during preparation of damping solution and precise control of the IPA concentration are of
Wireless - Amphenol Sensors
Combined Pressure & Temperature Sensors i2s i2s is your contact for the development and production of pressure sensors, temperature sensors, mass air flow sensors, as well as combination sensors for several measurands. Customers from the automotive, commercial vehicle, mechanical engineering and metrology industries have been relying on our experience and know-how for more than 15 […]
Telaire T6743 Automotive CO2 Sensor - Amphenol
• All units are factory calibrated to measure CO2 concentration levels up to 5000 ppm • Custom packaging available • Adjustable firmware variables Applications • Automotive HVAC – Automatic fresh air control • Automotive HVAC – Safety sensor for CO2 refrigerants Ordering Information • Sample requests:
2 Sensor for Automotive Applications - amphenol-sensors.com
• Factory-calibrated to measure CO2 concentration levels up to 5,000 ppm. • Adjustable firmware variables • Custom packaging options • Subject to commercial consideration, customization of firmware, connector and enclosure is possible The Telaire Internal Carbon Dioxide (CO2) Sensor is a nondispersive infrared (NDIR) CO2 sensor that
SGX - PRODUCTS - SGX Sensortech
Catalytic sensors are widely used for detecting flammable gases. They consist of a catalyst that promotes a chemical reaction when exposed to combustible gases, resulting in a change in temperature or resistance. This change is then measured to determine gas concentration levels. More information about this technology here...
Heavy Equipment & Off-Road (HVOR) - Amphenol Sensors
Amphenol Sensors is a leading innovator in sensor technologies and measurement solutions. Offering the most diverse sensor portfolio of standard and customized products for the world’s most demanding regulatory and industry-driven applications, Amphenol creates value by providing critical information for real-time decisions.
Grainmaster i Intergrated moisture and temperature measurement
matter concentration using the refraction of wavelength between photo transistor and diode. By using an optical transistor and optical diodes, an optical washing machine sensor measures the amount of light coming from the source of the light to the light receiver, in order to calculate water turbidity. Amphenol Advanced Sensors
All Sensors Archives - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
2 Sensor for Automotive Applications - amphenol-sensors.com
• Factory-calibrated to measure CO2 concentration levels up to 5,000 ppm. • Adjustable firmware variables • Custom packaging options • Subject to commercial consideration, customization of firmware, connector and enclosure is possible The Telaire Internal Carbon Dioxide (CO2) Sensor is a nondispersive infrared (NDIR) CO2 sensor that
Absolute, Non-Contact Position Sensors Data Sheet C ... - Temposonics
The dosing accuracy during preparation of damping solution and precise control of the IPA concentration are of considerable importance for the production and process stability in printing systems. The continuous discussion ... The sensors measure the stroke of steering cylinders on the port side and the bow side. Typically installed in multi ...
2 Sensor for Automotive Applications - amphenol-sensors.com
Accuracy and Measurement Range: • 400 to 5,000 ppm CO2: +/-200 ppm • 5,000 ppm to 4% CO2: +/- 10% of the reading • 4% to 6.5%: accuracy not specified • Temperature Dependence (outside 0C to 50C): +/- 0.5% of the reading Measurement and Sample Rate Characteristics: • Active Mode: 5 seconds sample rate
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.