Search Results for concentration of measure
Contact - Amphenol Sensors
Amphenol Sensors Headquarters Phone (814) 834-9140 Email sensors@amphenol-sensors.com Address 967 Windfall Road, St. Marys, PA 15857, US
Trasduttori di coppia | PCB Piezotronics
Reaction torque sensors are suitable for a wide array of torque measurement applications. They are typically used in torsional test machines, motor dynamometers, or in any application where rotation is limited to 360° or less. Due to the fact that these sensors do not utilize bearings, slip-rings, or other rotating elements, their installation ...
Datasheet - SGX Sensortech
2. Different gas sensors have different measurement concentration ranges (ranges), and should not be exposed to over-range/high concentrations for a longer time; 3. The sensor is covered with a waterproof and breathable filter (on the top of the sensor), which should not be damaged, scratched or pulled of; SGXEurope
An Introduction to Infrared Gas Sensors - SGX Sensortech
gas concentration ranges up to 5% by volume. They are ruggedly built using single active gas channel detection for economy and are best used in areas where monitoring for a few hours is required. The . IR31SE. is essentially the same as the . IR31SC, but has an integral diffusion mesh cover to protect against particulate entry. Both sensors may be
Amphenol
Power Consumption Peak (measurement mode) 0.27 0.45 W Power Consumption Idle 0.07 0.08 W CAN bus ... 5-6 NA H2 Concentration 0.0025 0 0 to 160.6375 % 7 354 Temperature 0.03125 -273 -273 to 1734.96875 % 8 NA Sensor Status #1 NA 0 to 255 . AAS-920-798A - 11/2022 www.amphenol-sensors.com ...
Quick-Connex Quick-Lock Safety Device and Master Lock - TPC Wire
Measure M = Meters F = Feet A = Inches Enter a three digit code in the box above Example: 5 = “005” 50 = “050” 500 = “500” Blank = Regular S = Stainless Steel P = Plastic HL = Hazardous Location Class I, Div. 2 Build Your Own Cord Sets with Quick-Lock Assembly for Hazardous Locations
PT06A-16-99P | Amphenol Global Search | Amphenol
16-bit Analog to Digital Conversion (ADC) for precise sensor outputs. Calibrate sensors with linear response and monitor gas concentration levels. PCB-mounted temperature sensor for enhanced accuracy.
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
PS1&PS4-H2S-500-MOD HydrogenSulfideModule Datasheet - SGX Sensortech
(Note: under different storage and measurement environments, the first electrode stabilization time is different) • When warming up, it is recommended to first warm the machine in clean air for about 20 minutes, observe whether the output of the hydrogen ... Different gas sensors have different measurement concentration ranges (ranges), and ...
Telaire T3000 Series CO2 Transmitters for Harsh Environments - Amphenol ...
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
ECVQ-EK3 Datasheet - SGX Sensortech
thermal conductivity) gas sensors, automatically measure the sensor outputs and calculate gas concentration levels. Sensors can be monitored automatically via the USB ... sensor has a linear response to concentration, a basic calibration can be performed using the supplied software to give a concentration reading in ppm, %volume or %LEL
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
Thermometrics TSW-10 Turbidity Sensor - amphenol-sensors.com
measurement taken at the end of each wash cycle. By measuring the turbidity of the wash water, the washing machine can conserve energy on lightly soiled loads by only washing as long as necessary. This will result in energy savings for the consumer. 22 ±0.4 5.7 ±0.1 DIODE (Light emitting part) Photo TR (Light receiving part) 34 ±0.4 Upper ...
Low Cost Accelerometers - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
2 Sensor for Automotive Applications - amphenol-sensors.com
• Factory-calibrated to measure CO2 concentration levels up to 5,000 ppm. • Adjustable firmware variables • Custom packaging options • Subject to commercial consideration, customization of firmware, connector and enclosure is possible The Telaire Internal Carbon Dioxide (CO2) Sensor is a nondispersive infrared (NDIR) CO2 sensor that
Telaire Air Quality Sensors
All units are factory calibrated to measure CO 2 concentration levels up to 5000ppm, while maintaining accuracy across the range. T6715 The new T6715 is the smallest most accurate dual channel CO 2 sensor available on the market today. Telaire dual channel technology allow self calibration in applications where ABC logic will not work. i.e.
Automotive Sensors | EV/HEV Battery
Thermometrics Dual Solar Sensor uses two photo diode cells to measure the intensity of the light that enters into the cabin of a vehicle. ... The output of the sensor is a ratio metric analog output with a detection range of 0 to 16% H2 gas concentration. REDCAN Thermal Runaway Sensor . A combination sensor capable of providing up to four ...
Process Control – Amphenol Sensors
Amphenol Sensors is a leading innovator in sensing technologies and measurement solutions. Offering the most diverse sensor portfolio of standard and customized products for the world’s most demanding regulatory and industry-driven applications, Amphenol creates value by providing critical information for real-time decisions.
Temposonics Archives - Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
TRDU Battery Leakage Detection Sensor - SGX Sensortech
BLD2 is a Battery Failure Detection sensor that measures H2 concentration when different battery leakage occur through CAN communication. ... The sensor must be exposed to measure the air from the battery pack only. Preferably, the filtering membrane included in the module should be facing downward. If this is not possible, it should be ...