Search Results for data analyst
Financials - Quarterly and Annual reports - Amphenol
Annual Reports and Proxy Statements. About Amphenol. Our Company; Product News; Investor Relations; Environmental, Social and Governance
MOTOR VIBRATION - PCB
Vibration analysts can use one accelerometer, mounted magnetically and rotate it around the motor to capture various data . collection points. In some cases the motor is in an inaccessible location and thus permanent mount sensors are used and routed to a junction box for walk up data collection. Accelerometers are permanently mounted by ...
Monitoring reciprocating gas compressors with 4-20 mA LPSTM vibration ...
a trained analyst can interpret the vibration data, effectively diagnose the problem(s) and make a final determi-nation of the state of the equipment. Still, the success of vibration analysis tools has significantly reduced the cost of vibration monitoring and enabled monitoring of more plant assets.
Vibration Monitoring of Gearboxes - PCB
encourages sparse data acquisition. The analyst will often turn to a much simpler means of attaching the sensor to the surface, such as using a two-rail magnet placed on a curved surface with the sensor attached to the magnet. This approach will often lead to not capturing the higher frequencies associated with impacting or friction.
Monitoring reciprocating gas compressors with 4-20 mA LPS™ vibration ...
analyst can interpret the vibration data, effectively diagnose the problem(s) and make a final determination of the state of the equipment. Still, the success of vibration analysis tools has significantly reduced the cost of vibration monitoring and enabled monitoring of more plant assets.
Magnet Mounting Techniques for Machinery Vibration Monitoring - PCB
proximity probes. Vibration analysts used the vibration data from the probes to assess machinery health. Analysis typically visited each plant 2 to 4 times per year to collect data. Although this practice . was. seen as a step toward predictive maintenance, it suffered from several shortcomings including; Data was acquired infrequently.
Monitoring reciprocating gas compressors with 4-20 mA LPSTM vibration ...
instances, only a trained analyst can interpret the vibration data, effectively diagnose the problem(s) and make a final determination of the state of the equipment. Still, the success of vibration analysis tools has significantly reduced the cost of vibration monitoring and enabled monitoring of more plant assets.
Continuous Condition Monitoring With Vibration Transmitters and ... - PCB
vibration analysts often realize that they wasted valuable time and resources taking vibration data on healthy machines. Plant size and the number of measurement points can make implementing a vibration monitoring program a formidable task. Determining the data collection routes and frequency of data collection also can be a difficult undertaking.
Detecting Rolling Element Bearing Faults Using the ECHO Wireless ... - PCB
In an ideal world, a vibration analyst would like to have a full set of overall and broadband data continuously on all vibration monitoring points. This would provide the best set of data to detect and diagnose machinery faults. Unfortunately, it is generally prohibitive to get a full set data more than once per month or quarter due to personnel
Vibration Monitoring of Paper Mill Machinery - PCB
the analyst. A block of data equal to 2.56 times the number of lines specified by the analyst is acquired. Upon completion of acquiring the time waveform, the spectral data are computed by transforming the time block of data to the spectra data block. The PeakVue™ 3 methodology differs by: 1.
Application solution - Wilcoxon Sensing Technologies
Machinery vibration analysts have developed some standard reference terminology for equipment locations. Monitoring points are usually designated as inboard (IB) or outboard (OB). Outboard is the side of the fan or motor away from the ... Data that is acquired at the same point hundreds or thousands of times per day affords the observer the ...
Wireless Vibration Monitoring System | PCB Piezotronics
Streamline your data collection safely with the Echo® Wireless system. The Echo® Wireless is a simple, effective, alarm-based vibration monitoring system designed to keep you ahead of potential faults without compromising the safety of your maintenance team. Its wireless transmitter allows for monitoring more channels with fewer resources ...
Echo® Wireless Vibration Monitoring System - PCB
Echo® Data Client Service. Echo® data can also be exported from the Echo® Data Presentation Software to a tab delimited spreadsheet file that is suitable for use with Excel or other data viewing applications for post processing. Contact IMI® to discuss other interfaces to legacy condition monitoring programs and plant monitoring systems.
Amphenol Reports First Quarter 2024 Results and Announces New Stock ...
First Quarter 2024 Highlights: Sales of $3.26 billion, up 9% in U.S. dollars and 6% organically compared to the first quarter of 2023 GAAP Diluted EPS of $0.87, up 23% compared to prior year Adjusted Diluted EPS of $0.80, up 16% compared to prior year GAAP and Adjusted Operating Margin of 21.0% Operating and Free Cash Flow of $599 million and $506 million, respectively Announces a new three ...
Q Microwave Joins Amphenol Corporation in Strategic Acquisition
Amphenol has a diversified presence as a leader in high-growth areas of the interconnect market including: Automotive, Broadband Communications, Commercial Aerospace, Industrial, Information Technology and Data Communications, Military, Mobile Devices and Mobile Networks. For more information, visit https://amphenol.com.
Installation of vibration sensors - Wilcoxon Sensing Technologies
The vibration analyst must evaluate and determine the mounting location of the individual sensor based on the ... Most vibration data collectors, monitors, and sensor power units contain an internal blocking capacitor for AC coupling. If not included, a blocking capacitor must be field installed. Page 2 Amplitude range and the supply voltage
Home - Amphenol Canada
Media Library- Catalogs, Data Sheets, Patents, Videos; Filter MIL-DTL-38999 Series III-----ACS: Amphenol Communications Solutions-----The Interface - Episode 93: Phil Baynes; The Interface - Episode 180: Tony Condello; Featured Products. ARINC 600. ARINC 600 Connectors are recognized standard rack and panel connectors for Aircraft applications. ...
IT Datacom | Markets - Amphenol
SUPPORTS 53.12Gb/s DATA RATE & LOW POWER The module is compliant with IEEE 802.3 cd, SFF-8472 Rev 12.4, and compatible with SFF-8432 and applicable portions of SFF-8431 Rev. 4.1. - Supports 53.125Gb/s data rate - 1.8W maximum power consumption with established link - Up to 10km on 9/125μm SMF - Operating temperature range: -40°C to 85°C ...
About Us - SV Microwave
Amphenol Corp. is the world's second-largest connector company, producing electronic and fiber optic connectors, cable, and interconnect systems for applications converging technologies of voice, video and data communications, industrial/automotive, and military/aerospace. Florida Cage code: 95077 Arizona Cage code: 8D6M2
Installation of vibration sensors - Wilcoxon Sensing Technologies
The vibration analyst must evaluate and determine the mounting location of the individual sensor based on the specific machine and vibration source to be monitored. With a firm ... For this reason, most commercially available data collectors and vibration monitors have power supply circuits that include a CCD to regulate the power supplied to ...