Search Results for do most electronics have electric shock protection
ICP ® Shock Accelerometers - PCB
ICP ® Shock Accelerometers. Piezoelectric ICP® accelerometers afford a very high signal output (+/- 5 volts full scale) and the ease of two-wire electrical connectivity. Their inherent ruggedness enables them to be severely over ranged without damage.
Connectors | Products - Amphenol
Amphenol has been designing and manufacturing electrical and electronic connectors since the company’s inception in 1932. For nearly a century, we’ve been helping customers transmit power, data and signal in the harshest environments, from subsea applications to the outer reaches of space and everywhere in between.
Model W138A01/-0022 ICP® Pressure Sensor Installation and Operating Manua
32 micro cable/connector, the high shock can flex the cable/connector joint enough to move the center pin of the 10-32 cable connector. This can cause noise on the output signal. Protecting the connection from shock may be required. PCB Model 070A03 adaptor can be used to adapt the 10-32 micro jack on the 138 to a BNC jack. A
Model 113B24 Platinum Stock Products; High frequency ICP ... - PCB
General Electric RTV type 106 is recommended. Apply the rubber coating to the surface of the diaphragm and allow it to cure in accordance with the manufacturer’s instructions. (If you have ordered the CA option, ablative coated models, further protection will not be necessary.) Although ICP® sensors have low-output impedance
Vibration monitoring FAQs - Wilcoxon Sensing Technologies
All electronic components produce some electrical noise. At high frequencies, amplifier noise is governed by circuit resistors in the form of Johnson Thermal or white noise. ... Overload protection circuitry should be incorporated to reduce settling time, lower susceptibility to distortion from electrical and mechanical shocks (e.g. spark ...
Model 482A22 4-channel, line-powered, ICP® sensor signal cond ... - PCB
This product is intended for use by qualified personnel who recognize shock hazards and are familiar with the safety precautions required to avoid injury. WARNING 2: This equipment is designed with user safety in mind; however, the protection provided by the equipment
Ethernet Switch & Media Converter - Amphenol Socapex
Each Ethernet MIL-STD switch is rugged and hardened to improve ingress, impact, and shock/vibration protection, as well as eliminate all moving parts through passive cooling. Our range of Ethernet military-grade switches feature numerous options: 4 to 28 LAN ports with options for fiber optic ports, fast, gigabit or even 10G datarate with a ...
Endevco Undamped High Shock Sensors | PCB Piezotronics
Endevco Undamped Piezoresistive Shock Accelerometers. PCB's acquisition of Endevco's full line of testing sensors means all Endevco sensors are now backed by PCB's Total Customer Satisfaction (TCS) guarantee. The Endevco brand has long been the industry standard for reliable measurements in extreme high g environments.
D38999 Series III Hermetic Connectors - Amphenol Aerospace
Contact Protection: Recessed pins in this 100% scoop-proof connector minimize potential contact damage; ... Vibration/Shock: Operates under severe high-temperature vibration, through 200°C; Lockwiring Eliminated: Unique, self-locking, quick coupling connector eliminates lockwiring; ... What are the electrical requirements?
Model 682M57 DIFFERENTIAL DIN RAIL CHARGE AMPLIFIER Installation ... - PCB
from the enclosure in either the up or down direction, terminate the wire in the correct location. Do not exceed a torque of 0.5Nm. Do not leave excess uninsulated wire which can short to adjacent wiring. Re-install the terminal block. This easy to assemble connection method allows devices to be exchanged easily and the electrical connection to
PCB PIEZOTRONICS
vacuum, shock, vibration, and acoustic stress. Supporting both commercial and military applications, we offer custom options to meet environmental standards and requirements, including program design requirements to RTCA-DO-160 and MIL-STD-810. Popular Aerospace & Defense Applications:
High Sensitivity ICP ® Accelerometers - PCB
Models that include a 2-pin, military style connector provide the added benefit of being electrically case isolated for superior RF and EMI protection. Vibration monitoring of buildings, monuments, and critical infrastructure is a key component in smart cities to identify exactly how much stress has been applied to a structure.
Signal Conditioning Basics | PCB Piezotronics
Do not apply more than 20 mA constant current to ICP ® sensors or in-line amplifiers. 2.) Do not exceed 30 VDC supply voltage. 3.) Do not apply voltage without constant current protection. Constant current is required for proper operation of ICP ® sensors 4.) Do not subject standard ICP ® sensors to temperatures above 250 °F (121 °C ...
Introduction to Dynamic Pressure Sensors - PCB
Others that are designed to maximize the frequency response may require thermal protection coating, recess mounting, or a combination of these to lessen the thermal shock effects. Coatings include silicone grease, (may also be used to fill a recess mounting hole), RTV silicone rubber, vinyl electrical tape, and ceramic.
Model 137A22 ICP® Pressure Sensor Installation and Operating Manual - PCB
General Electric RTV type 106 is recommended. Apply the rubber coating to the surface of the diaphragm and allow it to cure in accordance with the manufacturer’s instructions. (If you have ordered the ablative coated models, further protection will not be necessary.) 3.0 OPERATION
IR2 Single Gas Series Datasheet - SGX Sensortech
1. Do not allow sensors to fall on the floor. This could cause IR Source filament breakage, damage to the pins and the gas entrance aperture. 2. Do not apply mechanical force against the gas entrance aperture. 3. Do not immerse sensors in water or other fluids. 4. Protect the gas entrance aperture against dust ingress and sprayed materials. 5.
Transient Voltage Suppression in Military Connectors
As the shift to more-electric and all-electric aircraft accelerates, so too does the need to dramatically reduce airframe weight. Many commercial and military aircraft already have significant portions of their bodies constructed of advanced carbon composite materials, but the proliferation of this technology is still an aircraft manufacturer’s single-greatest opportunity for further weight ...
Filter Connectors - Amphenol Canada
become the mainstay of meeting RTCA/DO-160 for high end mili-tary systems. The heart of that filtering is the placing of a capacitor network inside the connector. This allows for a complete solution for the LRU to meet both conducted and radiated emissions as required in most systems. In the late 1980’s the development of the
IR1 Single Gas Series Datasheet - SGX Sensortech
1. Do not allow sensors to fall on the floor. This could cause IR Source filament breakage, damage to the pins and the gas entrance aperture. 2. Do not apply mechanical force against the gas entrance aperture. 3. Do not immerse sensors in water or other fluids. 4. Protect the gas entrance aperture against dust ingress and sprayed materials. 5.
Sensor solutions for industrial cooling tower and process cooler fans
and low noise electronics required for measuring slow speed machinery. Our sensors are hermetically sealed and housed in chlorine resistant 316L stainless steel. The Wilcoxon splash-proof connector ensures total sealing in all environmental conditions. Two types of sensors are recommended for monitoring cooling towers.