Search Results for do most electronics have electric shock protection
Model 3501B1260KG/-0001 Piezoresistive Accelerometer Installation and ...
have positive or negative slope, although it will be stable for any one unit. 3.0 Features The 3500/3600 Series uses micro-electromechanical systems (MEMS) technology, in which all structural and electronic components are manufactured in silicon using electronic microfabrication technologies. MEMS devices are preferred in
Pyroshock Sensors | PCB Piezotronics
PCB has several shock accelerometer designs that improve measurement of both high-level (e.g., gun launch and penetration events) and pyrotechnic shock. Pyrotechnic shock, often called pyroshock, is a measurement challenge due to its associated high frequency content, which typically excites the resonant frequency of any measuring accelerometer.
Development of a Damped Piezoresistive MEMS High Shock Sensor - PCB
external mechanical isolators have to be frequently employed to protect the transducer (isolate it from high frequencies). Isolator design has to pay considerable attention to preserving enough bandwidth to track the residual rigid body motion and/or structural dynamics of interest for the device under test. A different approach in MEMS shock
Fiber Optic Media Converters - Amphenol Socapex
Each Ethernet MIL-STD switch is rugged and hardened to improve ingress, impact, and shock/vibration protection, as well as eliminate all moving parts through passive cooling. Our range of Ethernet military-grade switches feature numerous options: 4 to 28 LAN ports with options for fiber optic ports, fast, gigabit or even 10G datarate with a ...
Model 482C15 Four-Channel, ICP Sensor Signal Conditioner ... - PCB
Any piece of electronic equipment is vulnerable to ESD when opened for adjustments. Internal adjustments should therefore be done ONLY at an ESD-safe work area. Many products have ESD protection, but the level of protection may be exceeded by extremely high voltage that is typically present in normal situations. 1-3. Equipment Rating
Model RH401B04 - PCB
who recognize shock hazards and are familiar with the precautions required to avoid injury. While our equipment is designed with user safety in mind, the protection provided by the equipment may be impaired if equipment is used in a manner not specified by this manual. Discontinue use and contact our 24-Hour Sensorline if:
Model 401B04 ICP® Source Follower Installation and Operating Manual - PCB
who recognize shock hazards and are familiar with the precautions required to avoid injury. While our equipment is designed with user safety in mind, the protection provided by the equipment may be impaired if equipment is used in a manner not specified by this manual. Discontinue use and contact our 24-Hour Sensorline if:
High Performing Military Connectors from Amphenol
Amphenol like any other industry player has reliable, high-performing, and robust solutions to meet critical military applications. We have a line of specific D-Subminiature connectors that conform to military standards and target military applications. These are part of our popular and proven D-Subminiature product lines that encompasses a wide variety of applications in telecommunications ...
Glossary of RF Terms - Amphenol RF
The speed of an electrical signal down a length of cable compared to speed in free space expressed as a percentage. Voltage The term most often used to designate electrical pressure that exists between two points and is capable of producing a flow of current when a closed circuit is connected between the two points.
Model 102A04 **OBSOLETE** See 102B04 High frequency ICP ... - PCB
General Electric RTV type 106 is recommended. Apply the rubber coating to the surface of the diaphragm and allow it to cure in accordance with the manufacturer’s instructions. (If you have ordered the CA option, ablative coated models, further protection will not be necessary.) Although ICP ® sensors have low-output impedance
Model 113A26 **OBSOLETE** See 113B26 High frequency ICP® pressure probe ...
General Electric RTV type 106 is recommended. Apply the rubber coating to the surface of the diaphragm and allow it to cure in accordance with the manufacturer’s instructions. (If you have ordered the CA option, ablative coated models, further protection will not be necessary.) Although ICP ® sensors have low-output impedance
Model 137A23 ICP® Pressure Sensor Installation and Operating Manual - PCB
1. Do not exceed specified maximum range. 2. Do not subject sensor to temperatures exceeding temperature shown on specification sheet. 3. Do not apply voltage to sensor without current-limiting diodes or other current protection. 4. Do not apply more than 20 mA of current to the sensor. Field repair of the piezoelectric element or amplifier
VQ21T Series Combustible Gas Sensor Elements FEATURES INTRODUCTION ...
Do not apply more than 50% of the maximum bridge voltage to either element or otherwise there may be adverse effects on the stability of sensitivity and zero offset. Although the VQ21T Series possesses a high degree of resistance to poisons, it will be affected by prolonged exposure. Additional protection may be provided by the use
Model 137A21 ICP® Pressure Sensor Installation and Operating Manual
1. Do not exceed specified maximum range. 2. Do not subject sensor to temperatures exceeding temperature shown on specification sheet. 3. Do not apply voltage to sensor without current-limiting diodes or other current protection. 4. Do not apply more than 20 mA of current to the sensor. Field repair of the piezoelectric element or amplifier
Model 137A FREE FIELD BLAST PRESSURE PENCIL PROBE Installation ... - PCB
General Electric RTV type 106 is recommended. Apply the rubber coating to the surface of the diaphragm and allow it to cure in accordance with the manufacturer’s instructions. (If you have ordered the ablative coated models, further protection will not be necessary.) 3.0 OPERATION
Model 685A39 Linear Adjust Mechanical Vibration Switch ... - PCB
- DO NOT insert, remove, or handle screw terminal plugs with live wires connected - DO NOT make any adjustments to the setpoint with live wires present - DO NOT open the unit if machine is powered or running - DO NOT open the unit if the Relays are energized - DO NOT open the unit if the Reset Coil is energized
Model 137BPBO PLACEBO (137B) Installation and Operating Manual - pcb.com
1. Do not exceed specified maximum range. 2. Do not subject sensor to temperatures exceeding temperature shown on specification sheet. 3. Do not apply voltage to sensor without current-limiting diodes or other current protection. 4. Do not apply more than 20 mA of current to the sensor. Field repair of the piezoelectric element or amplifier
Model 686B01 USB programmable electronic vibration switch with 2 ... - PCB
who recognize shock hazards and are familiar with the precautions required to avoid injury. While our equipment is designed with user safety in mind, the protection provided by the equipment may be impaired if equipment is used in a manner not specified by this manual. Discontinue use and contact our 24-Hour Sensorline if:
Automotive Interconnects | ADAS | EV Charging | Automotive Lighting ...
Connectors are typically used to connect sensors, actuators, and other components that make up the Advanced Driver Assistance System (ADAS). These connectors must be able to support high-speed data transmission, withstand vibration and temperature fluctuations, as well as provide superior electrical performance and EMI protection, and meet the stringent requirements of the automotive ...
Model 686C01 USB-programmable electronic vibration switch, relay ... - PCB
A solid state relay is an electronic component that functions in the same way as an electromechanical relay, but without any moving parts. A solid state relay offers the most reliable switch action, especially for vibration applications where moving relay components run a greater risk of malfunction. They are purely electronic devices