Search Results for do most electronics have electric shock protection
Model 130A25 ICP® ARRAY SHORT MICROPHONE WITH INTEGRAL PREAMPLIFIER. 10 ...
who recognize shock hazards and are familiar with the precautions required to avoid injury. While our equipment is designed with user safety in mind, the protection provided by the equipment may be impaired if equipment is used in a manner not specified by this manual. Discontinue use and contact our 24-Hour Sensorline if:
PCB Piezotronics | Measure vibration, pressure, force, and more
PCB ® manufactures sensors used by design engineers and predictive maintenance professionals to test and measure vibration, pressure, force, acoustics, load, and shock in research and development as well as industrial applications.
Model 674A91 Vibration Transmitter with an IO-Link communication ... - PCB
who recognize shock hazards and are familiar with the precautions required to avoid injury. While our equipment is designed with user safety in mind, the protection provided by the equipment may be impaired if equipment is used in a manner not specified by this manual. Discontinue use and contact our 24-Hour Sensorline if:
Operation Manual Level Plus LLE - Temposonics
1.Wear proper personal protection equipment such as hard hat, safety shoes, safety glasses, gloves, and hearing protection. 2.Do not open or dismantle the sensor. 3.Follow the specifications given in the technical documentation. 4.Two (2) individuals are recommended to conduct proper installation, commissioning, and repair of the level transmitter.
Model 137B24B Quartz, free-field, ICP® blast pressure pencil ... - PCB
1. Do not exceed specified maximum range. 2. Do not subject sensor to temperatures exceeding temperature shown on specification sheet. 3. Do not apply voltage to sensor without current-limiting diodes or other current protection. 4. Do not apply more than 20 mA of current to the sensor. Field repair of the piezoelectric element or amplifier
Model 357B02 High temp., ceramic shear, charge output accel., 15 pC/g ...
electronics permits operation to elevated temperatures of 500 °F (260 °C) for most ceramic crystal models and typically 900 °F (482 °C) and extreme application up to 1200 °F (650 °C) for UHT-12. These accelerometers are ideal for structural testing, machine monitoring, and vehicular shock and vibration
Marine & Industrial Support FAQs - Charles Industries, LLC
The 5000-Series has better EMI filtering (Electromagnetic Interference) providing additional protection from the radio frequency spectrum of external electronic devices. The 2000-Series has a 2-year warranty and the 5000-Series has a 5-year warranty.
Model 137B29B Quartz, free-field ICP® blast pressure pencil ... - PCB
1. Do not exceed specified maximum range. 2. Do not subject sensor to temperatures exceeding temperature shown on specification sheet. 3. Do not apply voltage to sensor without current-limiting diodes or other current protection. 4. Do not apply more than 20 mA of current to the sensor. Field repair of the piezoelectric element or amplifier
General Purpose Triaxial Piezoelectric Accelerometers - PCB
Electronic Switches; Mechanical Switches; Pressure Transducers. ICP® (Up to 250 F) Charge (Up to 1200 F) ... Electrical Connector: M3 Coaxial Jack; Electrical Connector: M3 Coaxial Jack; $1358.00 USD ... pressure, force, acoustics, load, and shock in research and development as well as industrial applications. Divisions of PCB.
Model 137A FREE FIELD BLAST PRESSURE PENCIL PROBE Installation ... - PCB
General Electric RTV type 106 is recommended. Apply the rubber coating to the surface of the diaphragm and allow it to cure in accordance with the manufacturer’s instructions. (If you have ordered the ablative coated models, further protection will not be necessary.) 3.0 OPERATION
Accelerometers / Vibration Sensors | PCB Piezotronics
The most commonly used technology is our proprietary integrated circuit piezoelectric, ICP® (IEPE) accelerometers, which require constant current power supply. Most data acquisition, digital control, and portable data systems provide ICP® sensor power. Each directional axis measured requires one channel of the data system or signal conditioner.
Model 130F21 ICP® Electret Array Microphone Installation and Operating ...
who recognize shock hazards and are familiar with the precautions required to avoid injury. While our equipment is designed with user safety in mind, the protection provided by the equipment may be impaired if equipment is used in a manner not specified by this manual. Discontinue use and contact our 24-Hour Sensorline if:
Model 137B21B Quartz, free-field, ICP® blast pressure pencil ... - PCB
1. Do not exceed specified maximum range. 2. Do not subject sensor to temperatures exceeding temperature shown on specification sheet. 3. Do not apply voltage to sensor without current-limiting diodes or other current protection. 4. Do not apply more than 20 mA of current to the sensor. Field repair of the piezoelectric element or amplifier
Circular Connectors | Products - Amphenol
Designed for applications that demand size and weight savings without sacrificing the electrical and mechanical performance of a standard MIL-DTL-38999. 70% Lighter and 50% Smaller than Similar MIL-DTL-38999 Connectors. Fully Intermateable, Intermountable, and Interchangeable with Mighty Mouse.
USB3CFTV - Rugged Ethernet, USB & Display connectors - Amphenol Socapex
With EMI protection and mating plug/receptacle cycles of 500, the Amphenol Socapex connector USB3CFTV provides reliable and secure connectivity in challenging environments. It also offers salt spray resistance, ROHS compliant platings, shock resistance, and operates within a wide temperature range of -40°C to +85°C (-40°F to 185°F), making ...
Modular Jack Connectors and Their Applications - Amphenol CS
These connectors feature die cast metal housings that are mechanically rugged and stable, providing protection against shock, vibration and impact, and prevent any resultant dimensional distortion. These connectors are capable of withstanding operating temperature range from -55°C to +105°C and are available in a wide variety of mounting and ...
Model 130F22 ICP® Electret Array Microphone Installation and ... - PCB
who recognize shock hazards and are familiar with the precautions required to avoid injury. While our equipment is designed with user safety in mind, the protection provided by the equipment may be impaired if equipment is used in a manner not specified by this manual. Discontinue use and contact our 24-Hour Sensorline if:
Connectors | Products - Amphenol
They meet the requirement of MIL-DTL-55181. MW series power connectors are designed with a center lock coupling screw. They are waterproof, polarized, and can withstand high shock and vibrations. They are primarily used for the interconnection of power and control circuits of electric equipment military communication systems.
Sensor selection guide - Wilcoxon Sensing Technologies
Two of the main parameters of a piezoelectric sensor are the sensitivity and the frequency range. In general, most high frequency sensors have low sensitivities and, conversely, most high sensitivity sensors have low frequency ranges. It is therefore necessary to compromise between the sensitivity and the frequency response.
Model 137B32 Quartz, free-field, ICP® blast pressure pencil ... - PCB
1. Do not exceed specified maximum range. 2. Do not subject sensor to temperatures exceeding temperature shown on specification sheet. 3. Do not apply voltage to sensor without current-limiting diodes or other current protection. 4. Do not apply more than 20 mA of current to the sensor. Field repair of the piezoelectric element or amplifier