Search Results for how to make print lines
843-191-2801 | Amphenol Global Search | Amphenol
191 Delaware Avenue Sidney, New York 13838-1395 Phone: 888-364-9011 Fax: 520-397-7169 View and download or print Amphenol catalogs on-line at: www.amphenol-industrial.com Amphenol Industrial is a Certified ISO 9001 Manufacturer.
INSTALLATION INSTRUCTIONS C-CHARGER & OWNER’S MANUAL - Charles Industries
5 FIELD YES The wire driven positive by the regulator to make the alternator charge. Volt-age at this point depends on how much current is being produced by the alternator, and varies from zero to battery voltage. 6 ALT. GND YES The return line for field current. Note: Absence or loss of this connection will prevent charging. Do NOT
Buried Cable Pedestal Installation Instructions - Charles Industries
Position the mounting stake inside the line of the cable with the base facing out. Drive the stake until approximately 4 inches remain above the final grade level. Attach the base to the stake (see Figure 6). Integral Stake Mount Position the base inside the line of the cable with the open section facing out. If additional depth is re-
C−PHONE INSTALLATION INSTRUCTIONS & OWNER’S MANUAL COMMUNICATIONS ...
Two input lines allow the C-PHONE to be connected to a dockside telephone line and a cellular line, or a com-bination of one or both, to send and receive telephone calls from any station. Typical installations designate Line 1 as the dockside telephone and Line 2 as the cellular line. Cellular line connection to the C-PHONE requires a
Accessories and Other | Products - Amphenol
Various build to print precision stamped components from thin gage to thick gage . Application for Infotainment system, connectivity,Shielding, Wirehardness, Safety & sensor, power train and interior. Industries : Datacom, Medical, Industrial, Renewable Energy , Semicon and Consumer Electronic industry
TEDS Sensors and technology - Introduction - PCB
These pulses interrogate the memory and the contents are then transmitted, via the same two wires, back to the signal conditioner and controlling PC. The data is then available within the application software for viewing, channel setup, printing or archiving in a spreadsheet or database format.
Issue 1 Print 4 LT–5000HQ–1 HQ-CHARGER 5000 SP SERIES INSTALLATION ...
LT–5000HQ–1 Issue 1 Print 4 All rights reserved. Printed in the United States of America.
12T KVA IsoTransformer INSTALLATION INSTRUCTIONS & OWNER’S MANUAL
The IsoTransformer is intended for installation inside an engine room or elsewhere inside the boat. Make sure that the location will not subject the unit to rain, snow, excessive moisture, or excessive heat. This device is ignition protected in accordance with U.S. Coast Guard regulations under 33 CFR 183.410. NOTICE Application Precaution
ANSYS HFSS 3D Component Models - Amphenol RF
Amphenol RF offers ANSYS HFSS 3D component models of printed circuit board connectors for download. These self-contained 3D models allow designers and engineers to simulate the performance of a PCB connector on their PCBa product within a specific design prior to placing an order.
PT/451-26482 Series I - Amphenol Socapex
The PT/451 Series connectors are a type of cylindrical MIL-DTL-26482 Series I connectors that offer a wide range of backshell and insert arrangements. With nine shell sizes available and up to 61 contacts, they are ideal for use in aeronautics, military, and industrial applications where high-quality connectors are required. The PT/451 connectors are available in crimp, solder, and PCB contact ...
LT93-PS1230-1 PR3 - Charles Industries
After determining the wire lengths and gauges, make the AC wiring connections to TB1. (Refer to the Block Dia-gram in Figure 1.) To make connections to the terminal blocks: Step Action 1. Remove the small screw in the center of the unit that secures the sliding door to the top cover 2. Gently slide the door up until it stops 3.
Micro SD Express Connector | Input Output Connectors | Amphenol
Its incredible speed, compatibility, and adaptability make it a versatile solution for a wide range of applications, from consumer electronics to industrial IoT devices. With a commitment to reliability and durability, Amphenol's microSD Express connector is set to redefine the way we store and access data, enabling us to keep pace with the ...
Autoclave Temperature Mapping | Temperature Validation System - KAYE
Advanced Validation Technology. The Kaye Validator AVS (Advanced Validation System) is an all-in-one temperature mapping and thermal validation system that combines precise sensor measurements with all GxP requirements for calibration and traceability to national standards, while generating compliant reports and managing the validated assets and validation equipment.
75 Ohms Coaxial Contacts - High speed contacts - Amphenol Socapex
Amphenol Socapex offers 75 Ohms Coaxial Contacts, a reliable and efficient solution for connectors used in video applications. These contacts are designed for use with D38999, EN3645, EN4165, 2M, and 387TV connectors and are available in contact sizes 16, 12, 8, and 6. Whether you need to transmit SD-SDI, HD-SDI, or 3G-SDI, the 75 Ohms Coaxial Contacts are a great choice.
N2K Panel Mount Wired 5-Pin (male) - Gemeco
Waterproof seals ensure the integrity of the NMEA 2000® connection and bulkhead/panel. The male panel mount wired connector can easily replace any of the existing ‘drop’ glands on the Actisense QNB-1 to create a quick pluggable NMEA 2000® connection option.
Ultrasonic Sensors - Amphenol Sensors
Airmar With a highly experienced team of scientists, designers, engineers and technicians as well as a vertically integrated business model, Airmar has the capability of bringing innovative products from concept to production. Today, Airmar employs over 300 people worldwide and is dedicated to producing a diverse and innovative line of products to satisfy the acoustic […]
4201–00 4-Wire 4-Way and 4202–00 4-Wire 6-Way Conference Bridges
All transmit line and receive line circuits for each port are identical; therefore, this circuit description is based on RCV LINE 1 and XMT LINE 1. Data or VF signals enter the 4201–00 on the RCV LINE 1 tip and ring leads (pins 1 and 2, respectively) and are transformer-coupled (via T1) to the input of operations amplifier U2–1.
The value of keeping sensors in-spec - PCB
read the fine print on how the sensors were tested. The more information you can get on a sensor’s proven perfor-mance over time, the better. Q: What happens when the sensors you are using to monitor vibration on machines are not giving accurate measurements? A: When you’re using sensors to monitor machinery, sometimes you’ll
Access Multiplexer User’s Guide - charlesindustries.com
to view some information from the AMUX, and are only allowed to make limited changes to the AMUX’s settings. The administrator-level allows full access to the AMUX, including access to all features prohibited to user-level access. The table below shows what features of the AMUX can be accessed at the user and administrator access levels.
IMPACT AND DROP TESTING - PCB
fracture a unit under test (UUT). Take for example a straight-line collision, such as a car crash. Using the work-energy principle where average impact force times the distance traveled equals the change in kinetic energy, design engineers can help reduce the impact force of a car by extending the stopping distance through the use of ‘crumple