Search Results for laser marking
U.S. Army air defense laser prototype successfully downs targets
A Raytheon 50 kilowatt-class laser mounted on a U.S. Army Stryker armored vehicle during a live-fire exercise at White Sands Missile Range in New Mexico. [U.S. ARMY] The U.S. Army reported its prototype Stryker-based short-range air defense laser system prototype successfully downed multiple targets during a recent live-fire test.
Called in by Experts - DC Electronics
A precision laser manufacturer was having frequent cable failure at different points in its assembly test operations. They thought they had a design problem and first contacted an engineering firm specializing in custom cables and connectors. The engineering firm referred them to DCE because of our manufacturing and assembly expertise.
Amphenol Charles Fiber Aerial Solutions
Never look into the end of a fiber optic line or use a magnifier in the presence of laser light or radiation. Exercise caution when installing, testing or maintaining live circuits. If eyes are exposed to laser light or radiation ... • Cable marking tool • Assorted cable ties • Buffer tube stripper tool (score/cut buffer tubes) • Fiber ...
Amphenol
the culmination of three years of research and development in laser welding copper based alloys. The markets and applications for the SurLok PlusTM Series include but are not limited to the following: Energy Storage EV/HEV* Process Control/Automation Heavy Equipment *Note: 1500V SurLok PlusTM option only
PRELIMINARY ISSUE - Amphenol RF
b. marking: bag to be marked "amphenol rf, 95-902-449-xxx and date code". 1/4" [6.35] hex typ(2) locate approximately at center as shown marking: amphenol rf interface per mil-std-348 series: sma plug typ(2) scale 0.600 customer outline drawing all other sheets are for internal use only preliminary issue.
Protimeter Moisture Meters
• Infrared non-contact surface temperature with laser pointer • Concrete and concrete floor moisture measurement (ASTM-F2170 Standard) • Fast temperature and humidity response • Highly accurate • Simple to use interface with color display • Replaceable humidity and temperature sensor • Psychrometric calculations • Data logging
TECHNICAL NOTE TN-15 - PCB
venting the sensor being calibrated to a known static reference pressure, by means of a fast-acting valve; by hydraulic impulse comparison calibration, using a transfer standard; or with the
About – Amphenol Sensors
We believe that making sustainable choices in the way we conduct our business creates short-term and long-term value for our stakeholders. We do not create long-term value by merely complying with regulations, but we go beyond compliance to find ways to green our operations and our products to ensure continuity of the material and human resources that we need to operate the business.
Home - XMA
Coupling transmission lines with low insertion loss; Resources. Distribution Partners Need components fast? Ask our distributors; Territorial Sales Representatives Your local resources; Publications Check us out in publications; XMA Blog Living and learning about quantum computing, space, and more; About
Virtual Tour | PCB Piezotronics
Laser Etching Section 18 of 20 Final Inspection Section 19 of 20 Conclusion Section 20 of 20. About PCB ...
Mil-Spec Contacts | Products | Amphenol Aerospace
MIL-DTL-38999 Series III, II, I Contacts 38999 Application Tools 38999 Assembly Instructions 26482 Contact Information 26482 Assembly Tools 83723 Contact Information 83723 Assembly Tools MIL-DTL-83723 (Pyle) Contacts and Tools Class L Contact Information Class L Installation Instructions
3652-35 4W E&M/ER Installation Guide - Charles Industries
3. XXXX Front panel marking +13 +32.5 4. N. O., N. C. relay contact +7 +26.5 5. Ganged switches are indicated by alphabetical suffixes. Numerical suffix denotes discrete switch within a package. –16 +3.5 6. PC MOUNT TEST JACKS: 8. The RCV output range at T1 & R1 is +13.0 to –19.5DBM. The RCV ATTN provides from 0 to 32.5DB of attenuation in ...
Measuring displacement using accelerometers - Wilcoxon Sensing Technologies
Wilcoxon Sensing Technologies 8435 Progress Drive Frederick, MD 21701 Tel: +1 (301) 330 8811 [email protected] www.wilcoxon.com Measuring displacement using accelerometers
Media - Connor Manufacturing
Corporate Headquarters Connor Manufacturing, Inc. 22867 NE Townsend Way Fairview, OR 97024 [email protected] Corporate Administration Offices Connor Manufacturing, Inc. 500 Park Blvd., Suite 820 Itasca, IL 60143 Phone +1-630-363-3300 [email protected] Asia Administration Offices Connor Manufacturing (Asia) Pte. Ltd. 2 Venture Drive Vision Exchange #24-01 to #24-32
IBflex® Scanning Receiver | Test & Measurement | PCTEL
The IBflex scanner combines a lightweight design with the power to test multiple technologies and bands simultaneously.It can be used to deploy 5G New Radio networks in sub-6 GHz spectrum, verify public safety coverage, optimize dense small cell deployments, and improve the reliability of IoT systems.
Charles Guy Wire Markers - Charles Industries
Please call for availability of custom lengths, pre-placed reflective marking tape, and other options. Charles Industries, Ltd. Telecommunications Group www.charlesindustries.com Voice: (847) 806-6300 FAX: (847) 806-6231 E-mail: [email protected] D-OSP149-G13
Machining - Connor Manufacturing
Corporate Headquarters Connor Manufacturing, Inc. 22867 NE Townsend Way Fairview, OR 97024 [email protected] Corporate Administration Offices Connor Manufacturing, Inc. 500 Park Blvd., Suite 820 Itasca, IL 60143 Phone +1-630-363-3300 [email protected] Asia Administration Offices Connor Manufacturing (Asia) Pte. Ltd. 2 Venture Drive Vision Exchange #24-01 to #24-32
CUSTOMER OUTLINE DRAWING - Amphenol RF
%PDF-1.7 %âãÏÓ 21 0 obj > endobj 36 0 obj >/Filter/FlateDecode/ID[]/Index[21 25]/Info 20 0 R/Length 93/Prev 822524/Root 22 0 R/Size 46/Type/XRef/W[1 3 1]>>stream ...
Charles Industries opens state-of-the-art manufacturing facility in ...
These capabilities include metal punching and bending, laser cutting, welding, powder coating, hardware insertion, mechanical and electrical assembly, fiber optic and cable assembly, testing, and inspection. The availability of a skilled labor pool at Amphenol Optimize to perform these tasks was an important factor in choosing the
WeatherStation Instruments - AIRMAR
Airmar’s ultrasonic WeatherStation® instruments deliver accurate, reliable weather data from a rugged, compact, maintenance-free design with no moving parts. These all-in-one multisensors can measure real-time apparent wind speed and direction, air temperature and calculated wind chill, barometric pressure, relative humidity, calculated dew point and heat index.