Search Results for laser marking
Consumer Electronics - Connor Manufacturing
Corporate Headquarters Connor Manufacturing, Inc. 22867 NE Townsend Way Fairview, OR 97024 [email protected] Corporate Administration Offices Connor Manufacturing, Inc. 500 Park Blvd., Suite 820 Itasca, IL 60143 Phone +1-630-363-3300 [email protected] Asia Administration Offices Connor Manufacturing (Asia) Pte. Ltd. 2 Venture Drive Vision Exchange #24-01 to #24-32
Mil-Spec Contacts | Products | Amphenol Aerospace
MIL-DTL-38999 Series III, II, I Contacts 38999 Application Tools 38999 Assembly Instructions 26482 Contact Information 26482 Assembly Tools 83723 Contact Information 83723 Assembly Tools MIL-DTL-83723 (Pyle) Contacts and Tools Class L Contact Information Class L Installation Instructions
Charles Guy Wire Markers - Charles Industries
Please call for availability of custom lengths, pre-placed reflective marking tape, and other options. Charles Industries, Ltd. Telecommunications Group www.charlesindustries.com Voice: (847) 806-6300 FAX: (847) 806-6231 E-mail: [email protected] D-OSP149-G13
Amphenol
Innovative Laser Welded construction of the RADSOK® cartridge provides the following benefits. ®Smaller outside diameter of RADSOK, saving space of package High volume automated assembly processes Consistency in performance Improved mechanical strength Lower voltage drop and resistance Low temperature rise
Amphenol
the culmination of three years of research and development in laser welding copper based alloys. The markets and applications for the SurLok PlusTM Series include but are not limited to the following: Energy Storage EV/HEV* Process Control/Automation Heavy Equipment *Note: 1500V SurLok PlusTM option only
Connectors with metal ferrules / FSMA | Amphenol Precision Optics
To support the installation of special fibers, Amphenol Precision Optics offers standard connectors, which are usually equipped with ceramic or with metal ferrules. This solution is available for ST, SC, and FC connectors as well as for LC and FSMA connectors (standard market model, e.g. for laser and high-power connector).
Amphenol Fiber Optic Termini Fiber Systems International
• Laser marked TICC codes eliminate the need to decipher complex color-code bands • Precision ferrule alignment with captivated split zirconia sleeves • Wide configuration selection • Superior optical performance • Custom sizes available (Commercial-off-the-Shelf only) • I nteg rad v io ml sch u • Precision Mpress fitN terminus design
2068-7002-21 - Model
marking none. finish: sheet 1 1 b mil-std-100 & 1000 drawing practices per ansi-y-14.5 5 4 inches c see notes apply before / after processing see notes material: dimensions are in inches and third angle projection. note: interpret iaw ansi y14.5-1982 3 decim als inch [m m ] drawn checked eng. appr. 2 scale date date date b size 3ht76 cage code
SSI Technologies Application Note PS-AN6 MediaGauge (Model MG1-9V ...
The MediaGauge™ MG1-9V is made of all laser-welded 316L stainless steel for optimal media isolation and usage in a wide variety of media and corrosion or oxidation resistant applications. These compact 2 ½ inch, robust gauges measure pressures from 5 PSI to 5000 PSI and are well suited for a variety of industrial and ...
Installation Guide Hazardous Areas 0908 CCS - Wilcoxon Sensing Technologies
Page 5 of 17 a a chemicals may be oxidizers. For example, elemental magnesium will react violently with water to release heat. The magnesium is the fuel and water provides the oxidizer.
Accessories Catalog Level Plus - Temposonics
6. Laser etch the fo lowing information on the float: MTS - above centerline of float Part Number - below MTS but above centerline of flo at Sp ec i fG r av ty - b lo w n l ( thi s ou ld b e ac Sp .Gr f ) D ateC od - b lw sp c i fgr v y n . D at e cod ns if lph um r c h art ef om n , l w d b y TUBE FLOAT HALF 2x RETAINER 2x RADIALY CHARGED 0.375 ID
Learn More about Connector Mating Cycles - Amphenol CS
The mating cycles of a connector are directly related to its resistance. If a connector has a low threshold, it indicates fewer mating cycles, while the ones with higher threshold will have a longer life in terms of mating.
FIBER OPTIC CABLE ASSEMBLY MANUFACTURABILITY AND DESIGN GUIDE
3. Marking Details Marking details are based on MIL-STD-130 and will be legible and permanent. a) Marking information example • Cage code = 0YPM2 for AFSI, part number = 2006112209MD-01, serial number with date code embedded. The info can be provided in any order, and two lines of info are recommended. 0YPM2 2006112209MD-01 SN: YYDDDXXXX NOTES:
WeatherStation Instruments - AIRMAR
Airmar’s ultrasonic WeatherStation® instruments deliver accurate, reliable weather data from a rugged, compact, maintenance-free design with no moving parts. These all-in-one multisensors can measure real-time apparent wind speed and direction, air temperature and calculated wind chill, barometric pressure, relative humidity, calculated dew point and heat index.
NovaSensor | Pressure Sensors and Pressure Sensor Die
A laser-trimmed, thick-film resistor network on a hybrid ceramic substrate provides temperature compensation. Nova Sensor NPI-12 Series | Stainless Steel Media Isolated Sensors The NovaSensor NPI-12 Series of Stainless Steel Media Isolated Sensors provide a cost effective solution for applications that detect tube blockages and pump performance.
Freshly printed metal - Lutze Inc.
The laser beam melts the metal particles at the precise spots in the powder bed defined in the CAD plan. Then the work area drops by a layer thickness, and a rake strokes the powder bed smooth again. In this way, another layer is written into the powder by the laser in an almost magical illumination process. The cycle is repeated until the ...
Connectors | Products | Amphenol
Amphenol has been designing and manufacturing electrical and electronic connectors since the company’s inception in 1932. For nearly a century, we’ve been helping customers transmit power, data and signal in the harshest environments, from subsea applications to the outer reaches of space and everywhere in between.
3652-35 4W E&M/ER Installation Guide - Charles Industries
3. XXXX Front panel marking +13 +32.5 4. N. O., N. C. relay contact +7 +26.5 5. Ganged switches are indicated by alphabetical suffixes. Numerical suffix denotes discrete switch within a package. –16 +3.5 6. PC MOUNT TEST JACKS: 8. The RCV output range at T1 & R1 is +13.0 to –19.5DBM. The RCV ATTN provides from 0 to 32.5DB of attenuation in ...
introduction | Temposonics
Temposonics is the pioneer and leading manufacturer of magnetostrictive technology for measuring position and/or liquid level. Our sensors permit high-precision and dynamic position and/or speed measurement in state-of-the-art automation and safety-critical applications.
Leonardo DRS - Custom Cable
Leonardo DRS is a leading defense technology contractor, serving all arms of the U.S. military—Army, Marine Corps, Air Force, and Navy at a global scale. With laser focus, teams of engineers are committed to developing life-critical solutions for defense systems, surveillance intelligence, and communications networks.