Search Results for lol ping
Category-8 (Cat-8) Ethernet Cable Guide: Frequently Asked Questions ...
Category 8 Network Patch Cords offer complete backwards compatibility with existing Ethernet over Twisted Pair standards, including Gigabit Ethernet (1000BASE-T) and 10-Gigabit Ethernet (10GBASE-T).
Network Switch Software Documentation - Amphenol Aerospace
This command is used to enable/disable the keepalive/ping/heartbeat function. This function allows the software to ping a remote host and track the number of pings and replies.
Series Five Lightweight Military Circular Connectors - Amphenol ...
High Temperature Series Five connectors are the ideal solution for interconnect and electrical wire assemblies near engines, firewalls, and other high-heat sources. REACH/RoHS compliant alternative to Cadmium plating. A complete line of AS39029 contacts for all major Mil-Spec circular connectors. Have any questions?
Sensor Configuration - marport.com
To configure the sensor, you need to connect it to Mosa2 using a wireless communication or using the Configuration Cable. You need to calibrate the catch sensor to make sure you have correct catch measures. This procedure applies for both Catch Explorer and Catch sensors.
Checking Speed Measures with EM Log Tester - marport.com
You can export in a *.txt file all the settings configured for the sensor (such as ping length, frequency, range, TVG...).
SS510 200 kHz Portable Survey - Airmar
Users with adjustable-frequency echosounders will be able to regulate the operating frequency and tailor the beamwidth to specific survey conditions. And the treaded stem allows portable mounting.
156-Channel 50G/400G PAM-4 Rugged Ethernet Switchbox
Amphenol’s Rugged 156-Channel 50G/400G PAM-4 Ethernet Switch Box is conduction cooled and configurable for system connectivity, speeds, port types, and interoperation with various high-speed media converters and connectors for system interfacing.
Exporting Sensor Configuration Settings for Record Keeping
You can export in a *.txt file all the settings configured for the sensor (such as ping length, frequency, range, TVG...).
ping | Amphenol Global Search | Amphenol
Q PL Approval Letter Defence Logistics Agency Defence Supply Centre, Columbus Post Office Box 3990 Columbus, OH 43218-3990 DSCC-VQP-09-017606 (Mr. Funk/614-692-6608/jf)
Understanding Why Cable Fails - TPC Wire
Even though you cannot turn back time, you can help prevent costly downtime in the future by understanding why your cable has failed. Selecting the appropriate cable for your harsh industrial environment is vital to your operation. Let’s look at six common types of cable failure modes. 1. Conductor Failures.
Modular Jack - RJE48 Series - Amphenol CS
It supports 1G and 2.5G Ethernet data rates and transmission frequencies up to 100MHz. These Modular Jacks come in right angle, low profile with LEDs for link activity and network speed verification.
Configuring the Uplink , Up (Side) and Down Settings - marport.com
TVG (Time Variable Gain) is a method that compensate signal loss in the water. Basically, the aim is to have targets or sea bottom displayed in the same color on the echogram, whatever the distance from the sensor.
SS510 EchoRange™ 200kHz Portable Survey, DT - 7.6m Cable - Gemeco
Airmar’s Smart™ sensors feature embedded microelectronics that process depth and temperature inside the sensor that can be instantly displayed on any device that accepts NMEA data. EchoRange technology transfers NMEA 0183 data in real time to a computer via the RS422 standard.
SS510 Analog 200kHz D/T Portable Survey - 10m Cable
Airmar’s commitment to innovative technology has produced the patented SS510. This broadband, 200 kHz transducer has a Q of 2 and very good sensitivity. It enables users to perform accurate surveys in shallow water with high resolution. This transducer can also be “chirped” with a long pulse over a wide-frequency band.
Maintenance Checklist - marport.com
Switch on the sensor by shorting the center lug to the negative lug, then listen for a ping noise and check if you see the LED switched on. Test the sensor measures with Mosa2: depth, temperature, pitch, roll, and if applicable: spread distance, echogram, catch status, speed measures (using the EM log tester).
SS510DT 200KHZ ECHORANGE INTERACTIVE NMEA0183 3M - AIRMAR EMEA
Airmar’s Smart™ sensors feature embedded microelectronics that process depth and temperature inside the sensor that can be instantly displayed on any device that accepts NMEA data. EchoRange technology transfers NMEA 0183 data in real time to a computer via the RS422 standard.
Configuring Sounding Frequencies - marport.com
You can export in a *.txt file all the settings configured for the sensor (such as ping length, frequency, range, TVG...).
Calibrating the Sensor for Target Strength Value - marport.com
For V3 version of the sensor, you need to calibrate the sensor to offset the variability of the sensor transducer and of sound transmission. The aim is to have all sensors displaying the same target strength value (echogram color) for a given target.
Examples of Installations for a Target Strength Calibration
Ping pong ball. Figure 3. Fishing line passes through the ball and is fixed with glue. Figure 4. Example of installation with counterweights. 1. 50 cm. 2. 1 m. 3. Counterweight. Related information. Calibrating the Sensor for Target Strength Value ...
Configuring the Uplink and Down Settings - marport.com
You need to calibrate the catch sensor to make sure you have correct catch measures. This procedure applies for both Catch Explorer and Catch sensors.