Search Results for lol ping
Exporting Sensor Configuration Settings for Record Keeping
You can export in a *.txt file all the settings configured for the sensor (such as ping length, frequency, range, TVG...). Exporting Sensor Configuration Settings for the Receiver. You can export on an XML file the sensor settings that you configured on Mosa2. You can afterward use this file when adding the sensor to a receiver.
− CFXC FIBER CROSS-CONNECT PEDESTAL INSTALLATION GUIDE −
ping, cutting, shaving or scoring cables and tubing. - WARNING - Cable/fiber cleaning solvents may contain hazardous materials or harmful ingredients. Always read and follow the manufacturer’s precautions, warnings, and instructions when working with cleaning solvents or products. - WARNING - Never look inside any fiber cable, adapter, or ...
Maintenance Checklist - marport.com
If the sensor has not been not used for more than 3 months, we highly recommend to check the following points before using it: Make sure the sensors on the end cap are in good condition and clean.
Configuring the Uplink Power - marport.com
You can increase the uplink power of the sensor to increase the power of the signal transmitted. It is useful if you have interferences or if the sensor is far from the vessel.