Search Results for motion control
Temposonics
motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide. This creates a momentary radial magnetic field and torsional strain on the waveguide. The momentary interaction of the magnetic fields releases a torsional strain pulse that propagates the length of the ...
ACCESS PORT DESCRIPTION (CONNECTORS) - Amphenol Antenna Solutions
CONTROL & AISG PROTOCOL SELECT ACTUATOR SELECT CONNECTOR TYPE ANTENNA MODEL NUMBER Manual Electrical Tilt (MET) ---4.3-10 Female 6890308N 7/16-DIN Female 6890308 Remote Electrical Tilt (RET) AISG v2.0 / 3GPP Multi-Device Control Unit (MDCU) 4.3-10 Female 6890308NG 7/16-DIN Female 6890308G
Rolling Mill - Temposonics
Rolling mills depend on linear position sensors to precisely control the roller displacement using Automatic Gauge Control (AGC) cylinders. The sensor models with SSI output and optional linearization provide the speed and accuracy required for this application. With the robustness of Temposonics technology, the lifetime maintenance costs and ...
Sensing Technologies used for Accelerometers | PCB Piezotronics
The amount of force is proportional to applied acceleration as governed by Newton's law of motion F=ma. Piezoelectric accelerometers cannot measure constant acceleration because they are inherently AC coupled, however, they are typically the most versatile and economic choice for measuring fast transient and periodic acceleration.
CO2-based Ventilation Control Where Required and Recommended
CO2-based Ventilation Control Where Required and Recommended Amphenol Advanced Sensors ® Application Note Ventilation is an important part of maintaining a comfortable, healthy, productive environment for students
Technical Information | PCB Piezotronics
Download technical information on PCB's products. PCB ® manufactures sensors used by design engineers and predictive maintenance professionals to test and measure vibration, pressure, force, acoustics, load, and shock in research and development as well as industrial applications.. Divisions of PCB
General Purpose Piezoelectric Accelerometers - PCB
PCB ® manufactures sensors used by design engineers and predictive maintenance professionals to test and measure vibration, pressure, force, acoustics, load, and shock in research and development as well as industrial applications.. Divisions of PCB
Profile - Custom Cable
Situation Headline. NBC broadcasts live from 30 Rockefeller Plaza, New York City, and reports news events throughout the world 24/7/365. To keep connected on the street and in the studio, NBC Studios requires a myriad of critical connections, from road case fiber rack panels (FRP) for easier transport and handling of panels to a fiber-to-the-desk (FTTD) cassette solutions.
Magnetostrictive Linear Position Sensors INDUSTRIAL - Temposonics
magnet, connected to the object in motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide. This creates a momentary radial magnetic field and torsional strain on the waveguide. The momentary interaction of
Triaxial variable capacitance accelerometer - PCB
applications require the measurement of whole body motion in three mutually orthogonal directions immediately following shock motion or in the presence of severe vibrational inputs. State of the art temperature compensation electronics provide for precise compensation over a wide temperature range, while maintaining a full analog signal path.
Load Cells article - PCB
PCB LOAD & TORQUE, INC. 24350 Indoplex Circle, Farmington Hills, MI 48335 USA Phone: 866-684-7107 Fax: 716-684-0987 Email: ltinfo@pcbloadtorque.com www.pcbloadtorque.com
Data Sheet R-Series V RH5 EtherNet/IP 551954 - Temposonics
control coordination in time-critical applications. Internal linearization The sensor is available with internal linearization which offers improved linearity for overall higher accuracy of the position measurement value. In addition the R-Series V EtherNet/IP™ scores with the following features: 20 positions simultaneously
Data Sheet R-Series V RP5 EtherNet/IP - Temposonics
The magnet, connected to the object in motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide. This creates a ... EtherNet/IP™ network, allowing for increased control coordination in time-critical applications. DLR capability provides a fault-tolerant
A real desire to integrate sustainable development - CMR Group
Today, CMR develops, manufactures and implements control and supervision solutions for the energy, industrial and marine sectors. It does this by integrating its own smart sensors and automated systems. With nearly 1000 employees – including 100 based in France– CMR Group has offices and production sites in 11 countries and generates 90% of ...
R-Series RP CANbus 551780 - Temposonics
to the control unit. The bus interface is appropriate for serial data transfer of 1 Mbit/s maximum. Sensor integrated software supports the profiles CANopen and CANbasic for a comprehensive customized configuratio n of the sensor-bus system. 4 5 3 1 Measurement Cycle 1 Current pulse generates magnetic fi eld 2 Interaction with position magnet ...
Temposonics
motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide. This creates a momentary radial magnetic field and torsional strain on the waveguide. The momentary interaction of the magnetic fields releases a torsional strain pulse that propagates the length of the ...
Sensing Geometries for Piezoelectric Accelerometers - PCB
For an accelerometer, a seismic mass is coupled to the crystal. When under the influence of acceleration, the mass will cause a force to act upon the crystal, thus generating a proportional electrical output. This cause and effect relationship is defined by Newton's Law of Motion F=ma.
Contact Us | PCB Piezotronics
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
History - Temposonics
1984. Temposonics Inc. is acquired by MTS Systems Corporation and the MTS Sensors Division is formed. Temposonics remains the brand name for the measurement technology that characterizes the sensors.
HEX456CW0000x - Amphenol Antenna Solutions
Tri Band, 6-Port, Panel, XPOL, 45°, 696-960 | 1695-2180 | 1695-2180 MHz, 16.2|18.3|18.3 dBi, 0-12°|0-10°|0-10°, 1780 mm (70.1 in)