Search Results for motion control
PCB Piezotronics | Measure vibration, pressure, force, and more
PCB Piezotronics | Measure vibration, pressure, force, and more
Control cabinet with LUTZE LSC
During the control cabinet LSC frame installation the prefabricated frame can be immediately populated, wired and then installed into the control cabinet, thus resulting in reduced installation time. Share : Fast start and completion of assembly.
Magnetostrictive Linear Position Sensors INDUSTRIAL - Temposonics
magnet, connected to the object in motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide. This creates a momentary radial magnetic field and torsional strain on the waveguide. The momentary interaction of
PCB Piezotronics | Measure vibration, pressure, force, and more
PCB Piezotronics | Measure vibration, pressure, force, and more
SSI Technologies – TULC Application Note
SSI TECHNOLOGIES, INC. Controls Division 3200 Palmer Drive Janesville, WI 53547-5011 Phone: (608)758-1500 Fax: (608) 758-2491 www.ssitechnologies.com
MDCU Module - Amphenol Antenna Solutions
RET Actuator, Multi-Device Control Unit for Single Band or Multi-Band Antennas
SENSORS FOR MOTORSPORT TESTING - PCB
series 3711F, 3713F, 3741F, and 3743F DC response sensors are used to measure low frequency motion down to zero. hertz. These accelerometers are used in motorsport applications with low frequency and amplitude requirements, as well as ... single axis accelerometers provide the measurement signals needed to control the vibratory input and to ...
PCB Price List | PCB Piezotronics
3425 Walden Avenue Depew, NY 14043. Sensorline SM 716.684.0001. info@pcb.com +1 800-828-8840
Data Sheet R-Series V RP5 Analog - Temposonics
electronics. The magnet, connected to the object in motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide. This creates a momentary radial magnetic field and torsional strain on the waveguide. The momentary interaction of the magnetic fields releases a torsional
Spread Sensors Pro - marport.com
The distance is calculated from the warp lengths sent by a winch control system. Scala2 application can calculate the positioning of the trawl from this distance, the depth and bearing angle. The distance between the two hydrophones (2) is called the baseline (1). To have positioning data, the system must have the following equipment:
Installation Manual MH-Series Flexible MH - Temposonics
motion in the application, generates a magnetic field at its location on the waveguide. A short current pulse is applied to the waveguide. This creates a momentary radial magnetic field and torsional strain on the waveguide. The momentary interaction of the magnetic fields releases a torsional strain pulse that propagates the length of the ...
Force Sensors | PCB Piezotronics
PCB's quartz, piezoelectric force, and strain sensors are durable measurement devices with exceptional characteristics for measuring high frequency dynamic force and strain events.
6177788G - Amphenol Antenna Solutions
Extreme operational conditions and/or stress on structural supports is beyond our control. Such conditions may result in damage to this product. Improvements to products may be made without notice. ... Power Consumption ≤ 2W (Idle), ≤ 10W (In Motion) Hardware Interface RS485 and Power Logical Interface HEX Coded Commands Based on HDLC ...
Product Finder - Lutze Inc.
LUTZE Inc. 13330 South Ridge Drive • Charlotte, North Carolina 28273 • USA Phone: 704-504-0222 • Fax: 704-504-0223 • E-Mail: info (at) lutze.com
Acceleration Sensing Technologies for Severe Mechanical Shock - PCB
6 Since optimal damping cannot be attained with a simple elastomeric material, nominal 2-pole low pass electrical filtering is also incorporated in the accelerometer to attenuate any residual resonant peak associated with the isolator.
Load Cells - PCB
• Quality Control • Tank Weigh Application Questions 1. Determine the capacity required: A. What is the maximum expected load? B. What is the minimum expected load? C. What is the typical expected load ? D. What are the dynamics of the system, i.e. frequency response? E. What are the maximum extraneous loads that the load cell will be ...
AirSTREAM in detail - Lutze Inc.
AirSTREAM with module parts for individually configurable frames offer unrestricted freedom and flexibility for modern control cabinet construction. Compatibility to previous systems. The new AirSTREAM is compatible with the old LSC-B, even existing design plans can be used, without re-design.
PRODUCT SPECIFICATION GS-12-400 - Amphenol CS
Pin Stability No visible motion of the board interface Pins assembled to a PCB shall experience a motion of 30° magnitude in any radial direction at ... FCI is committed to a Zero Defect Philosophy utilizing Statistical Process Control. Our commitment to Zero Defects is a continuous improvement in process quality.
Isotron accelerometer - PCB
Vibration limit (sinusoidal motion) [4] g 500 Shock limit [5] g pk 5000 Base strain sensitivity at 250 µstrain g/µstrain 0.001 Electromagnetic equiv g/100 gauss 0.005 ... support of stringent Quality Control requirements, and compulsory corrective action procedures. These measures, together with conservative specifications ...
Select a Part - Positronic The Science of Certainty
The AD series is part of the Adapter/Saver family and Helps prevent unwanted wear during testing. Offers industrial performance with size 20 contacts.