Search Results for what is a ultrasonic sensor
Certificate of Registration SSI Technologies, LLC
Ultrasonic Level and Concentration Sensors; Heater Modules; Tank Assemblies and Printed Circuit Board Assemblies. Jennifer Morecraft, Senior Managing Director Page 1 of 2 Certificate Number: C0161575-IS11 Certificate Issue Date: 25-MAY-2022 Registration Date: 24-MAY-2022 Expiration Date *: 23-MAY-2025
Temposonics
ultrasonic wave reaches the end of the waveguide it is converted into an electrical signal. Since the speed of the ultrasonic wave in the waveguide ... sensors at a manufacturing facility, it can be extremely challenging in the field. Trained service technicians can remove and replace the
Data Sheet R-Series V RDV Analog - temposonics.com
ultrasonic wave reaches the beginning of the waveguide it is converted into an electrical signal. Since the speed of the ultrasonic wave in the ... sensor RDV is the version of the R-Series V with a detached sensor electronics. The main advantages of the version RDV are:
Marport Appoints New Distributor in the United Kingdom
commercial fishing fleet and has been a leading innovator in sensor solutions in that sector ever since. Marport is a subsidiary of the Airmar Technology Corporation. www.marport.com About Airmar AIRMAR Technology Corporation is a world leader in the design and manufacture of ultrasonic sensor technology for marine and industrial applications.
Model 112A05/061M319 Charge Output Pressure Sensor Installation ... - PCB
The Series 113A High Frequency Miniature Sensor is a charge mode pressure sensor designed to measure shock wave, blast, explosion, ultrasonic and dynamic combustion pressures requiring ultra-fast response times. The Series 113A consists of the Models 113A, 113A02, and 113A03, having pressure ranges of 3 000, 100, and
Absolute, Non-Contact Position Sensors Data Sheet C ... - Temposonics
The customer-specific sensors are used to monitor the steering position of rear drives and to provide position feedback. Based on the linear C-series position sensor, these sensors are equipped with a special housing, which was developed by the end user and realized by Temposonics. The sensors measure the stroke of steering cylinders
Temposonics
Since the speed of the ultrasonic wave in the wave-guide is precisely known, the time required to receive the return signal ... accuracy and repeatability. GB-M / GB-T SENSOR Robust, non-contact and wear free, the Temposonics® linear position sensors provide the best durability and accurate position measure-ment solutions in harsh industrial ...
Data Sheet *%ZLWKWKUHDGHG DQJH$QDORJ
The GB sensors fulfill the requirements of the EMC directives 2014/30/EU, UKSI 2016 No. 1091 and TR CU 020/2011 Operating pressure 350 bar (5,076 psi), 700 bar (10,153 psi) peak (at 10 × 1 min) Magnet movement velocity Any Design/Material Sensor electronics housing3 Stainless steel 1.4305 (AISI 303) Sensor flange Stainless steel 1.4305 (AISI 303)
careers | Amphenol Global Search | Amphenol
Level Sensors. Whatever your media, tank depth, and profile, SSI Technologies, LLC most likely has an ultrasonic liquid level sensor for you. Our ultrasonic liquid level sensors use ultrasonic technology to generate a high-frequency sound wave to measure the time for the echo to reflect off of the target and return to the ultrasonic liquid level sensor.
Data Sheet R-Series V RP5 SSI - Temposonics
The sensor is characterized by a very stable position signal with a minimum resolution of 0.1 μm. Synchronous measurement The sensor offers one asynchronous mode as well as three different synchronous modes to match the measurement to the data request cycle of the controller. Extrapolation The sensor supports linear extrapolation. This
Data Sheet R-Series V RP5 Profinet 551961 - Temposonics
Fig. 2: R-Series V sensor with TempoLink smart assistant MEASURING TECHNOLOGY The absolute, linear position sensors provided by Temposonics rely on the company’s proprietary magnetostrictive technology, which can determine position with a high level of precision and robustness. Each Temposonics position sensor consists of a ferromagnetic
TB MH-Sensor 551217 RevE EN - Temposonics
position magnet. The runtime of this ultrasonic wave is measured precisely and compiled into standard electronic output signals. Simple Mechanics The extremely robust sensor consists of the following main parts: The innovative connector system which is easy to install in a few seconds, any soldering or crimping needless, dust-and waterproof
Level Plus - Temposonics
ultrasonic wave reaches the end of the waveguide it is converted into an electrical signal. Since the speed of the ultrasonic wave in the waveguide is precisely known, the time required to receive the return signal can be converted into a linear position measurement with both high accuracy and repeatability.
Temposonics
sensors provide best durability and accurate position measurement solutions in harsh industrial environments. The position measurement ... When the ultrasonic wave reaches the end of the waveguide it is converted into an electrical signal. Since the speed of the ultrasonic wave in the waveguide is pre-
Temposonics
When the ultrasonic wave reaches the end of the waveguide it is con-verted into an electrical signal. Since the speed of the ultrasonic wave in the waveguide is precisely known, the time required to receive the return signal can be converted into a linear position measurement with both high accuracy and repeatability. ER SENSOR
Privacy Policy - Amphenol Sensors
Ultrasonic Fluid Level Sensors. Continuously monitors liquid levels within tank or reservoir, including fuel, coolant and hydraulic fluids. High accuracy; Robust, non-contact sensing; Slosh filtering; Customizable options Vibration Sensors. Continuously monitoring engine balance.
B164 50/200kHz, 1kW, 0° Tilt, Garmin 6-Pin, DT - AIRMAR EMEA
1 kW. Step up to a 1 kW—without a fairing! The 1 kW, flush-mount, Tilted Element ™ transducer is perfect for fast, trailered vessels that cannot accommodate a High-performance Fairing. The flush-mounted, bronze housing extends less than 6.35 mm (1/4") below the hull, so it can sit on trailer rollers and bunks.
PCB Piezotronics | Measure vibration, pressure, force, and more
PCB ® manufactures sensors used by design engineers and predictive maintenance professionals to test and measure vibration, pressure, force, acoustics, load, and shock in research and development as well as industrial applications. Divisions of PCB. Subscribe.
Temposonics
When the ultrasonic wave reaches the end of the waveguide it is con-verted into an electrical signal. Since the speed of the ultrasonic wave ... sensor provide the best durability and precise position measurement feedback in harsh industrial environments. Measurement accuracy is
Acu-Trac™ NEMA 6 Liquid Level Transmitter Product Overview
Acu-Trac™ NEMA6 uses ultrasonic technology to generate a high frequency sound wave and measure the time for the echo to reflect off of the liquid’s surface and return. The distance from the liquid l evel transmitter to the fuel is calculated based on the speed of sound. The measured distance is converted into a