Search Results for where is this place
GS-12-240 Rev E - Amphenol CS
Place the connector on the PCB and expose to the reflow oven. Peak Temp: 260℃ for 10sec. No physical damage such as crack and deformation of housing. 5.3.5 Solderability EIA 364-52 ( or MIL-STD-202F, Method 208G ). The surface of the portion to be soldered shall at least 95% covered with new solder coating.
Industrial Sensor Resource Hub | Amphenol Advanced Sensors
For initial screening of individuals before gaining access to a specified area, such as a place of work, store, school, or public transportation. CO2 SENSOR SNIFFS OUT HUMAN SMUGGLERS Learn how advanced CO2 sensor technology can help in the fight against human trafficking.
Liquid-Nitrogen (LN2) Solutions - KAYE
Cryogenic gases like liquid nitrogen (LN 2) are crucial in the pharmaceutical and biotechnology industries, enabling the safe storage of intermediates and raw materials by preventing interactions with moisture or oxygen.LN 2 and dry ice are also used in various processes, including mixing, storage, and cryogenic cooling.. Benefits of Cryogenic Containers
Model 638A06 Cryogenic, industrial, quartz shear ICP accel, 25 mV ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
LT93-SMTBST50-1 PR2 - Charles Industries
After wiring is complete and all access covers are in place, shore power may be applied. The green AC Power light should be on. The Boost light may or may not be on depending on input voltage. If the AC Power light is not on, consult the Troubleshooting section of this manual. TROUBLESHOOTING Table 2. Troubleshooting Suggestions Item Symptom ...
Cable Assemblies | Interconnects | Mobile, RF, Optics - Amphenol CS
Amphenol Communications Solutions (ACS), a division of Amphenol Corporation, is a world leader in interconnect solutions for Communications, Mobile, RF, Optics, and Commercial electronics markets.
Model TO622B01 Platinum Precision Industrial ICP® Accelerometer ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
RF Technology: The Real MVP in Large Scale Sporting Events
Since then, RF technology has found a place in areas other than broadcasting, which alone has evolved substantially in the last century. Communication systems within stadiums, especially those involving wireless connectivity, such as Wi-Fi which utilizes IoT antennas on ISM bands and wireless ticketing devices that use NFC antennas, are among ...
Charles Fiber Optic Dome Closure FODCC Series General Description and ...
in place Tighten hose clamp . LT-FODCC 1 st Printing Page 5 of 8 10 . Route the buffer tube or the ribbon fiber slack into the transport basket. Use the cable ties included in the Accessories bag. If preferred, use customer supplied Velcro. Note: if using ribbon cable, use cable ties on
Charles Universal Broadband Enclosure SH60-482420 Universal Backplane ...
• Do not place this product on weak or unstable surfaces which may allow the product to fall, resulting in potentially serious damage(s) to persons or product. • Only authorized trained personnel shall install the SHRD60. • In windy conditions, be sure to engage the door latches to secure the door in a stationary position. 3.3.
Temposonics® Operation Manual E-Series IO-Link 551845
When returning sensors, place protective caps on male and female connectors of the sensor. For pigtail cables, place the cable ends in a static shielding bag for electrostatic discharge (ESD) protection. Fill the outer packaging around the sensor completely to prevent damage during transport.
Machinery health monitoring using displacement sensors
P 3 PC420DPP-40, 2008 Proprietary PC420DPP- 40 PC: Designed to work with an existing process control system for machinery health and process monitoring 420: Outputs a value between 4 and 20 mA that represents the overall vibration at the monitoring point D: The vibration is integrated to displacement to detect faults at the the 1x running speed
CONFIGURATION CONTROL LEVEL: REV DESCRIPTION DATE - SV Microwave
cable in place as shown. date approved revision history rev description n/a n/a n/a third angle projection 1) all dimensions are after plating. 2) break corners & edges .005 r. max. 3) cham. 1st & last threads. 4) surface roughness 63 mil-std-10. 5) dia.’s on common centers to be concentric within .004 t.i.r. 6) remove all burrs unless ...
Model 353B31 High sensitivity, quartz shear ICP® accel., 50 mV/g ... - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
Model M608A11/030BZ Platinum Low-cost Industrial ICP® Accelerometer ...
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
Continuous Condition Monitoring With Vibration Transmitters and ... - PCB
since the monitoring instrumentation already is installed and trained personnel are in place. Once the decision is made to implement a vibration monitoring program using existing monitoring instrumentation, the next task is to determine the equipment to be monitored and to define the machinery faults that need to be detected.
Operation Manual R-Series V Powerlink 552010 - Temposonics
When returning sensors, place protective caps on male and female connectors of the sensor. For pigtail cables, place the cable ends in a static shielding bag for electrostatic discharge (ESD) protection. Fill the outer packaging around the sensor completely to prevent . Temposonics® R-Series V POWERLINK O
ROKK Wireless - Waterproof Wireless Phone Charging Mat 12/24V - Gemeco
Simply place your phone onto the center of the charging mat and instantly start wirelessly charging. The cleverly designed edging bumpers stops your phone from sliding out, and lets the mat Catch your phone from any angle! Constructed from our Closed Cell EVA foam, Catch offers great shock absorption and anti-vibration for your phone while ...
Ultrasonic Point Level Sensor
it is important to place the Fluid-Trac® PLS sensor’s face in the center of the tank perpendicular to the liquid level and with no obstructions in the beam path to the liquid. Cone Angle Fluid-Trac® PLS mounting that is not perpendicular to the fluid causes a reduction in its sensor performance. As shown in Figure 3, the amount of
Charles Universal Broadband Enclosure CUBE PM648154N1 General ...
Do not place this product on weak or unstable surfaces which may allow the product to fall, resulting in potentially serious damage(s) to persons or product. Only authorized trained personnel shall install the CUBE. In windy conditions, be sure to engage the door latches to secure the door in a stationary position. 3.3.