Search Results for where is this place
Applying predictive maintenance technologies to improve efficiencies
place. By adding a vibration sensor to each end of a generator, both the drive end and opposite drive end can be monitored on a continuous basis to detect changes such as alignment and looseness. Wheel drive motors These units are typically equipped with roller element bearings. It is well documented that accelerometers de-
Model 333B30 ACCELEROMETER Installation and Operating Manual - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
Model 3741F12100G Differential MEMS DC accelerometer, 27 mV/g, 100 g ...
sockets. Then thread the connector into place by turning the cable connector’s outer shell onto the accelerometer’s electrical connector. 4.1 SCREW MOUNT This mounting technique requires smooth, flat contact .
Model 625B21 Precision Industrial ICP® Accelerometer ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
RJ45 Modular Jack Connector | FCI Basics - Amphenol CS
Amphenol's FCI Basics RJ45 Jacks offer single/multi-port solutions for Telecom, Data, Networking, and Home Entertainment, supporting a variety of applications.
MEASURING CONDENSATION IN BUILDINGS BUILDING SURVEYOR’S GUIDE
2. Place the hygrometer in the area where you suspect there may be condensation. Be sure to keep it away from windows, doors, or other areas where it may be exposed to direct sunlight or drafts. 3. Allow the hygrometer to acclimate to the room temperature for at least 15-20 minutes and make sure the room stays undisturbed. 4.
Introduction to Piezoelectric Force Sensors | PCB Piezotronics
This is especially true with force sensor applications where static calibration or quasi-static measurements take place. (Before performing tests of this nature, it is important to DC couple the entire monitoring system to prevent rapid signal loss. PCB 484 Series signal conditioners have AC/DC mode of operation and are designed for such ...
GS-12-240 Rev E - Amphenol CS
Place the connector on the PCB and expose to the reflow oven. Peak Temp: 260℃ for 10sec. No physical damage such as crack and deformation of housing. 5.3.5 Solderability EIA 364-52 ( or MIL-STD-202F, Method 208G ). The surface of the portion to be soldered shall at least 95% covered with new solder coating.
Kaye ValProbe (RT) Transport / Storage Tray
The space-optimized slots for the data loggers hold each individual logger securely in place, preventing damage during transport and ensuring that the loggers remain in optimal condition for accurate data logging. This organized layout supports systematic calibration and qualification procedures, saving valuable time and reducing the risk of ...
Model 638A06 Cryogenic, industrial, quartz shear ICP accel, 25 mV ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
Quality - LID Technologies
Finally, we place Social, Economic and Environmental Responsibility at the heart of our corporate project. This voluntary approach has been implemented through numerous initiatives such as the establishment of a code of conduct for our suppliers, raising their awareness about over-packaging, the renovation of our offices, waste sorting, the ...
3652-35 4-Wire E&M with Extended Range (4W E&M/ER) Channel Unit
Do not force a module into place. If excessive resistance is encountered while installing a module, remove the module, and check the card guides and connector to verify proper alignment and the absence of foreign material. Align the channel unit with the appropriate card-guided slot of the terminal. Slide the unit into the slot with the
Model 352C65 ACCELEROMETER KIT Installation and Operating Manual - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
7305–46 Data Channel Interface W/SC Generator - Charles Industries
Do not force a module into place. If excessive resistance is encountered while installing a module, remove the module and check the card guides and connector to verify proper alignment and the absence of foreign material. CAUTION. Section 730-546-203 5 Figure 2. 7305-46 Data Channel Interface with SCG (Issue 3) Block Diagram
Protimeter Standard Speedy | Dependable Pressure Testing
Applications. Speedy moisture testers from Ashworth Instrumentation are used throughout the world by a diverse range of industries to measure the moisture content of materials including soils, aggregates, concrete, sand and powders.
Model 623C10 High Frequency Industrial ICP® Accelerometer ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
Model M607A01 Swiveler® Industrial ICP® Accelerometer ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
Charles Universal Broadband Enclosure CUBE-MP1310 General Description ...
• Do not place this product on weak or unstable surfaces which may allow the product to fall, resulting in potentially serious damage(s) to persons or product. • Only authorized trained personnel shall install the CUBE. 3.3. Obtaining Tools and Equipment Obtain the following recommende d or needed items for installing the CUBE.
MIL-DTL-38999 Assemblies - Amphenol PCDAmphenol PCD
Interconnect systems optimized for the extensive data transmissions that take place within modern missiles and guided munition systems during flight. Ruggedized products, optimized for performance and endurance in the world’s harshest environments, and engineered to achieve consistently exceptional performance.
Model 105C22 Subminiature ICP® pressure sensor, 1 mV/psi, 0.099 ... - PCB
may be epoxied in place if necessary. Do not over torque clamp nut, as to do so may distort the body of the sensor and affect the sensitivity of the device. The electrical connection to this model is made by soldering the positive (center conductor) lead from the power unit to the .040 diameter solder terminal provided. (IMPORTANT!