Search Results for where is this place
Model 356A67 Triaxial ICP® Accel., 10 mV/g, 500 g, 0.5 to 2.5 kHz, 1/4 ...
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
Model 355B02 Ring-style, general purpose, ceramic shear ICP ... - PCB
3.) for best results, place a thin layer of silicon grease (or equivalent) on interface a prior to mounting. [3> mounting surface should be flat to within .001 [0.03] tir over dim" a" with a minimum 63 [1 \yfinish for best results. [r> drill perpendicular to mounting surface to within :i: 10.
Providing Fiber-Based Business Services - amphenol-ns.com
The stubs are then run to a central collector terminal, which is the only place that on-site splicing is required. This approach minimizes the impact on operations, ensures a consistent deployment throughout, and reduces project costs by eliminating much of the labor involved in the more traditional approach, particularly those dollars spent on ...
Model HT354C02 Triaxial, thru-hole mtg, ceramic shear ICP® accel ... - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
Model 059740-01185 Fastener Torque-Tension Load Cell, Clamp Load ... - PCB
are in place to prevent any personal injury or equipment damage. 3.0 OVERVIEW Fastener torque-tension load cells come in a wide range of capacities to handle bolt diameters ranging from #4 (3mm) to 2½ inches (64mm). 3.1 Dimensions 8 7 Figure 2 - Dimensions Table 2 - Dimension Values Table 1 - Full-Scale Capacities 1 4 5 3 7 11
Vibration Monitoring of Gearboxes - PCB
1 VIBRATION MONITORING OF GEARBOXES Article by: James C Robinson, Technical Consultant, IMI division of PCB Piezotronics Curated by: Meredith Christman, Product Marketing Manager, IMI division of PCB Piezotronics INTRODUCTION Gearboxes are a common component in many industries, including chemicals, sugar, steel, mining, plastics, oil &
Model M601A02 Low-cost Industrial ICP® Accelerometer Installation and ...
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
CE23-0106 MHD2 Connector Design Guidelines Revision
1.4. General Product Description 1.4.1. The standard XHD2 differential interconnect platform consists of connectors featuring 3, 4, or 6 differential pairs, with an optional extra ground lead available on the A wafer. 2 Pair and 8 Pair
LTR-90 Ultra Cool Dry Block Calibrator - KAYE
Kaye ValProbe RT CO 2 Logger. The 3-in-1 data logger from the Kaye ValProbe RT product line offers the capability to measure critical parameters such as CO 2 (carbon dioxide), relative humidity (RH), and temperature with a single device. For applications where these measurements are quality-critical, the Kaye ValProbe RT CO 2 Logger provides economical, accurate, and GxP-compliant recording ...
Model 356A14 Triaxial ICP® Accel., 100 mV/g, 50 g, 0.5 to 5 kHz ... - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
Operation Manual R-Series V EtherCAT 552059 - Temposonics
For pigtail cables, place the cable ends in a static shielding bag for electrostatic discharge (ESD) protection. Fill the outer packaging around the sensor completely to prevent damage during transport. Temposonics® R-Series V EtherCAT ...
SMA Female PCB Thru-Hole Connector 2985-6004 | SV Microwave
SV Microwave proudly presents the SMA Female PCB Thru-Hole Connector 2985-6004. Check out the product specifications and place your order.
Is a Custom Connector Your Best Option? - Positronic
Custom connectors may also be a good option in situations where the connector selection is taking place late in the design process and the use of a standard connector is not possible for one reason or another. By opting for a uniquely tailored or fully custom component, manufacturers can specify the size, shape, number of contacts, performance ...
6-Port Antenna
RET control, the transparent caps must be in place and locked. The tilt angle indicators always remain visible and the antenna still has manual tilt control (manual override). Do not remove the transparent cap(s) from the antenna.
Model 123A Charge Output Pressure Sensor Installation and Operating Manual
During in-place calibration static methods (dead weight tester) may be used in a drift-free system by placing the charge amplifier in "LONG TC" position. However, during actual use, the TC mode switch should be in "SHORT" position for two reasons. Often times, the dynamic pressure being measured
Model W138A01/038CY003AC Tourmaline ICP® underwater blast sensor ... - PCB
coaxial cable (eg. RG-58/U) can now be used in place of the micro cable. Because of e largeth mass of the 070A03 compared to the 1032 jack, this- connection should be sealed and protected from shock and turbulence. Putting a two to three inch diameter of duct seal, wrapped with a waterprooftape, will seal the
Application Notes | Protimeter Moisture Meters
The theoretical ideal is to cover the suspect damp area with a waterproof tent of polythene, foil, or box and place a humidity measurement device under it. Water evaporating from the wall, into the small amount of air trapped in the tent or box will raise the relative humidity (RH) until it is in equilibrium. Then, by measuring the RH, it is ...
Model 117M50 Charge Output Pressure Sensor Installation and ... - PCB
place it around sensor barrel. 4. Begin threading the sensor clamp nut into the threaded mounting port, sliding slotted clamp fore and aft as needed to allow guide pin to fully enter hole. Continue to turn clamp nut into hole by hand or using 5/16 open end wrench. Do not tighten when sensor bottoms. 5.
PRODUCT BULLETIN - Charles Industries
To place orders or should you have any questions regarding this bulletin, please contact your Charles Inside Sales Representative directly, or phone 847-258-8526. QUESTIONS/COMMENTS: Dave Schwass Sr. Product Manager, Charles Industries, Ltd. 847-258-8388 dschwass@charlesindustries.com .
550905G M-Series Model MR Sanitary Application data sheet 07/13 (US)
Drain-in-place with end plug CP Clean-in-place DN Drain-in-place no through hole End plug style comes with permanently mounted floats. These floats cannot be removed from the pipe. IMPORTANT: Float, part number 401513-X is recommended for use with all Sanitary transmitters as other floats could enter the ‘Inactive Zone’ when the tank is ...