Search Results for where is this place
Model 352A60 High frequency, ceramic shear ICP® accel., 10 mV/g ... - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
Environmental Monitoring - KAYE
KAYE HEADQUARTERS. Amphenol Advanced Sensors Germany GmbH Sinsheimer Strasse 6 D-75179 Pforzheim. T +49 (0) 7231-14 335 0 F +49 (0) 7231-14335 29 kaye-ccpf@amphenol-sensors.com
Whip Antennas MU 5-X/... - AMPHENOL PROCOM
Mounting can take place exclusively with access from the outside when drilling an 18 mm dia. hole. Mounting can take place from the inside by drilling a 14 mm dia. hole. When mounting in a 14 mm dia. hole, remove the bottom plastic ring of the packing gasket with a sharp cutter.
The Magical World of Virtual Reality - Amphenol CS
These devices have a slot to place the smartphone inside, which acts as the screen. VR products have numerous applications, including simulations of actual situations. Though they were initially used to revolutionize gaming, the UK and US military have adopted VR to train their armies through flight, military, and emergency simulations.
FIBER OPTIC CABLE ASSEMBLY MANUFACTURABILITY AND DESIGN GUIDE
b) Character size • Character height of 0.1 inches is the default. Maximum number of characters per line is 22 to 25. • Different character heights may be used for specific applications so that information fits into the available space on the label. • All marking shall be legible or free from smears and smudges. c) Number of lines of information
Conformal Sensor Measures Ammunition Pressure Through Cartridge Case - PCB
pressure)readings)[1].Furthermore,thegaspassagein) frontofthesensormaybecomerest rictedorpluggedand) require)frequentcleaning.))) Drilled&cartridge&location&
Model 353B32 ACCELEROMETER KIT Installation and Operating Manual - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
Issue 1 Print 5 LT‐IMCHRGR60‐1 IMC Series & OWNER’S MANUAL Model 93 ...
Never place the IMC Series directly above the battery being charged; gases from the battery will corrode and damage the IMC Series . 3. Never allow battery acid to drip on the IMC Series when reading gravity or filling the battery. 4. Do not operate the IMC Series in an enclosed area or restrict ventilation in any way.
Brochures - kayeinstruments.com
KAYE HEADQUARTERS. Amphenol Advanced Sensors Germany GmbH Sinsheimer Strasse 6 D-75179 Pforzheim. T +49 (0) 7231-14 335 0 F +49 (0) 7231-14335 29 kaye-ccpf@amphenol-sensors.com
APQP - CUMMINS AND CMR GROUP WORKING TOGETHER
During this partnership, CMR continued to learn and develop its understanding of APQP but also how each of its elements could work best and within its organization, with the aim of improving controls and to introduce new products. For each project, controls on CMR products have been put in place and are improved during each work session, as well as the documentation which is updated and which ...
Using Probe Microphones for Nearfield Acoustic Holography ... - PCB
place at not only different spatial points, but also different temporal points, the phase of the acoustic waves must be considered. To do this, one probe microphone was used as an amplitude and phase reference microphone. It was fixed to the base as shown below. If we denote the moving and reference microphones as A and B,
Motorsport Testing Sensors | PCB Piezotronics
Motorsport encompasses more than just Formula 1 and NASCAR automobiles vying for first place glory as they power around a track at speeds topping 220 mph/350 kph. The Motorsport industry also entails the racing of motorcycles, trucks, water craft, snowmobiles, go carts, and even lawn mowers. Whatever it is that’s racing, these vehicles are ...
VibraLINK switchable junction boxes Installation and operating guide ...
12 channels. Once cables are installed use the compression bridge to hold the cables in place. For single output accelerometers, J9T2A two conductor shielded cable is recommended. For multi-function (dual-output) transducers, J9T3A three conductor shielded cable is recommended. Both
Launching Into The New Year - TPC Wire
A Mobile Catalog. Customers were seeking a way to access our product information at their fingertips 24/7. This year we are happy to announce that we will be launching a new catalog app in 2020 allowing mobile users to have access to the most complete and accurate cable, wire, connectors, and accessories data from TPC.
Catch Sensors User Guide - Marport
Never place the product in a hazardous and/or flammable atmosphere. Product installation and use Install and use this product in accordance with this user manual. Incorrect use of the product may cause damage to the components or void the warranty. Only qualified Marport dealers can do maintenance and repairs on internal components of the sensors.
Model 607A61/030BZ Spindler® Industrial ICP® Accelerometer ... - PCB
constant current circuits in place of the diodes, particularly when driving long signal cables (see Section 5). Decoupling of the data signal occurs at the output stage of the signal conditioner. A 10 to 30 µF capacitor coupled with a resistor shifts the signal level to essentially eliminate the sensor bias voltage.
21-33595-121-33595-1 21-33595-1 Contact, Socket, Triaxial Type ARINC ...
IN PLACE 21-33595-121-33595-1 Contact, Socket, Triaxial Type ARINC 600 Crimp Installation Instructions 1. Slide piggyback grommet seal over the cable jacket. 2. Slide theouter crimpbushing,flangeendfirst,over cablejacketsecure bushinginplacewithapieceof tape that can be removed later. 3. Trim cable and jacket to .485 inches as shown. 4.
Model 130B40 ICP® ELECTRET SURFACE MICROPHONE Installation and ... - PCB
Figure 5: One sided Adhesive Pad securing the Surface Microphone and Fairing in place Moderate to heavy air flow Microphone Top single-sided adhesive pad Base double-sided adhesive pad Fairing Low air flow All conditions/ no air flow - 5 - 4.2. Mounting Procedure
10141272 | Amphenol Global Search | Amphenol
Search Results for 10141272 c146 10g010 500 4 | Amphenol Global Search | Amphenol Parallel connectors are a type of electrical connector used to join two or more wires together side-by-side. They provide a secure and reliable connection, as the wires are inserted into a metal or plastic housing and secured in place with screws or clamps.
Model 132A31 Micro ICP® pressure sensor, 140 mV/psi, pigtail ... - PCB
place, maximum pressure specifications are given to prevent the sensors from being extruded from the mounting holes. Static or slow dynamic overpressures are more apt to cause a problem than a short dynamic shock pulse. Use of backing nuts will minimize the possibility of a problem. The microsensors are capable of responding to ICP