Search Results for where is this place
A5 A4 - MODIFY DIMENSIONS AND TOLERANCES 02NOV22 IAN TOMMY A5 - UPDATE ...
(13 place) 6 12.8 42.1±0.5 ∅40.1 1 11/16-18 unef thread 1 11/16-12 un thread 10.7 2.6 recommended panel mounting hole recommended panel thickness:1.6 to 4.7mm Ø43.08±0.12 41.45 +0.2-0 Ø50.8 47.6 110°ref 110°ref main polarizing keyway-1 9- p r - w t a a a h d p 0 4 24 m p h e n o l y y m m d d a2 c0765s update specifications 23nov17 ...
Model 138A Tourmaline underwater blast sensor, 7.6 length, 25k ... - PCB
coaxial cable (eg. RG-58/U) can now be used in place of the micro cable. Because of e largeth mass of the 070A03 compared to the 1032 jack, this- connection should be sealed and protected from shock and turbulence. Putting a two to three inch diameter of duct seal, wrapped with a waterprooftape, will seal the
Protimeter - Professional Moisture Meters & Hygrometers
Professional Moisture Meters & Accessories That Deliver . An industry leader with more than 70 years of experience, Protimeter offers innovative, dynamic, and high-performance professional moisture meters and accessories.Designed with the end-user in mind, Protimeter devices allow for accuracy, are easy to use, and are built with durable quality for everyday use.
PL 1300EV N SERIES Industrial Ethernet Connectors For Industrial ...
Place mounting ring between the panel and panel nut and tighten nut. Sealing Cap with Tether Sealing Cap In-Line Plug P/N 107304-01 Plug Sealing Cap P/N 107288-01 To install onto a cable assembly; open wire clip, place cable between the halves and close clip. Author: Matthew Smith
C70210M0080063 C702Y Landing EZ C702Y is a robust product li
Shock (w/o Disconnection): 10 g; 11 ms; halfsine 2 shocks / direction in 3 axis Insulation Resistance: 10(9) mΩ Contact Resistance: 100 mΩ data; 200 mΩ switch Extraction Force: 12 N Shock (w/o Destruction): 200 g; 6 ms; halfsine2 shocks / direction in 3 axis Chattering Time: 5 ms Insertion Force: > 2.5 N Climatic Category: 25 / 85 / 21 Operating Temperature:-25°C to +85°C
Charles Retrofit Kit 97-002497-A General Description and Installation
studs fit into these holes and secure in place using 1/4-20 Keps nuts (fourteen nuts in total, Figure 4). Figure 3 Install L-brackets (4) L-BRACKETS (2) 1/4-20 KEPS NUTS PER BRACKE T Figure 4 Mount Base Panel (12) 1/4-20 KEPS NUTS SECURED BEHIND SHRD60 (2) 1/4-20 KEPS NUTS PER BRACKET; LT-97-002497
Recent Design Updates and Selection Considerations - PCB
force that holds the crystal in place is perpendicular to the polarization axis, a shear design has extremely stable output over time. This enables extensive design flexibility and performance optimization (see Figure 4). Figure 4 There are numerous temperatures, bandwidth, mounting and other tradeoffs that must
Wilcoxon Sensing Technologies new brand and logo
You can expect initial changes to take place across our website, specification/data sheets, and sales materials. For purchases and other business communications, please transition to our new company name: Wilcoxon Sensing Technologies, 20511 Seneca Meadows Pkwy, Germantown, MD 20876
Meet the experts - Wilcoxon Sensing Technologies
With balance-of-plant monitoring and control in one place, it’s much simpler to realize the reliability gains that digital manufacturing offers: improved safety, optimized performance and longer machine life are there for all to take advantage of.
Machinery health monitoring using displacement sensors
P 3 PC420DPP-40, 2008 Proprietary PC420DPP- 40 PC: Designed to work with an existing process control system for machinery health and process monitoring 420: Outputs a value between 4 and 20 mA that represents the overall vibration at the monitoring point D: The vibration is integrated to displacement to detect faults at the the 1x running speed
Kaye ValProbe Freeze Dryer Logger
The X2534 ValProbe surface temperature logger design provides enhanced and precision wireless measurement capability ideal for freeze dryer shelf temperature measurement over an extended temperature range from -85°C to +140°C.
Mobile Mounts CX-Mount - AMPHENOL PROCOM
Installation. CX-mount antenna types can be mounted anywhere on the car, however, roof top mounting is always recommended. Mounting can take place exclusively with access from the outside when drilling an 18 mm dia. hole. Mounting can take place from the inside by drilling a 14 mm dia. hole, in which case the bottom plastic ring of the gasket should be removed with a sharp cutter.
Temposonics
place itself into the fail safe state. In this case the controller is able to separate the channels and the system can enter into a safe operational mode, where the machine is able to continue performing the function with one channel operation until the failed sensor gets replaced. 3.3 The safety function
Charles Universal Broadband Enclosure SH60-362322 Series General ...
• Do not place this product on weak or unstable surfaces which may allow the product to fall, resulting in potentially serious damage(s) to persons or product. • Only authorized trained personnel shall install the SHRD60. • In windy conditions, be sure to engage the wind latch to secure the door in a stationary position. 3.3.
Model 353B03 ACCELEROMETER KIT Installation and Operating Manual - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
Model 353B51 High sensitivity, quartz shear ICP® accel., 500 mV ... - PCB
3.) for best results, place a thin layer of silicone grease (or equivalent) on interface prior to mounting. mounting surface should be flat to within .001(0.03) tir over dim 'a' with a or better finish for best results. drill perpendicular to mounting surface to within 1 . sensor sensor "thru-bolt"
Application guide for PC420V Series LPS™ transducers
The rotating shaft is being held in place by the bearings the machine. Because the machine shaft is turning, the vibration is repeating at the rate the shaft turns. This repetitious vibration is considered to be “periodic.” The machine bearing also acts like a spring-mass system to transmit the vibration to the machine case.
Liquid Nitrogen Comparator - KAYE
Kaye ValProbe RT CO 2 Logger. The 3-in-1 data logger from the Kaye ValProbe RT product line offers the capability to measure critical parameters such as CO 2 (carbon dioxide), relative humidity (RH), and temperature with a single device. For applications where these measurements are quality-critical, the Kaye ValProbe RT CO 2 Logger provides economical, accurate, and GxP-compliant recording ...
Protimeter ReachMaster Pro | Moisture Meter on Telescoping Handle
Protimeter ReachMaster Pro = Efficiency + Safety. Allowing for fast and safe moisture inspections, the ReachMaster Pro lets users spend less time navigating obstacles while staying safe.. Able to survey areas just out of reach -- such as high ceilings or cramped crawlspaces -- the ReachMaster Pro decreases survey inspection times by up to 60%. With its extendable handle, this non-invasive ...
Smart Coil DSL Line Conditioning Device - An Amphenol Company
A service provider’s legacy copper network is a major financial asset. Telephone companies place the value of a single copper pair from several hundred to over a thousand dollars. Used in conjunction with the latest digital technology, Smart Coil-equipped legacy copper pairs help not only retain but increase revenue from customers.